Page 4 of 12
Be careful using this feature! It will output 5V and only 5V! If you’re working
with a 3.3V or 1.8V system, make sure this switch is in the No Power
position.
Installing Drivers
Driver installation is required on Windows machines only. If you’re using
Mac or Linux, feel free to click over to the next section. Otherwise, follow
along below as we overview the installation process.
There are two sets of instruction for driver installation on this page. The first
is the easiest, quickest method, and should work for most everyone. The
second installation process is only required if the first one fails – it takes a
more manual approach to the driver installation.
Install the Drivers Automatically with Zadig
To begin, plug the AVR Pocket Programmer into your computer. Upon
initially connecting the board, Windows will try to automatically install the
drivers. Some computers may be lucky, but most will turn up with a
message notifying you that the driver install failed.
Click the link below to download the drivers:
Download the Zadig USBtiny Drivers
Use your favorite unzipper to extract the ZIP file. Don’t forget where you put
the extracted folder!
After you’ve plugged the AVR Pocket Programmer into your computer and
your machine has run through the process of checking for and failing to
install drivers, proceed to the “zadig_v2.0.1.160” folder you just unzipped.
Then Run zadig.exe.
Zadig is a wonderful tool that can install the drivers on just about any
Windows platform out there. Upon opening the program, you should be
greeted with a window like this:
There are a few options to verify before installing the driver:
•Select the device – The top dropbox controls which device you want
to install the driver for. Hopefully you only have one option here,
something like “Unknown Device #1”. If you have more than one
option, check your device manager to see if you can make sense of
which is which (plugging and unplugging a device usually helps).
•Select the driver – Click the arrows in this box until you happen
upon libusb-win32 (vx.x.x.x), that’s the driver we want to install.
After verifying those two selections, click “Install Driver”. The installation
process can take a few minutes, but after you’ve watched the scroll bar
zoom by countless times, you should be greeted with a “The driver was
installed successfully” message.
If you were successful, close out of the Zadig program and proceed to the
next section!
If Zadig didn’t work for you, check out the instructions below for help
manually installing the drivers.
Page 4 of 1