I TEXAS
INSTRUMENTS
Vm.
er on
DE7 (NEE)
V Hm Vans :3
w 9
{sumam Baa
mas
um
Decocsr
ass
3 at H h 092
» ‘ as
A/D Convener um
use (LSB)
2.5v Eandgap
V Wm” WM AND conoL cmcmwv M
(MD
Vnsmur MCDE G fifiz/an
OBSOLETE
ADC08161
www.ti.com
SNAS075D –JUNE 1999–REVISED APRIL 2013
ADC08161 500 ns A/D Converter with S/H Function and
2.5V Bandgap Reference
Check for Samples: ADC08161
1FEATURES DESCRIPTION
This product is on Lifetime Buy and is NOT
2• No External Clock Required RECOMMENDED for new designs.
• Analog Input Voltage Range from GND to V+
Using a patented multi-step A/D conversion
• 2.5V Bandgap Reference technique, the 8-bit ADC08161 CMOS A/D converter
offers 500 ns conversion time, internal sample-and-
APPLICATIONS hold (S/H), a 2.5V bandgap reference, and dissipates
• Mobile Telecommunications only 100 mW of power. The ADC08161 performs an
8-bit conversion with a 2-bit voltage estimator that
• Hard-Disk Drives generates the 2 MSBs and two low-resolution (3-bit)
• Instrumentation flashes that generate the 6 LBSs.
• High-Speed Data Acquisition Systems Input signals are tracked and held by the input
sampling circuitry, eliminating the need for an
KEY SPECIFICATIONS external sample-and-hold. The ADC08161 can
perform accurate conversions of full-scale input
• Resolution: 8 Bits signals at frequencies from DC to typically more than
• Conversion time (tCONV): 560 (WR-RD Mode) ns 300 kHz (full power bandwidth) without the need of
max an external sample-and-hold (S/H).
• Full power bandwidth: 300 kHz (typ) For ease of interface to microprocessors, this part
• Throughput rate: 1.5 MHz min has been designed to appear as a memory location
• Power dissipation: 100 mW max or I/O port without the need for external interfacing
logic.
• Total unadjusted error: ±½ LSB and ±1 LSB
max
Block Diagram
1
Please be aware that an important notice concerning availability, standard warranty, and use in critical applications of
Texas Instruments semiconductor products and disclaimers thereto appears at the end of this data sheet.
2All trademarks are the property of their respective owners.
PRODUCTION DATA information is current as of publication date. Copyright © 1999–2013, Texas Instruments Incorporated
Products conform to specifications per the terms of the Texas
Instruments standard warranty. Production processing does not
necessarily include testing of all parameters.
l TEXAS
INSTRUMENTS
nau—
um —
m—
n?!—
vw, m—
m: —
an—
M—
m—
“mam
m
—V.
-Vm~.n
—or,
—Ca7
—r.ras
—:as
—ca¢
— :s
-Vnm
-Vw
OBSOLETE
ADC08161
SNAS075D –JUNE 1999–REVISED APRIL 2013
www.ti.com
Connection Diagram
Wide-Body Small-Outline SOIC Package
See Package Number DW
PIN DESCRIPTIONS
VIN This is the analog input. The input range is GND–50 mV = VINPUT = V++ 50 mV.
DB0–DB7 TRI-STATE data outputs—bit 0 (LSB) through bit 7 (MSB).
WR /RDY WR-RD Mode (Logic high applied to MODE pin)
WR: With CS low, the conversion is started on the rising edge of WR. The digital result will be strobed into the
output latch at the end of conversion (Figure 2,Figure 3,Figure 4).
RD Mode (Logic low applied to MODE pin)
RDY: This is an open drain output (no internal pull-up device). RDY will go low after the falling edge of CS and
returns high at the end of conversion.
MODE Mode: Mode (RD or WR-RD ) selection input– This pin is pulled to a logic low through an internal 50 µA
current sink when left unconnected.
RD Mode is selected if the MODE pin is left unconnected or externally forced low. A complete conversion is
accomplished by pulling RD low until output data appears.
WR-RD Mode is selected when a high is applied to the MODE pin. A conversion starts with the WR signal's
rising edge and then using RD to access the data.
RD WR-RD Mode (logic high on the MODE pin)
This is the active low Read input. With a logic low applied to the CS pin, the TRI-STATE data outputs
(DB0–DB7) will be activated when RD goes low (Figure 2,Figure 3,Figure 4).
RD Mode (logic low on the MODE pin)
With CS low, a conversion starts on the falling edge of RD. Output data appears on DB0–DB7 at the end of
conversion (Figure 1,Figure 5).
INT This is an active low output that indicates that a conversion is complete and the data is in the output latch. INT
is reset by the rising edge of RD.
GND This is the power supply ground pin. The ground pin should be connected to a “clean” ground reference point.
VREF-, VREF+ These are the reference voltage inputs. They may be placed at any voltage between GND - 50 mV and V++ 50
mV, but VREF+ must be greater than VREF-. Ideally, an input voltage equal to VREF-produces an output code of 0,
and an input voltage greater than VREF+ - 1.5 LSB produces an output code of 255.
For the ADC08161 an input voltage that exceeds V+by more than 100 mV or is below GND by more than 100
mV will create conversion errors.
CS This is the active low Chip Select input. A logic low signal applied to this input pin enables the RD and WR
inputs. Internally, the CS signal is ORed with RD and WR signals.
OFL Overflow Output. If the analog input is higher than VREF+, OFL will be low at the end of conversion. It can be
used when cascading two ADC08161s to achieve higher resolution (9 bits). This output is always active and
does not go into TRI-STATE as DB0–DB7 do. When OFL is set, all data outputs remain high when the
ADC08061's output data is read.
V+Positive power supply voltage input. Nominal operating supply voltage is +5V. The supply pin should be
bypassed with a 10 µF bead tantalum in parallel with a 0.1 ceramic capacitor. Lead length should be as short
as possible.
VREFOUT The internal bandgap reference's 2.5V output is available on this pin. Use a 220 µF bypass capacitor between
this pin and analog ground.
2Submit Documentation Feedback Copyright © 1999–2013, Texas Instruments Incorporated
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
OBSOLETE
ADC08161
www.ti.com
SNAS075D –JUNE 1999–REVISED APRIL 2013
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam
during storage or handling to prevent electrostatic damage to the MOS gates.
ABSOLUTE MAXIMUM RATINGS(1)(2)
Supply Voltage (V+) 6V
Logic Control Inputs −0.3V to V++ 0.3V
Voltage at Other Inputs and Outputs −0.3V to V++ 0.3V
Input Current at Any Pin(3) 5 mA
Package Input Current(3) 20 mA
Power Dissipation(4) 875 mW
Lead Temperature (Vapor Phase, 60 sec.) +215°C
(Infrared, 15 sec.) +220°C
Storage Temperature −65°C to +150°C
ESD Susceptibility(5) 750V
(1) All voltages are measured with respect to the GND pin, unless otherwise specified.
(2) Absolute Maximum Ratings indicate limits beyond which damage to the device may occur. DC and AC electrical specifications do not
apply when operating the device beyond its specified operating ratings. Operating Ratings indicate conditions for which the device is
functional, but do not ensure performance limits. For ensured specifications and test conditions, see the Electrical Characteristics. The
ensured specifications apply only for the test conditions listed. Some performance characteristics may degrade when the device is not
operated under the listed test conditions.
(3) When the input voltage (VIN) at any pin exceeds the power supply voltage (VIN < GND or VIN > V+), the absolute value of the current at
that pin should be limited to 5 mA or less. The 20 mA package input current specification limits the number of pins that can exceed the
power supply boundaries with a 5 mA current limit to four.
(4) The power dissipation of this device under normal operation should never exceed 875 mW (Quiescent Power Dissipation + TTL Loads
on the digital outputs). Caution should be taken not to exceed absolute maximum power rating when the device is operating in a severe
fault condition (e.g., when any input or output exceeds the power supply). The maximum power dissipation must be derated at elevated
temperatures and is dictated by TJMAX (maximum junction temperature), θJA (package junction to ambient thermal resistance), and TA
(ambient temperature). The maximum allowable power dissipation at any temperature is PDmax = (TJMAX −TA)/θJA or the number given
in the Absolute Maximum Ratings, whichever is lower. For this device, TJMAX = 105°C and θJA = 85°C/W.
(5) Human body model, 100 pF discharged through a 1.5 kΩresistor.
OPERATING RATINGS(1)
Temperature Range TMIN ≤TA≤TMAX
ADC08161CIWM −40°C ≤TA≤85°C
Supply Voltage, (V+) 4.5V to 5.5V
(1) All voltages are measured with respect to the GND pin, unless otherwise specified.
CONVERTER CHARACTERISTICS
The following specifications apply for RD Mode, V+= 5V, VREF+ = 5V, and VREF−= GND unless otherwise specified. Boldface
limits apply for TA= TJ= TMIN to TMAX;all other limits TA= TJ= 25°C.
Symbol Parameter Conditions Typical(1) Limits(2) Units (Limit)
INL Integral Non Linearity VREF = 5V ±1 LSB (max)
TUE Total Unadjusted Error(3) VREF = 5V ±1 LSB (max)
INL Integral Non Linearity VREF = 2.5V ±1 LSB (max)
TUE Total Unadjusted Error VREF = 2.5V ±1 LSB (max)
VREF = 5V 0Bits (max)
Missing Codes VREF = 2.5V 0Bits (max)
700 500 Ω(min)
Reference Input Resistance 700 1250 Ω(max)
VREF+ Positive Reference Input Voltage VREF−V (min)
V+V (max)
(1) Typicals are at 25°C and represent most likely parametric norm.
(2) Limits are specified to AOQL (Average Output Quality Level).
(3) Total unadjusted error includes offset, full-scale, and linearity errors.
Copyright © 1999–2013, Texas Instruments Incorporated Submit Documentation Feedback 3
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
OBSOLETE
ADC08161
SNAS075D –JUNE 1999–REVISED APRIL 2013
www.ti.com
CONVERTER CHARACTERISTICS (continued)
The following specifications apply for RD Mode, V+= 5V, VREF+ = 5V, and VREF−= GND unless otherwise specified. Boldface
limits apply for TA= TJ= TMIN to TMAX;all other limits TA= TJ= 25°C.
Symbol Parameter Conditions Typical(1) Limits(2) Units (Limit)
GND V (min)
VREF−Negative Reference Input Voltage VREF+ V (max)
GND −0.1 V (min)
VIN Analog Input Voltage See(4)
V++ 0.1 V (max)
On Channel Input = 5V,
Off Channel Input = 0V −0.4 −20 μA (max)
See(5)
On-Channel Input Current On Channel Input = 0V,
Off Channel Input = 5V −0.4 −20 μA (max)
See(5)
All Codes Tested,
PSS Power Supply Sensitivity VREF = 4.75V, ±1/16 ±½ LSB (max)
V+= 5V ±5%,
VIN = 4.85 Vp-p ,
Effective Bits 7.8 Bits
fIN = 20 Hz to 20 kHz
Full-Power Bandwidth VIN = 4.85 Vp-p 300 kHz
VIN = 4.85 Vp-p,
THD Total Harmonic Distortion 0.5 %
fIN = 20 Hz to 20 kHz
VIN = 4.85 Vp-p,
S/N Signal-to-Noise Ratio 50 dB
fIN = 20 Hz to 20 kHz
VIN = 4.85 Vp-p
IMD Intermodulation Distortion 50 dB
fIN = 20 Hz to 20 kHz
CVIN Analog Input Capacitance 25 pF
(4) Two on-chip diodes are tied to each analog input and are reversed biased during normal operation. One is connected to V+and the
other is connected to GND. They will become forward biased and conduct when an analog input voltage is equal to or greater than one
diode drop above V+or below GND. Therefore, caution should be exercised when testing with V+= 4.5V. Analog inputs with magnitudes
equal to 5V can cause an input diode to conduct, especially at elevated temperatures. This can create conversion errors for analog
signals near full-scale. The specification allows 50 mV forward bias on either diode; e.g., the output code will be correct as long as the
analog input signal does not exceed the supply voltage by more than 50 mV. Exceeding this range on an unselected channel will corrupt
the reading of a selected channel. An absolute analog input signal voltage range of 0V ≤VIN ≤5V can be achieved by ensuring that the
minimum supply voltage applied to V+is 4.950V over temperature variations, initial tolerance, and loading.
(5) Off-channel leakage current is measured on the on-channel selection.
AC ELECTRICAL CHARACTERISTICS
The following specifications apply for V+= 5V, tr= tf= 10 ns, VREF+ = 5V, VREF−= 0V unless otherwise specified. Boldface
limits apply for TA= TJ= TMIN to TMAX;all other limits TA= TJ= 25°C.
Units
Symbol Parameter Conditions Typical(1) Limit(2) (Limit)
Mode Pin to V+
tWR Write Time 100 100 ns (min)
Figure 2,Figure 3,Figure 4
Read Time (Time from Rising Edge of 350
tRD Mode Pin to V+,Figure 2 350 ns (min)
WR to Falling Edge of RD )
200 250 ns (min)
tRDW RD Width Mode Pin to GND, Figure 5 400 400 ns (max)
WR -RD Mode Conversion Time
tCONV Mode Pin to V+,Figure 2 500 560 ns (max)
(tWR + tRD + tACC1)
tCRD RD Mode Conversion Time Mode Pin to GND, Figure 1 655 900 ns (max)
Access Time (Delay from Falling Edge CL≤100 pF, Mode Pin to GND
tACCO 640 900 ns (max)
of RD to Output Valid) Figure 1
(1) Typicals are at 25°C and represent most likely parametric norm.
(2) Limits are specified to AOQL (Average Output Quality Level).
4Submit Documentation Feedback Copyright © 1999–2013, Texas Instruments Incorporated
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
OBSOLETE
ADC08161
www.ti.com
SNAS075D –JUNE 1999–REVISED APRIL 2013
AC ELECTRICAL CHARACTERISTICS (continued)
The following specifications apply for V+= 5V, tr= tf= 10 ns, VREF+ = 5V, VREF−= 0V unless otherwise specified. Boldface
limits apply for TA= TJ= TMIN to TMAX;all other limits TA= TJ= 25°C.
Units
Symbol Parameter Conditions Typical(1) Limit(2) (Limit)
Mode Pin to V+, tRD ≤tINTL,
Figure 2
Access Time (Delay from Falling Edge
tACC1 of RD to Output Valid) CL= 10 pF 45 ns
CL≤100 pF 50 110 ns (max)
tRD > tINTL,Figure 3 Figure 5
CL≤10 pF 25 ns
Access Time (Delay from Falling Edge
tACC2 of RD to Output Valid) CL= 100 pF 30 55 ns (max)
RL= 3 kΩ, CL= 10 pF Figure 1
TRI-STATE Control (Delay from Rising
t1H, t0H Figure 2 Figure 3 Figure 4 30 60 ns (max)
Edge of RD to HI-Z State) Figure 5
Delay from Rising Edge ofWR to Mode Pin = V+, CL= 50 pF 520
tINTL 690 ns (max)
Falling Edge of INT Figure 3,Figure 4
CL= 50 pF,
Delay from Rising Edge of RD to
tINTH Figure 1,Figure 2,Figure 3 and 50 95 ns (max)
Rising Edge of INT Figure 5
Delay from Rising Edge of WR to
tINTH CL= 50 pF, Figure 4 45 95 ns (max)
Rising Edge of INT
Mode Pin = 0V, CL= 50 pF,
tRDY Delay from CS to RDY 25 45 ns (max)
RL= 3 kΩ,Figure 1
RL= 3 kΩ, CL= 100 pF
tID Delay from INT to Output Valid 0 15 ns (max)
Figure 4
tRI Delay from RD to INT Mode Pin = V+, tRD ≤tINTL 60 115 ns (max)
Figure 2
Time between End of RD and Start of Figure 1,Figure 2,Figure 3,
tN50 50 ns (min)
New Conversion Figure 4 and Figure 5
Figure 1,Figure 2,Figure 3,
tCSS CS Setup Time 0 0ns (max)
Figure 4 and Figure 5
Figure 1,Figure 2,Figure 3,
tCSH CS Hold Time 0 0ns (max)
Figure 4 and Figure 5
DC ELECTRICAL CHARACTERISTICS
The following specifications apply for V+= 5V unless otherwise specified. Boldface limits apply for TA= TJ= TMIN to TMAX;
all other limits TA= TJ= 25°C.
Units
Symbol Parameter Conditions Typical(1) Limit(2) (Limit)
V+= 5.5 V
VIH Logic “1” Input Voltage CS, WR, RD, A0, A1, A2 Pins 2.0 V (min)
Mode Pin 3.5
V+= 4.5V
VIL Logic “0” Input Voltage CS, WR, RD, A0, A1, A2 Pins 0.8 V (max)
Mode Pin 1.5
VH= 5V
CS, RD, A0, A, A2 Pins 0.005 1
IIH Logic “1” Input Current WR Pin 0.1 3μA (max)
Mode Pin 50 200
VL= 0V
IIL Logic “0” Input Current CS, RD, WR, A0, A1, A2 −0.005 −2μA (max)
Mode Pins
(1) Typicals are at 25°C and represent most likely parametric norm.
(2) Limits are specified to AOQL (Average Output Quality Level).
Copyright © 1999–2013, Texas Instruments Incorporated Submit Documentation Feedback 5
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
OBSOLETE
ADC08161
SNAS075D –JUNE 1999–REVISED APRIL 2013
www.ti.com
DC ELECTRICAL CHARACTERISTICS (continued)
The following specifications apply for V+= 5V unless otherwise specified. Boldface limits apply for TA= TJ= TMIN to TMAX;
all other limits TA= TJ= 25°C.
Units
Symbol Parameter Conditions Typical(1) Limit(2) (Limit)
V+= 4.75V
IOUT =−360 μA2.4 V (min)
VOH Logic “1” Output Voltage DB0–DB7, OFL, INT
IOUT =−10 μA4.5 V (min)
DB0–DB7, OFL, INT
V+= 4.75V
VOL Logic “0” Output Voltage IOUT = 1.6 mA 0.4 V (max)
DB0–DB7, OFL, INT, RDY
VOUT = 5.0V 0.1 3μA (max)
DB0–DB7, RDY
IOTRI-STATE Output Current VOUT = 0V −0.1 −3μA (max)
DB0–DB7, RDY
VOUT = 0V
ISOURCE Output Source Current −26 −6mA (min)
DB0–DB7, OFL, INT
VOUT = 5V
ISINK Output Sink Current 24 7mA (min)
DB0–DB7, OFL, INT, RDY
ICSupply Current CS = WR = RD = 0 11.5 20 mA (max)
COUT Logic Output Capacitance 5 pF
CIN Logic Input Capacitance 5 pF
BANDGAP REFERENCE ELECTRICAL CHARACTERISTICS
The following specifications apply for V+= 5V unless otherwise specified. Boldface limits apply for TMIN to TMAX;all other
limits TA= TJ= 25°C.
Symbol Parameter Conditions Typical(1) Limits(2) Units (Limit)
VREFOUT Internal Reference Output Voltage 2.5 ± 2.0% V (max)
Internal Reference Temperature
ΔVREF/ΔT 40 ppm/°C
Coefficient
ΔVREF/ΔILInternal Reference Load Regulation Sourcing (0 ≤IL≤+10 mA) 0.01 0.1 %/mA (max)
Line Regulation 4.75V ≤V+≤5.25V 0.5 6.0 mV (max)
ISC Short Circuit Current VREV = 0V 35 mA (max)
ΔVREF/ΔtLong Term Stability 200 ppm/kHr
Start-Up Time V+: 0V→5V, CL= 220 μF 40 ms
(1) Typicals are at 25°C and represent most likely parametric norm.
(2) Limits are specified to AOQL (Average Output Quality Level).
6Submit Documentation Feedback Copyright © 1999–2013, Texas Instruments Incorporated
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
v.
T v.
7 m
RD 7 Arum“ DAM 00
C5 “ cuwur
3m VDH
ummms
: m
v. v.
, 3w
Rao—
, um
55 Ancaam WW
Damouvms
V m
u,
a was- W7 *1 /—
E
w mm
~> ‘an mm: 7* ‘N
m f \ f
a W ._
w
Dawns?
‘CSS
7 k 7
M '
7 .
N
RD
'm * ‘wTw
neuron -
new» ‘7 ~> <7 w-‘uu="">7>OBSOLETE
ADC08161
www.ti.com
SNAS075D –JUNE 1999–REVISED APRIL 2013
TRI-STATE TEST CIRCUIT AND WAVEFORMS
t1H t1H, CL= 10 pF
tr= 10 ns t0H t0H, CL= 10 pF
Figure 1. RD Mode (Mode Pin is Low)
Figure 2. WR-RD Mode with tRD ≤tINTL (Mode Pin is High)
Copyright © 1999–2013, Texas Instruments Incorporated Submit Documentation Feedback 7
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
‘c’ss
a W W
W»
To
» kuw
WV
WW“-
uaarum
um» <7 »="" *‘w‘hh="" e="" rt:="" ww="" um="" um="" “my="">._.-
A
m
cs t \ I \
‘55: ‘EN
7 ‘m
in \—
naaiw -----
W «w »W
7>OBSOLETE
ADC08161
SNAS075D –JUNE 1999–REVISED APRIL 2013
www.ti.com
Figure 3. WR-RD Mode with tRD > tINTL (Mode Pin is High)
Figure 4. WR-RD Mode Reduced Interface System Connection with CS = RD = 0 (Mode Pin is High)
Figure 5. RD Mode (Pipeline Operation); tRDW must be between 200 ns and 400 ns.
(Mode Pin is Low)
8Submit Documentation Feedback Copyright © 1999–2013, Texas Instruments Incorporated
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
300 0.6
750 I A M \
m
/ fl
‘2: 0.4
a 700 g
E v‘=5.5v E 03
2 >—
: 550 :
V‘:50V 5‘: 0.2
V g
600 V':A.5V 4 0“
550 0
-100 -50 0 50 mo ‘50 0 1 2 3 4 5
AMBIENT TEMPERATURE(°C) REFERENCE VOLTAGEW)
0.5 , ‘5 ‘.
VZSV V:55V
TA=25°C
0.4 A
a < v)="" 5="" d="">7
m 0.3 3,
o m
K m
5 2
o
5 0.2 y
:1 5‘
8 %
0.1 "’ a
0 6
0 1 2 3 4 5 -100 -50 0 50 100 ‘50
REFERENCE VOLIAGEW) IEMPERATURE<°c) 2.515="" .="" v="§V" v="" pm="" 2.5m="" mom="" 2.505="" 2.500="" 2.495="" 2.490="" 2.aas="" -1ao="">50 0 50 100 ‘50
TEMPERATURE (°C)
°c)>OBSOLETE
ADC08161
www.ti.com
SNAS075D –JUNE 1999–REVISED APRIL 2013
TYPICAL PERFORMANCE CHARACTERISTICS
Linearity Error vs
tCRD vs Temperature Reference Voltage
Figure 6. Figure 7.
Offset Error vs
Reference Voltage Supply Current vs Temperature
Figure 8. Figure 9.
Reference Output Voltage vs
Temperature
Figure 10.
Copyright © 1999–2013, Texas Instruments Incorporated Submit Documentation Feedback 9
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
vons (v)
1,5
L4 A
< v'="5.5v" e="" _="" k="" ls="" 5="" m="" %="" l)="" m="" k="" e="" s="" m="" q="" \="" to="" sum:="" 400="" -50="" o="" 50="" mo="" ‘50="" 400="" -50="" 0="" 5a="" i00="" 150="" temperature(°c)="" temperature(°c)="">OBSOLETE
ADC08161
SNAS075D –JUNE 1999–REVISED APRIL 2013
www.ti.com
TYPICAL PERFORMANCE CHARACTERISTICS (continued)
Output Current
Logic Threshold vs vs
Temperature Temperature
Figure 11. Figure 12.
10 Submit Documentation Feedback Copyright © 1999–2013, Texas Instruments Incorporated
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
VRm
mm
mm;
am
me
we
3/‘5
er
DAC
mm
037
ms
COMFARAIOR‘ Mum PLEXER
was
TR‘ -STATE
OUTF‘UI
BUFFER
nu
was
DJ:
Dan
VOLTAGE ESTIMATOR DECUDER
OBSOLETE
ADC08161
www.ti.com
SNAS075D –JUNE 1999–REVISED APRIL 2013
APPLICATION INFORMATION
This product is on Lifetime Buy and NOT recommended for new designs.
Figure 13. Block Diagram of the ADC08161 Multi-Step Flash Architecture
FUNCTIONAL DESCRIPTION
The ADC08161 performs an 8-bit analog-to-digital conversion using a multi-step flash technique. The first flash
generates the five most significant bits (MSBs) and the second flash generates the three least significant bits
(LSBs). Figure 13 shows the major functional blocks of the ADC08161 multi-step flash converter. It consists of an
over-encoded 2½-bit Voltage Estimator, an internal DAC with two different voltage spans, a 3-bit half-flash
converter and a comparator multiplexer.
The resistor string near the center of the block diagram in Figure 13 forms the internal main DAC. Each of the
eight resistors at the bottom of the string is equal to 1/256 of the total string resistance. These resistors form the
LSB Ladder and have a voltage drop of 1/256 of the total reference voltage (VREF+ −VREF−) across them. The
remaining resistors make up the MSB Ladder . They are made up of eight groups of four resistors connected in
series. Each MSB Ladder section has ⅛of the total reference voltage across it. Within a given MSB Ladder
section, each of the MSB resistors has 8/256, or ⅓2 of the total reference voltage across it. Tap points are found
between all of the resistors in both the MSB and LSB Ladders. Through the Comparator Multiplexer these tap
points can be connected, in groups of eight, to the eight comparators shown at the right of Figure 13. This
function provides the necessary reference voltages to the comparators during each flash conversion.
Copyright © 1999–2013, Texas Instruments Incorporated Submit Documentation Feedback 11
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
OBSOLETE
ADC08161
SNAS075D –JUNE 1999–REVISED APRIL 2013
www.ti.com
The six comparators, seven-resistor string (estimator DAC), and Estimator Decoder at the left of Figure 13 form
the Voltage Estimator. The estimator DAC connected between VREF+ and VREF−generates the reference voltages
for the six Voltage Estimator comparators. These comparators perform a very low resolution A/D conversion to
obtain an “estimate” of the input voltage. This estimate is then used to control the Comparator Multiplexer,
connecting the appropriate MSB Ladder section to the eight flash comparators. Only 14 comparators, six in the
Voltage Estimator and eight in the flash converter, are needed to achieve the full eight-bit resolution, instead of
32 comparators that would be needed by traditional half-flash methods.
A conversion begins with the Voltage Estimator comparing the analog input signal against the six tap voltages on
the estimator DAC. The estimator decoder then selects one of the groups of tap points along the MSB Ladder.
These eight tap points are then connected to the eight flash comparators. For example, if the analog input signal
applied to VIN is between 0 and 3/16 of VREF (VREF = VREF+ −VREF−), the estimator decoder instructs the
comparator multiplexer to select the eight tap points between 8/256 and 2/8 of VREF and connects them to the
eight flash comparators. The first flash conversion is now performed, producing the five MSBs of data.
The remaining three LSBs are generated next using the same eight comparators that were used for the first flash
conversion. As determined by the results of the MSB flash, a voltage from the MSB Ladder equivalent to the
magnitude of the five MSBs is subtracted from the analog input voltage as the upper switch is moved from
position one to position two. The resulting remainder voltage is applied to the eight flash comparators and, with
the lower switch in position two, compared with the eight tap points from the LSB Ladder.
By using the same eight comparators for both flash conversions, the number of comparators needed by the
multi-step converter is significantly reduced when compared to standard half-flash techniques.
Voltage Estimator errors as large as 1/16 of VREF(16 LSBs) will be corrected since the flash comparators are
connected to ladder voltages that extend beyond the range specified by the Voltage Estimator. For example, if
7/16 VREF < VIN < 9/16 VREF the Voltage Estimator's comparators tied to the tap points below 9/16 VREF will
output “1”s (000111). This is decoded by the estimator decoder to “10”. The eight flash comparators will be
placed at the MSB Ladder tap points between ⅜VREF and ⅝VREF. The overlap of 1/16 VREF on each side of the
Voltage Estimator's span will automatically correct an error of up to 16 LSBs (16 LSBs = 312.5 mV for VREF =
5V). If the first flash conversion determines that the input voltage is between ⅜VREF and 4/8 VREF −LSB/2, the
Voltage Estimator's output code will be corrected by subtracting “1”. This results in a corrected value of “01”. If
the first flash conversion determines that the input voltage is between 8/16 VREF −LSB/2 and ⅝VREF, the
Voltage Estimator's output code remains unchanged.
After correction, the 2-bit data from both the Voltage Estimator and the first flash conversion are decoded to
produce the five MSBs. Decoding is similar to that of a 5-bit flash converter since there are 32 tap points on the
MSB Ladder. However, 31 comparators are not needed since the Voltage Estimator places the eight
comparators along the MSB Ladder where reference tap voltages are present that fall above and below the
magnitude of VIN. Comparators are not needed outside this selected range. If a comparator's output is a “0”, all
comparators above it will also have outputs of “0” and if a comparator's output is a “1”, all comparators below it
will also have outputs of “1”.
DIGITAL INTERFACE
The ADC08161 has two basic interface modes which are selected by connecting the MODE pin to a logic high or
low.
RD Mode
With a logic low applied to the MODE pin, the converter is set to Read mode. In this configuration (Figure 1), a
complete conversion is done by pulling RD low, and holding low, until the conversion is complete and output data
appears. This typically takes 655 ns. The INT (interrupt) line goes low at the end of conversion. A typical delay of
50 ns is needed between the rising edge of CS (after the end of a conversion) and the start of the next
conversion (by pulling RD low). The RDY output goes low after the falling edge of CS and goes high at the end-
of-conversion. It can be used to signal a processor that the converter is busy or serve as a system Transfer
Acknowledge signal.
12 Submit Documentation Feedback Copyright © 1999–2013, Texas Instruments Incorporated
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
OBSOLETE
ADC08161
www.ti.com
SNAS075D –JUNE 1999–REVISED APRIL 2013
RD Mode Pipelined Operation
Applications that require shorter RD pulse widths than those used in the Read mode as described above can be
achieved by setting RD's width between 200 ns–400 ns (Figure 5). RD pulse widths outside this range will create
conversion linearity errors. These errors are caused by exercising internal interface logic circuitry using CS
and/or RD during a conversion.
When RD goes low, a conversion is initiated and the data from the previous conversion is available on the
DB0–DB7 outputs. Reading DB0–DB7 for the first two times after power-up produces random data. The data will
be valid during the third RD pulse that occurs after the first conversion.
WR-RD (WR then RD ) Mode
The ADC08161 is in the WR-RD mode with the MODE pin tied high. A conversion starts on the rising edge of
the WR signal. There are two options for reading the output data which relate to interface timing. If an interrupt-
driven scheme is desired, the user can wait for the INT output to go low before reading the conversion result
(Figure 3). Typically, INT will go low 690 ns, maximum, after WR's rising edge. However, if a shorter conversion
time is desired, the processor need not wait for INT and can exercise a read after only 350 ns (Figure 2). If RD is
pulled low before INT goes low, INT will immediately go low and data will appear at the outputs. This is the
fastest operating mode (tRD ≤tINTL) with a conversion time, including data access time, of 560 ns. Allowing 100
ns for reading the conversion data and the delay between conversions gives a total throughput time of 660 ns
(throughput rate of 1.5 MHz).
WR-RD Mode with Reduced Interface System Connection
CS and RD can be tied low, using only WR to control the start of conversion for applications that require reduced
digital interface while operating in the WR-RD mode (Figure 4). Data will be valid approximately 705 ns following
WR's rising edge.
REFERENCE INPUTS
The ADC08161's two VREF inputs are fully differential and define the zero to full-scale input range of the A to D
converter. This allows the designer to vary the span of the analog input since this range will be equivalent to the
voltage difference between VREF+and VREF−. Transducers that have outputs that minimum output voltages above
GND can also be compensated by connecting VREF−to a voltage that is equal to this minimum voltage. By
reducing VREF (VREF = VREF+–VREF−) to less than 5V, the sensitivity of the converter can be increased (i.e., if VREF
= 2.5V, then 1 LSB = 9.8 mV). The reference arrangement also facilitates ratiometric operation and in may cases
the power supply can be used for transducer power as well as the VREF source. Ratiometric operation is
achieved by connecting VREF−to GND and connecting VREF+ and a transducer's power supply input to V+. The
ADC08161s accuracy degrades when VREF+–|VREF−| is less than 2.0V.
The voltage at VREF−sets the input level that produces a digital output of all zeroes. Through VIN is not itself
differential, the reference design affords nearly differential-input capability for some measurement applications.
Figure 14 shows one possible differential configuration.
It should be noted that, while the two VREF inputs are fully differential, the digital output will be zero for any
analog input voltage if VREF−≥VREF+.
ANALOG INPUT AND SOURCE IMPEDANCE
The ADC08161's analog input circuitry includes an analog switch with an “on” resistance of 70Ωand a 1.4 pF
capacitor (Figure 14). The switch is closed during the A/D's input signal acquisition time (while WR is low when
using the WR-RD Mode). A small transient current flows into the input pin each time the switch closes. A
transient voltage, whose magnitude can increase as the source impedance increases, may be present at the
input. So long as the source impedance is less than 500Ω, the input voltage transient will not cause errors and
need not be filtered.
Large source impedances can slow the charging of the sampling capacitors and degrade conversion accuracy.
Therefore, only signal sources with output impedances less than 500Ωshould be used if rated accuracy is to be
achieved at the minimum sample time (100 ns maximum). A signal source with a high output impedance should
have its output buffered with an operational amplifier. Any ringing or voltage shifts at the op amp's output during
the sampling period can result in conversion errors.
Copyright © 1999–2013, Texas Instruments Incorporated Submit Documentation Feedback 13
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
mm:
sum:
OBSOLETE
ADC08161
SNAS075D –JUNE 1999–REVISED APRIL 2013
www.ti.com
Some suggested input configurations using the internal 2.5V reference, an external reference, and adjusting the
input span are shown in Figure 15.
Correct conversion results will be obtained for input voltages greater than GND −100 mV and less than V++
100 mV. Do not allow the signal source to drive the analog input pin more than 300 mV higher than V+, or more
than 300 mV lower than GND. The current flowing through any analog input pin should be limited to 5 mA or less
to avoid permanent damage to the IC if an analog input pin is forced beyond these voltages. The sum of all the
overdrive currents into all pins must be less than 20 mA. Some sort of protection scheme should be used when
the input signal is expected to extend more than 300 mV beyond the power supply limits. A simple protection
network using resistors and diodes is shown in Figure 16.
INHERENT SAMPLE-AND-HOLD
An important benefit of the ADC08161's input architecture is the inherent sample-and-hold (S/H) and its ability to
measure relatively high speed signals without the help of an external S/H. In a non-sampling converter,
regardless of its speed, the input must remain stable to at least ½ LSB throughout the conversion process if full
accuracy is to be maintained. Consequently, for many high speed signals, this signal must be externally sampled
and held stationary during the conversion.
The ADC08161 is suitable for DSP-based systems because of the direct control of the S/H through the WR
signal. The WR input signal allows the A/D to be synchronized to a DSP system's sampling rate or to other
ADC08161s.
The ADC08161 can perform accurate conversions of full-scale input signals at frequencies from DC to more than
300 kHz (full power bandwidth) without the need of an external sample-and-hold (S/H).
INTERNAL BANDGAP REFERENCE
The ADC08161 has an internal bandgap 2.5V reference that can be used as the VREF+ input. A parallel
combination of a 0.1 μF ceramic capacitor and a 220 μF tantalum capacitor should be used to bypass the
VREFOUT pin. This reduces possible noise pickup that could cause conversion errors.
LAYOUT, GROUNDS, AND BYPASSING
In order to ensure fast, accurate conversions from the ADC08161, it is necessary to use appropriate circuit board
layout techniques. Ideally, the analog-to-digital converter's ground reference should be low impedance and free
of noise from other parts of the system. Digital circuits can produce a great deal of noise on their ground returns
and, therefore, should have their own separate ground lines. Best performance is obtained using separate
ground planes should be provided for the digital and analog parts of the system.
The analog inputs should be isolated from noisy signal traces to avoid having spurious signals couple to the
input. Any external component (e.g., an input filter capacitor) connected across the inputs should be returned to a
very clean ground point. Incorrectly grounding the ADC08161 may result in reduced conversion accuracy.
The V+supply pin, VREF+, and VREF−(if not grounded) should be bypassed with a parallel combination of a 0.1 μF
ceramic capacitor and a 10 μF tantalum capacitor placed as close as possible to the pins using short circuit
board traces. See Figure 15 and Figure 16.
Figure 14. ADC08161 Equivalent Input Circuit Model
14 Submit Documentation Feedback Copyright © 1999–2013, Texas Instruments Incorporated
Product Folder Links: ADC08161
l hams
INSTRUMENTS
Vw
VREH
<7) vwm="" 0—="" vw="" cm:="" szu="" w="" va="" gnd="" var.="" vnw="" vmow="" *="" :="" aquzzow="" 5v="" va:="" ad008161="" m="" n="" ‘2="" ‘9="" mr»="" ‘="" vn="" 220m="" -="" mm="" i:="" and="" j.="" l="">7)>OBSOLETE
ADC08161
www.ti.com
SNAS075D –JUNE 1999–REVISED APRIL 2013
Internal Reference 2.5V Full-Scale
(Standard Application) Power Supply as Reference Input Not Referred to GND
*Signal source driving VIN(−) must be capable of sinking 5 mA.
Figure 15. Analog Input Options
Note: Bypass capacitors consist of a 0.1 μF ceramic in parallel with a 10 μF bead tantalum, unless otherwise
specified.
Note the multiple bypass capacitors on the reference and power supply pins. VREF−should be bypassed to analog
ground using multiple capacitors if it is not grounded (See section on LAYOUT, GROUNDS, AND BYPASSING). VIN1
is shown with an optional input protection network.
Figure 16. Typical Connection.
Copyright © 1999–2013, Texas Instruments Incorporated Submit Documentation Feedback 15
Product Folder Links: ADC08161
l TEXAS
INSTRUMENTS
OBSOLETE
ADC08161
SNAS075D –JUNE 1999–REVISED APRIL 2013
www.ti.com
REVISION HISTORY
Changes from Revision C (April 2013) to Revision D Page
• Changed layout of National Data Sheet to TI format .......................................................................................................... 14
16 Submit Documentation Feedback Copyright © 1999–2013, Texas Instruments Incorporated
Product Folder Links: ADC08161

IMPORTANT NOTICE
Texas Instruments Incorporated and its subsidiaries (TI) reserve the right to make corrections, enhancements, improvements and other
changes to its semiconductor products and services per JESD46, latest issue, and to discontinue any product or service per JESD48, latest
issue. Buyers should obtain the latest relevant information before placing orders and should verify that such information is current and
complete. All semiconductor products (also referred to herein as “components”) are sold subject to TI’s terms and conditions of sale
supplied at the time of order acknowledgment.
TI warrants performance of its components to the specifications applicable at the time of sale, in accordance with the warranty in TI’s terms
and conditions of sale of semiconductor products. Testing and other quality control techniques are used to the extent TI deems necessary
to support this warranty. Except where mandated by applicable law, testing of all parameters of each component is not necessarily
performed.
TI assumes no liability for applications assistance or the design of Buyers’ products. Buyers are responsible for their products and
applications using TI components. To minimize the risks associated with Buyers’ products and applications, Buyers should provide
adequate design and operating safeguards.
TI does not warrant or represent that any license, either express or implied, is granted under any patent right, copyright, mask work right, or
other intellectual property right relating to any combination, machine, or process in which TI components or services are used. Information
published by TI regarding third-party products or services does not constitute a license to use such products or services or a warranty or
endorsement thereof. Use of such information may require a license from a third party under the patents or other intellectual property of the
third party, or a license from TI under the patents or other intellectual property of TI.
Reproduction of significant portions of TI information in TI data books or data sheets is permissible only if reproduction is without alteration
and is accompanied by all associated warranties, conditions, limitations, and notices. TI is not responsible or liable for such altered
documentation. Information of third parties may be subject to additional restrictions.
Resale of TI components or services with statements different from or beyond the parameters stated by TI for that component or service
voids all express and any implied warranties for the associated TI component or service and is an unfair and deceptive business practice.
TI is not responsible or liable for any such statements.
Buyer acknowledges and agrees that it is solely responsible for compliance with all legal, regulatory and safety-related requirements
concerning its products, and any use of TI components in its applications, notwithstanding any applications-related information or support
that may be provided by TI. Buyer represents and agrees that it has all the necessary expertise to create and implement safeguards which
anticipate dangerous consequences of failures, monitor failures and their consequences, lessen the likelihood of failures that might cause
harm and take appropriate remedial actions. Buyer will fully indemnify TI and its representatives against any damages arising out of the use
of any TI components in safety-critical applications.
In some cases, TI components may be promoted specifically to facilitate safety-related applications. With such components, TI’s goal is to
help enable customers to design and create their own end-product solutions that meet applicable functional safety standards and
requirements. Nonetheless, such components are subject to these terms.
No TI components are authorized for use in FDA Class III (or similar life-critical medical equipment) unless authorized officers of the parties
have executed a special agreement specifically governing such use.
Only those TI components which TI has specifically designated as military grade or “enhanced plastic” are designed and intended for use in
military/aerospace applications or environments. Buyer acknowledges and agrees that any military or aerospace use of TI components
which have not been so designated is solely at the Buyer's risk, and that Buyer is solely responsible for compliance with all legal and
regulatory requirements in connection with such use.
TI has specifically designated certain components as meeting ISO/TS16949 requirements, mainly for automotive use. In any case of use of
non-designated products, TI will not be responsible for any failure to meet ISO/TS16949.
Products Applications
Audio www.ti.com/audio Automotive and Transportation www.ti.com/automotive
Amplifiers amplifier.ti.com Communications and Telecom www.ti.com/communications
Data Converters dataconverter.ti.com Computers and Peripherals www.ti.com/computers
DLP® Products www.dlp.com Consumer Electronics www.ti.com/consumer-apps
DSP dsp.ti.com Energy and Lighting www.ti.com/energy
Clocks and Timers www.ti.com/clocks Industrial www.ti.com/industrial
Interface interface.ti.com Medical www.ti.com/medical
Logic logic.ti.com Security www.ti.com/security
Power Mgmt power.ti.com Space, Avionics and Defense www.ti.com/space-avionics-defense
Microcontrollers microcontroller.ti.com Video and Imaging www.ti.com/video
RFID www.ti-rfid.com
OMAP Applications Processors www.ti.com/omap TI E2E Community e2e.ti.com
Wireless Connectivity www.ti.com/wirelessconnectivity
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2013, Texas Instruments Incorporated
Products related to this Datasheet
IC ADC 8BIT SIGMA-DELTA 20SOIC