founded by Phlhps
1. General description
The PCA9633 is an I2C-bus controlled 4-bit LED driver optimized for
Red/Green/Blue/Amber (RGBA) color mixing applications. Each LED output has its own
8-bit resolution (256 steps) fixed frequency Individual PWM controller that operates at
97 kHz with a duty cycle that is adjustable from 0 % to 99.6 % to allow the LED to be set
to a specific brightness value. A fifth 8-bit resolution (256 steps) Group PWM controller
has both a fixed frequency of 190 Hz and an adjustable frequency between 24 Hz to once
every 10.73 seconds with a duty cycle that is adjustable from 0 % to 99.6 % that is used to
either dim or blink all LEDs with the same value.
Each LED output can be off, on (no PWM control), set at its Individual PWM controller
value or at both Individual and Group PWM controller values. The LED output driver is
programmed to be either open-drain with a 25 mA current sink capability at 5 V or totem
pole with a 25 mA sink, 10 mA source capability at 5 V. The PCA9633 operates with a
supply voltage range of 2.3 V to 5.5 V and the outputs are 5.5 V tolerant. LEDs can be
directly connected to the LED output (up to 25 mA, 5.5 V) or controlled with external
drivers and a minimum amount of discrete components for larger current or higher voltage
LEDs.
The PCA9633 is one of the first LED controller devices in a new Fast-mode Plus (Fm+)
family. Fm+ devices offer higher frequency (up to 1 MHz) and more densely populated bus
operation (up to 4000 pF).
The active LOW Output Enable input pin (OE) allows asynchronous control of the LED
outputs and can be used to set all the outputs to a defined I2C-bus programmable logic
state. The OE can also be used to externally PWM the outputs, which is useful when
multiple devices need to be dimmed or blinked together using software control. This
feature is available for the 16-pin version only.
Software programmable LED Group and three Sub Call I2C addresses allow all or defined
groups of PCA9633 devices to respond to a common I2C address, allowing for example,
all red LEDs to be turned on or off at the same time or marquee chasing effect, thus
minimizing I2C-bus commands.
The PCA9633 is offered with 3 different I2C-bus address options: fixed I2C-bus address
(8-pin version), 4 different I2C-bus addresses from 2 programmable address pins (10-pin
version), and 126 different I2C-bus addresses from 7 programmable address pins (16-pin
version). They are software identical except for the different number of address
combinations.
The Software Reset (SWRST) Call allows the master to perform a reset of the PCA9633
through the I2C-bus, identical to the Power-On Reset (POR) that initializes the registers to
their default state causing the outputs to be set HIGH (LED off). This allows an easy and
quick way to reconfigure all device registers to the same condition.
PCA9633
4-bit Fm+ I2C-bus LED driver
Rev. 05 — 25 July 2008 Product data sheet

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 2 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
2. Features
n4 LED drivers. Each output programmable at:
uOff
uOn
uProgrammable LED brightness
uProgrammable group dimming/blinking mixed with individual LED brightness
n1 MHz Fast-mode Plus I2C-bus interface with 30 mA high drive capability on SDA
output for driving high capacitive buses
n256-step (8-bit) linear programmable brightness per LED output varying from fully off
(default) to maximum brightness using a 97 kHz PWM signal
n256-step group brightness control allows general dimming (using a 190 Hz PWM
signal) from fully off to maximum brightness (default)
n256-step group blinking with frequency programmable from 24 Hz to 10.73 s and
duty cycle from 0 % to 99.6 %
nFour totem pole outputs (sink 25 mA and source 10 mA at 5 V) with software
programmable open-drain LED outputs selection (default at totem pole). No input
function.
nOutput state change programmable on the Acknowledge or the STOP Command to
update outputs byte-by-byte or all at the same time (default to ‘Change on STOP’).
nActive LOW Output Enable (OE) input pin. LED outputs programmable to ‘1’, ‘0’ or
‘high-impedance’ (default at power-up) when OE is HIGH, thus allowing hardware
blinking and dimming of the LEDs (16-pin version only).
n2 hardware address pins (10-pin version) and 7 hardware address pins (16-pin
version) allow respectively up to 4 and 126 devices to be connected to the same
I2C-bus. No hardware address pins in the 8-pin version.
n4 software programmable I2C-bus addresses (one LED Group Call address and three
LED Sub Call addresses) allow groups of devices to be addressed at the same time in
any combination (for example, one register used for ‘All Call’ so that all the PCA9633s
on the I2C-bus can be addressed at the same time and the second register used for
three different addresses so that 1⁄3 of all devices on the bus can be addressed at the
same time in a group). Software enable and disable for I2C-bus address.
nSoftware Reset feature (SWRST Call) allows the device to be reset through the
I2C-bus
n25 MHz internal oscillator requires no external components
nInternal power-on reset
nNoise filter on SDA/SCL inputs
nEdge rate control on outputs
nNo glitch on power-up
nSupports hot insertion
nLow standby current
nOperating power supply voltage range of 2.3 V to 5.5 V
n5.5 V tolerant inputs
n−40 °C to +85 °C operation
nESD protection exceeds 2000 V HBM per JESD22-A114, 200 V MM per
JESD22-A115, and 1000 V CDM per JESD22-C101
nLatch-up testing is done to JEDEC Standard JESD78 which exceeds 100 mA

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 3 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
nPackages offered: SO, TSSOP (MSOP), HVQFN, HVSON
3. Applications
nRGB or RGBA LED drivers
nLED status information
nLED displays
nLCD backlights
nKeypad backlights for cellular phones or handheld devices
4. Ordering information
Table 1. Ordering information
Type number Topside
mark Package
Name Description Version
PCA9633D16 PCA9633 SO16 plastic small outline package; 16 leads; body width 3.9 mm SOT109-1
PCA9633DP1 9633 TSSOP8 plastic thin shrink small outline package; 8 leads;
body width 3 mm SOT505-1
PCA9633DP2 9633 TSSOP10 plastic thin shrink small outline package; 10 leads;
body width 3 mm SOT552-1
PCA9633PW PCA9633 TSSOP16 plastic thin shrink small outline package; 16 leads;
body width 4.4 mm SOT403-1
PCA9633BS 9633 HVQFN16 plastic thermal enhanced very thin quad flat package; no leads;
16 terminals; body 4 ×4×0.85 mm SOT629-1
PCA9633TK 9633 HVSON8 plastic thermal enhanced very thin small outline package;
no leads; 8 terminals; body 3 ×3×0.85 mm SOT908-1
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 4 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
5. Block diagram
Fig 1. Block diagram of PCA9633
A0 A1 A2 A3 A4 A5 A6
16-pin version
002aab283
10-pin version
I2C-BUS
CONTROL
INPUT FILTER
PCA9633
POWER-ON
RESET
SCL
SDA
VDD
VSS LED
STATE
SELECT
REGISTER
PWM
REGISTER X
BRIGHTNESS
CONTROL
GRPFREQ
REGISTER GRPPWM
REGISTER
MUX/
CONTROL
OE
(16-pin
version
only)
'0' – permanently OFF
'1' – permanently ON
VDD
LEDn
190 Hz
24.3 kHz
97 kHz
25 MHz
OSCILLATOR
, chLC c
3§33 33333333
0
fiEEE :::::::: 3333
3
3:33:33:
:33: cccc
U H
U H
U fl
0 U m
EEC: O 3333
EEEEEEEE
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 5 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
6. Pinning information
6.1 Pinning
Fig 2. Pin configuration for TSSOP8 Fig 3. Pin configuration for TSSOP10
Fig 4. Pin configuration for TSSOP16 Fig 5. Pin configuration for SO16
Fig 6. Pin configuration for HVQFN16 Fig 7. Pin configuration for HVSON8
PCA9633DP1
LED0 VDD
LED1 SDA
LED2 SCL
LED3 VSS
002aab314
1
2
3
4
6
5
8
7PCA9633DP2
LED0 VDD
LED1 SDA
LED2 SCL
LED3 A1
A0 VSS
002aab315
1
2
3
4
56
8
7
10
9
PCA9633PW
002aab316
1
2
3
4
5
6
7
8
10
9
12
11
14
13
16
15
A0 VDD
A1 A6
LED0 A5
LED1 SDA
LED2 SCL
LED3 A4
A2 OE
A3 VSS
A0 VDD
A1 A6
LED0 A5
LED1 SDA
LED2 SCL
LED3 A4
A2 OE
A3 VSS
002aab313
1
2
3
4
5
6
7
8
10
9
12
11
14
13
16
15
PCA9633D16
002aab317
Transparent top view
LED3 A4
LED2 SCL
LED1 SDA
LED0 A5
A2
A3
VSS
OE
A1
A0
VDD
A6
4 9
3 10
2 11
1 12
5
6
7
8
16
15
14
13
terminal 1
index area
PCA9633BS
002aab807
PCA9633TK
VSS
LED2
LED3
SCL
LED1 SDA
LED0 VDD
Transparent top view
45
3 6
2 7
1 8
terminal 1
index area

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 6 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
6.2 Pin description
Table 2. Pin description for TSSOP8 and HVSON8
Symbol Pin Type Description
LED0 1 O LED driver 0
LED1 2 O LED driver 1
LED2 3 O LED driver 2
LED3 4 O LED driver 3
VSS 5 power supply supply ground
SCL 6 I serial clock line
SDA 7 I/O serial data line
VDD 8 power supply supply voltage
Table 3. Pin description for TSSOP10
Symbol Pin Type Description
LED0 1 O LED driver 0
LED1 2 O LED driver 1
LED2 3 O LED driver 2
LED3 4 O LED driver 3
A0 5 I address input 0
VSS 6 power supply supply ground
A1 7 I address input 1
SCL 8 I serial clock line
SDA 9 I/O serial data line
VDD 10 power supply supply voltage

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 7 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
[1] HVQFN16 package die supply ground is connected to both the VSS pin and the exposed center pad. The
VSS pin must be connected to supply ground for proper device operation. For enhanced thermal, electrical,
and board-level performance, the exposed pad needs to be soldered to the board using a corresponding
thermal pad on the board, and for proper heat conduction through the board thermal vias need to be
incorporated in the PCB in the thermal pad region.
Table 4. Pin description for SO16 and TSSOP16
Symbol Pin Type Description
A0 1 I address input 0
A1 2 I address input 1
LED0 3 O LED driver 0
LED1 4 O LED driver 1
LED2 5 O LED driver 2
LED3 6 O LED driver 3
A2 7 I address input 2
A3 8 I address input 3
VSS 9 power supply supply ground
OE 10 I active LOW Output Enable
A4 11 I address input 4
SCL 12 I serial clock line
SDA 13 I/O serial data line
A5 14 I address input 5
A6 15 I address input 6
VDD 16 power supply supply voltage
Table 5. Pin description for HVQFN16
Symbol Pin Type Description
LED0 1 O LED driver 0
LED1 2 O LED driver 1
LED2 3 O LED driver 2
LED3 4 O LED driver 3
A2 5 I address input 2
A3 6 I address input 3
VSS[1] 7 power supply supply ground
OE 8 I active LOW Output Enable
A4 9 I address input 4
SCL 10 I serial clock line
SDA 11 I/O serial data line
A5 12 I address input 5
A6 13 I address input 6
VDD 14 power supply supply voltage
A0 15 I address input 0
A1 16 I address input 1

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 8 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
7. Functional description
Refer to Figure 1 “Block diagram of PCA9633”.
7.1 Device addresses
Following a START condition, the bus master must output the address of the slave it is
accessing.
There are a maximum of 128 possible programmable addresses using the 7 hardware
address pins. Two of these addresses, Software Reset and LED All Call, cannot be used
because their default power-up state is ON, leaving a maximum of 126 addresses. Using
other reserved addresses, as well as any other subcall address, will reduce the total
number of possible addresses even further.
7.1.1 Regular I2C-bus slave address
The I2C-bus slave address of the PCA9633 is shown in Figure 8. To conserve power, no
internal pull-up resistors are incorporated on the hardware selectable address pins and
they must be pulled HIGH or LOW (10-pin and 16-pin versions).
Remark: Using reserved I2C-bus addresses will interfere with other devices, but only if the
devices are on the bus and/or the bus will be open to other I2C-bus systems at some later
date. In a closed system where the designer controls the address assignment these
addresses can be used since the PCA9633 treats them like any other address. The
LED All Call, Software Reset and PCA9564 or PCA9665 slave address (if on the bus) can
never be used for individual device addresses.
•PCA9633 LED All Call address (1110 000) and Software Reset (0000 0110) which
are active on start-up
•PCA9564 (0000 000) or PCA9665 (1110 000) slave address which is active on
start-up
•‘reserved for future use’ I2C-bus addresses (0000 011, 1111 1XX)
•slave devices that use the 10-bit addressing scheme (1111 0XX)
•slave devices that are designed to respond to the General Call address (0000 000)
•High-speed mode (Hs-mode) master code (0000 1XX).
The last bit of the address byte defines the operation to be performed. When set to logic 1
a read is selected, while a logic 0 selects a write operation.
a. 8-pin version b. 10-pin version c. 16-pin version
Fig 8. Slave address
R/W
002aab318
1100010
fixed
slave address R/W
002aab295
1 1 0 0 0 A1 A0
fixed hardware
selectable
slave address
R/W
002aab319
A6 A5 A4 A3 A2 A1 A0
hardware selectable
slave address

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 9 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
7.1.2 LED All Call I2C-bus address
•Default power-up value (ALLCALLADR register): E0h or 1110 000X
•Programmable through I2C-bus (volatile programming)
•At power-up, LED All Call I2C-bus address is enabled. PCA9633 sends an ACK when
E0h (R/W = 0) or E1h (R/W = 1) is sent by the master.
See Section 7.3.8 “LED All Call I2C-bus address, ALLCALLADR” for more detail.
Remark: The default LED All Call I2C-bus address (E0h or 1110 000X) must not be used
as a regular I2C-bus slave address since this address is enabled at power-up. All the
PCA9633s on the I2C-bus will acknowledge the address if sent by the I2C-bus master.
7.1.3 LED Sub Call I2C-bus addresses
•3 different I2C-bus addresses can be used
•Default power-up values:
–SUBADR1 register: E2h or 1110 001X
–SUBADR2 register: E4h or 1110 010X
–SUBADR3 register: E8h or 1110 100X
•Programmable through I2C-bus (volatile programming)
•At power-up, Sub Call I2C-bus addresses are disabled. PCA9633 does not send an
ACK when E2h (R/W = 0) or E3h (R/W = 1), E4h (R/W = 0) or E5h (R/W = 1), or
E8h (R/W = 0) or E9h (R/W = 1) is sent by the master.
See Section 7.3.7 “I2C-bus subaddress 1 to 3, SUBADRx” for more detail.
Remark: The default LED Sub Call I2C-bus addresses may be used as regular I2C-bus
slave addresses as long as they are disabled.
7.1.4 Software Reset I2C-bus address
The address shown in Figure 9 is used when a reset of the PCA9633 needs to be
performed by the master. The Software Reset address (SWRST Call) must be used with
R/W = 0. If R/W = 1, the PCA9633 does not acknowledge the SWRST. See Section 7.6
“Software Reset” for more detail.
Remark: The Software Reset I2C-bus address is a reserved address and cannot be used
as a regular I2C-bus slave address (16-pin version) or as an LED All Call or LED Sub Call
address.
Fig 9. Software Reset address
0
002aab416
0000011
R/W

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 10 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
7.2 Control register
Following the successful acknowledgement of the slave address, LED All Call address or
LED Sub Call address, the bus master will send a byte to the PCA9633, which will be
stored in the Control register.
The lowest 4 bits are used as a pointer to determine which register will be accessed
(D[3:0]). The highest 3 bits are used as Auto-Increment flag and Auto-Increment options
(AI[2:0]). Bit 4 is unused and must be programmed with zero (0) for proper device
operation.
When the Auto-Increment flag is set (AI2 = 1), the four low order bits of the Control
register are automatically incremented after a read or write. This allows the user to
program the registers sequentially. Four different types of Auto-Increment are possible,
depending on AI1 and AI0 values.
Remark: Other combinations not shown in Table 6 (AI[2:0] = 001, 010, and 011) are
reserved and must not be used for proper device operation.
AI[2:0] = 000 is used when the same register must be accessed several times during a
single I2C-bus communication, for example, changes the brightness of a single LED. Data
is overwritten each time the register is accessed during a write operation.
AI[2:0] = 100 is used when all the registers must be sequentially accessed, for example,
power-up programming.
AI[2:0] = 101 is used when the four LED drivers must be individually programmed with
different values during the same I2C-bus communication, for example, changing color
setting to another color setting.
reset state = 80h
Remark: The Control register does not apply to the Software Reset I2C-bus address.
Fig 10. Control register
Table 6. Auto-Increment options
AI2 AI1 AI0 Function
0 0 0 no Auto-Increment
1 0 0 Auto-Increment for all registers. D3, D2, D1, D0 roll over to ‘0000’ after
the last register (1100) is accessed.
1 0 1 Auto-Increment for individual brightness registers only. D3, D2, D1, D0
roll over to ‘0010’ after the last register (0101) is accessed.
1 1 0 Auto-Increment for global control registers only. D3, D2, D1, D0 roll over
to ‘0110’ after the last register (0111) is accessed.
1 1 1 Auto-Increment for individual and global control registers only. D3, D2,
D1, D0 roll over to ‘0010’ after the last register (0111) is accessed.
002aab296
AI2 AI1 AI0 0 D3 D2 D1 D0
Auto-Increment flag
register address
Auto-Increment options
Tb
Tb
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 11 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
AI[2:0] = 110 is used when the LED drivers must be globally programmed with different
settings during the same I2C-bus communication, for example, global brightness or
blinking change.
AI[2:0] = 111 is used when individual and global changes must be performed during the
same I2C-bus communication, for example, changing a color and global brightness at the
same time.
Only the 4 least significant bits D[3:0] are affected by the AI[2:0] bits.
When the Control register is written, the register entry point determined by D[3:0] is the
first register that will be addressed (read or write operation), and can be anywhere
between 0000 and 1100 (as defined in Table 7). When AI[2] = 1, the Auto-Increment flag
is set and the rollover value at which the point where the register increment stops and
goes to the next one is determined by AI[2:0]. See Table 6 for rollover values. For
example, if the Control register = 1110 1000 (E8h), then the register addressing sequence
will be (in hex):
08 →…→0C →00 →…→07 →02 →…→07 →02 →…→07 →02 →… as long
as the master keeps sending or reading data.
7.3 Register definitions
[1] Only D[3:0] = 0000 to 1100 are allowed and will be acknowledged. D[3:0] = 1101, 1110, or 1111 are reserved and will not be
acknowledged.
[2] When writing to the Control register, bit 4 must be programmed with logic 0 for proper device operation.
Table 7. Register summary[1][2]
Register number (hex) D3 D2 D1 D0 Name Type Function
00h 0 0 0 0 MODE1 read/write Mode register 1
01h 0 0 0 1 MODE2 read/write Mode register 2
02h 0 0 1 0 PWM0 read/write brightness control LED0
03h 0 0 1 1 PWM1 read/write brightness control LED1
04h 0 1 0 0 PWM2 read/write brightness control LED2
05h 0 1 0 1 PWM3 read/write brightness control LED3
06h 0 1 1 0 GRPPWM read/write group duty cycle control
07h 0 1 1 1 GRPFREQ read/write group frequency
08h 1 0 0 0 LEDOUT read/write LED output state
09h 1 0 0 1 SUBADR1 read/write I2C-bus subaddress 1
0Ah 1 0 1 0 SUBADR2 read/write I2C-bus subaddress 2
0Bh 1 0 1 1 SUBADR3 read/write I2C-bus subaddress 3
0Ch 1 1 0 0 ALLCALLADR read/write LED All Call I2C-bus address
VRT,
RV,
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 12 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
7.3.1 Mode register 1, MODE1
[1] It takes 500 µs max. for the oscillator to be up and running once SLEEP bit has been set to logic 0. Timings on LEDn outputs are not
guaranteed if PWMx, GRPPWM or GRPFREQ registers are accessed within the 500 µs window.
[2] When the oscillator is off (Sleep mode) the LED outputs cannot be turned on, off or dimmed/blinked.
7.3.2 Mode register 2, MODE2
Table 8. MODE1 - Mode register 1 (address 00h) bit description
Legend: * default value.
Bit Symbol Access Value Description
7 AI2 read only 0 Register Auto-Increment disabled
1* Register Auto-Increment enabled
6 AI1 read only 0* Auto-Increment bit1=0
1 Auto-Increment bit1=1
5 AI0 read only 0* Auto-Increment bit0=0
1 Auto-Increment bit0=1
4 SLEEP R/W 0 Normal mode[1].
1* Low power mode. Oscillator off[2].
3 SUB1 R/W 0* PCA9633 does not respond to I2C-bus subaddress 1.
1 PCA9633 responds to I2C-bus subaddress 1.
2 SUB2 R/W 0* PCA9633 does not respond to I2C-bus subaddress 2.
1 PCA9633 responds to I2C-bus subaddress 2.
1 SUB3 R/W 0* PCA9633 does not respond to I2C-bus subaddress 3.
1 PCA9633 responds to I2C-bus subaddress 3.
0 ALLCALL R/W 0 PCA9633 does not respond to LED All Call I2C-bus address.
1* PCA9633 responds to LED All Call I2C-bus address.
Table 9. MODE2 - Mode register 2 (address 01h) bit description
Legend: * default value.
Bit Symbol Access Value Description
7 - read only 0* reserved
6 - read only 0* reserved
5 DMBLNK R/W 0* Group control = dimming
1 Group control = blinking
4 INVRT[1] R/W 0* Output logic state not inverted. Value to use when no external driver used.
Applicable when OE = 0 for PCA9633 16-pin version.
1 Output logic state inverted. Value to use when external driver used.
Applicable when OE = 0 for PCA9633 16-pin version.
3 OCH R/W 0* Outputs change on STOP command.[2]
1 Outputs change on ACK.
2 OUTDRV[1] R/W 0 The 4 LED outputs are configured with an open-drain structure.
1* The 4 LED outputs are configured with a totem pole structure.

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 13 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
[1] See Section 7.7 “Using the PCA9633 with and without external drivers” for more details. Normal LEDs can be driven directly in either
mode. Some newer LEDs include integrated Zener diodes to limit voltage transients, reduce EMI and protect the LEDs, and these must
be driven only in the open-drain mode to prevent overheating the IC.
[2] Change of the outputs at the STOP command allows synchronizing outputs of more than one PCA9633. Applicable to registers from
02h (PWM0) to 08h (LEDOUT) only.
[3] See Section 7.4 “Active LOW output enable input” for more details.
[4] OUTNE[1:0] is only for PCA9633 16-pin version.
7.3.3 PWM registers 0 to 3, PWMx — Individual brightness control registers
A 97 kHz fixed frequency signal is used for each output. Duty cycle is controlled through
256 linear steps from 00h (0 % duty cycle = LED output off) to FFh
(99.6 % duty cycle = LED output at maximum brightness). Applicable to LED outputs
programmed with LDRx = 10 or 11 (LEDOUT register).
(1)
7.3.4 Group duty cycle control, GRPPWM
When DMBLNK bit (MODE2 register) is programmed with 0, a 190 Hz fixed frequency
signal is superimposed with the 97 kHz individual brightness control signal. GRPPWM is
then used as a global brightness control allowing the LED outputs to be dimmed with the
same value. The value in GRPFREQ is then a ‘Don’t care’.
General brightness for the 4 outputs is controlled through 256 linear steps from 00h
(0 % duty cycle = LED output off) to FFh (99.6 % duty cycle = maximum brightness).
Applicable to LED outputs programmed with LDRx = 11 (LEDOUT register).
1 to 0 OUTNE[1:0]
[3][4] R/W 00 When OE = 1 (output drivers not enabled), LEDn = 0.
01* When OE = 1 (output drivers not enabled):
LEDn = 1 when OUTDRV = 1
LEDn = high-impedance when OUTDRV = 0 (same as OUTNE[1:0] = 10)
10 When OE = 1 (output drivers not enabled), LEDn = high-impedance.
11 reserved
Table 9. MODE2 - Mode register 2 (address 01h) bit description
…continued
Legend: * default value.
Bit Symbol Access Value Description
Table 10. PWM0 to PWM3 - PWM registers 0 to 3 (address 02h to 05h) bit description
Legend: * default value.
Address Register Bit Symbol Access Value Description
02h PWM0 7:0 IDC0[7:0] R/W 0000 0000* PWM0 Individual Duty Cycle
03h PWM1 7:0 IDC1[7:0] R/W 0000 0000* PWM1 Individual Duty Cycle
04h PWM2 7:0 IDC2[7:0] R/W 0000 0000* PWM2 Individual Duty Cycle
05h PWM3 7:0 IDC3[7:0] R/W 0000 0000* PWM3 Individual Duty Cycle
duty cycle IDC 7:0[]
256
------------------------
=
Table 11. GRPPWM - Group duty cycle control register (address 06h) bit description
Legend: * default value.
Address Register Bit Symbol Access Value Description
06h GRPPWM 7:0 GDC[7:0] R/W 1111 1111 GRPPWM register

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 14 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
When DMBLNK bit is programmed with 1, GRPPWM and GRPFREQ registers define a
global blinking pattern, where GRPFREQ contains the blinking period (from 24 Hz to
10.73 s) and GRPPWM the duty cycle (ON/OFF ratio in %).
(2)
7.3.5 Group frequency, GRPFREQ
GRPFREQ is used to program the global blinking period when DMBLNK bit (MODE2
register) is equal to 1. Value in this register is a ‘Don’t care’ when DMBLNK = 0.
Applicable to LED outputs programmed with LDRx = 11 (LEDOUT register).
Blinking period is controlled through 256 linear steps from 00h (41 ms, frequency 24 Hz)
to FFh (10.73 s).
(3)
7.3.6 LED driver output state, LEDOUT
LDRx = 00 — LED driver x is off (default power-up state).
LDRx = 01 — LED driver x is fully on (individual brightness and group dimming/blinking
not controlled).
LDRx = 10 — LED driver x individual brightness can be controlled through its PWMx
register.
LDRx = 11 — LED driver x individual brightness and group dimming/blinking can be
controlled through its PWMx register and the GRPPWM registers.
duty cycle GDC 7:0[]
256
---------------------------
=
Table 12. GRPFREQ - Group Frequency register (address 07h) bit description
Legend: * default value.
Address Register Bit Symbol Access Value Description
07h GRPFREQ 7:0 GFRQ[7:0] R/W 0000 0000* GRPFREQ register
global blinking period GFRQ 7:0[]1+
24
----------------------------------------in ondssec()=
Table 13. LEDOUT - LED driver output state register (address 08h) bit description
Legend: * default value.
Address Register Bit Symbol Access Value Description
08h LEDOUT 7:6 LDR3 R/W 00* LED3 output state control
5:4 LDR2 R/W 00* LED2 output state control
3:2 LDR1 R/W 00* LED1 output state control
1:0 LDR0 R/W 00* LED0 output state control

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 15 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
7.3.7 I2C-bus subaddress 1 to 3, SUBADRx
Subaddresses are programmable through the I2C-bus. Default power-up values are E2h,
E4h, E8h, and the device(s) will not acknowledge these addresses right after power-up
(the corresponding SUBx bit in MODE1 register is equal to 0).
Once subaddresses have been programmed to their right values, SUBx bits need to be
set to 1 in order to have the device acknowledging these addresses (MODE1 register).
Only the 7 MSBs representing the I2C-bus subaddress are valid. The LSB in SUBADRx
register is a read-only bit (0).
When SUBx is set to 1, the corresponding I2C-bus subaddress can be used during either
an I2C-bus read or write sequence.
7.3.8 LED All Call I2C-bus address, ALLCALLADR
The LED All Call I2C-bus address allows all the PCA9633s in the bus to be programmed
at the same time (ALLCALL bit in register MODE1 must be equal to 1, power-up default
state). This address is programmable through the I2C-bus and can be used during either
an I2C-bus read or write sequence. The register address can be programmed as a
sub call.
Only the 7 MSBs representing the All Call I2C-bus address are valid. The LSB in
ALLCALLADR register is a Read-only bit (0).
If ALLCALL bit = 0, the device does not acknowledge the address programmed in register
ALLCALLADR.
Table 14. SUBADR1 to SUBADR3 - I2C-bus subaddress registers 0 to 3 (address 09h to
0Bh) bit description
Legend: * default value.
Address Register Bit Symbol Access Value Description
09h SUBADR1 7:1 A1[7:1] R/W 1110 001* I2C-bus subaddress 1
0 A1[0] R only 0* reserved
0Ah SUBADR2 7:1 A2[7:1] R/W 1110 010* I2C-bus subaddress 2
0 A2[0] R only 0* reserved
0Bh SUBADR3 7:1 A3[7:1] R/W 1110 100* I2C-bus subaddress 3
0 A3[0] R only 0* reserved
Table 15. ALLCALLADR - LED All Call I2C-bus address register (address 0Ch) bit
description
Legend: * default value.
Address Register Bit Symbol Access Value Description
0Ch ALLCALLADR 7:1 AC[7:1] R/W 1110 000* ALLCALL I2C-bus
address register
0 AC[0] R only 0* reserved

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 16 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
7.4 Active LOW output enable input
The active LOW output enable (OE) pin, allows to enable or disable all the LED outputs at
the same time.
This control signal is only available for the 16-pin version and does not apply to the 8-pin
or 10-pin versions.
•When a LOW level is applied to OE pin, all the LED outputs are enabled and follow the
output state defined in the LEDOUT register with the polarity defined by INVRT bit
(MODE2 register).
•When a HIGH level is applied to OE pin, all the LED outputs are programmed to the
value that is defined by OUTNE[1:0] in the MODE2 register.
The OE pin can be used as a synchronization signal to switch on/off several PCA9633
devices at the same time. This requires an external clock reference that provides blinking
period and the duty cycle.
The OE pin can also be used as an external dimming control signal. The frequency of the
external clock must be high enough not to be seen by the human eye, and the duty cycle
value determines the brightness of the LEDs.
Remark: Do not use OE as an external blinking control signal when internal global
blinking is selected (DMBLNK = 1, MODE2 register) since it will result in an undefined
blinking pattern. Do not use OE as an external dimming control signal when internal global
dimming is selected (DMBLNK = 0, MODE2 register) since it will result in an undefined
dimming pattern.
7.5 Power-on reset
When power is applied to VDD, an internal Power-on reset holds the PCA9633 in a reset
condition until VDD has reached VPOR. At this point, the reset condition is released and the
PCA9633 registers and I2C-bus state machine are initialized to their default states (all
zeroes) causing all the channels to be deselected. Thereafter, VDD must be lowered below
0.2 V to reset the device.
Table 16. LED outputs when OE=1
OUTNE1 OUTNE0 LED outputs
000
0 1 1 if OUTDRV = 1, high-impedance if OUTDRV = 0
1 0 high-impedance
1 1 reserved

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 17 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
7.6 Software Reset
The Software Reset Call (SWRST Call) allows all the devices in the I2C-bus to be reset to
the power-up state value through a specific formatted I2C-bus command. To be performed
correctly, it implies that the I2C-bus is functional and that there is no device hanging the
bus.
The SWRST Call function is defined as the following:
1. A START command is sent by the I2C-bus master.
2. The reserved SWRST I2C-bus address ‘0000 011’ with the R/W bit set to 0 (write) is
sent by the I2C-bus master.
3. The PCA9633 device(s) acknowledge(s) after seeing the SWRST Call address
‘0000 0110’ (06h) only. If the R/W bit is set to 1 (read), no acknowledge is returned to
the I2C-bus master.
4. Once the SWRST Call address has been sent and acknowledged, the master sends
2 bytes with 2 specific values (SWRST data byte 1 and byte 2):
a. Byte 1 = A5h: the PCA9633 acknowledges this value only. If byte 1 is not equal to
A5h, the PCA9633 does not acknowledge it.
b. Byte 2 = 5Ah: the PCA9633 acknowledges this value only. If byte 2 is not equal to
5Ah, then the PCA9633 does not acknowledge it.
If more than 2 bytes of data are sent, the PCA9633 does not acknowledge any more.
5. Once the right 2 bytes (SWRST data byte 1 and byte 2 only) have been sent and
correctly acknowledged, the master sends a STOP command to end the SWRST Call:
the PCA9633 then resets to the default value (power-up value) and is ready to be
addressed again within the specified bus free time (tBUF).
The I2C-bus master must interpret a non-acknowledge from the PCA9633 (at any time) as
a ‘SWRST Call Abort’. The PCA9633 does not initiate a reset of its registers. This
happens only when the format of the SWRST Call sequence is not correct.

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 18 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
7.7 Using the PCA9633 with and without external drivers
The PCA9633 LED output drivers are 5.5 V only tolerant and can sink up to 25 mA at 5 V.
If the device needs to drive LEDs to a higher voltage and/or higher current, use of an
external driver is required.
•INVRT bit (MODE2 register) can be used to keep the LED PWM control firmware the
same (PWMx and GRPPWM values directly calculated from their respective formulas
and the LED output state determined by LEDOUT register value) independently of the
type of external driver. This bit allows LED output polarity inversion/non-inversion only
when OE=0.
•OUTDRV bit (MODE2 register) allows minimizing the amount of external components
required to control the external driver (N-type or P-type device).
[1] OE applies to 16-pin version only. When OE = 1, LED output state is controlled only by OUTNE[1:0] bits (MODE2 register).
[2] Correct configuration when LEDs directly connected to the LEDn outputs (connection to VDD through current limiting resistor).
[3] Optimum configuration when external N-type (NPN, NMOS) driver used.
[4] Optimum configuration when external P-type (PNP, PMOS) driver used.
Table 17. Use of INVRT and OUTDRV based on connection to the LEDn outputs when OE=0
[1]
INVRT OUTDRV Direct connection to LEDn External N-type driver External P-type driver
Firmware External
pull-up
resistor
Firmware External
pull-up
resistor
Firmware External
pull-up
resistor
0 0 formulas and LED
output state values
apply[2]
LED current
limiting R[2] formulas and LED
output state
values inverted
required formulas and LED
output state values
apply
required
0 1 formulas and LED
output state values
apply[2]
LED current
limiting R[2] formulas and LED
output state
values inverted
not required formulas and LED
output state values
apply[4]
not
required[4]
1 0 formulas and LED
output state values
inverted
LED current
limiting R formulas and LED
output state
values apply
required formulas and LED
output state values
inverted
required
1 1 formulas and LED
output state values
inverted
LED current
limiting R formulas and LED
output state
values apply[3]
not
required[3] formulas and LED
output state values
inverted
not required

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 19 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
[1] OE applies to 16-pin version only. When OE = 1, LED output state is controlled only by OUTNE[1:0] bits (MODE2 register).
[2] External pull-up or LED current limiting resistor connects LEDn to VDD.
Table 18. Output transistors based on LEDOUT registers, INVRT and OUTDRV bits when OE = 0[1]
LEDOUT INVRT OUTDRV Upper transistor
(VDD to LEDn) Lower transistor
(LEDn to VSS)LEDn state
00
LED driver off
0 0 off off high-Z[2]
0 1 on off VDD
1 0 off on VSS
1 1 off on VSS
01
LED driver on
0 0 off on VSS
0 1 off on VSS
1 0 off off high-Z[2]
1 1 on off VDD
10
Individual
brightness
control
0 0 off Individual PWM
(non-inverted) VSS or high-Z[2] = PWMx value
0 1 Individual PWM
(non-inverted) Individual PWM
(non-inverted) VSS or VDD = PWMx value
1 0 off Individual PWM
(inverted) high-Z[2] or VSS = 1 −PWMx value
1 1 Individual PWM
(inverted) Individual PWM
(inverted) VDD or VSS = 1 −PWMx value
11
Individual +
Group
dimming/blinking
0 0 off Individual + Group
PWM
(non-inverted)
VSS or high-Z[2] = PWMx/GRPPWM values
0 1 Individual PWM
(non-inverted) Individual PWM
(non-inverted) VSS or VDD = PWMx/GRPPWM values
1 0 off Individual + Group
PWM (inverted) high-Z[2] or VSS = (1 −PWMx) or
(1 −GRPPWM) values
1 1 Individual PWM
(inverted) Individual PWM
(inverted) VDD or VSS =(1−PWMx) or
(1 −GRPPWM) values
fl pimaons
mm N = (o m 255)
WWW Register)
L—J
256 x All ns :10.“ us
(97 5 kHz)
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 20 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
7.8 Individual brightness control with group dimming/blinking
A 97 kHz fixed frequency signal with programmable duty cycle (8 bits, 256 steps) is used
to control individually the brightness for each LED.
On top of this signal, one of the following signals can be superimposed (this signal can be
applied to the 4 LED outputs):
•A lower 190 Hz fixed frequency signal with programmable duty cycle (8 bits,
256 steps) is used to provide a global brightness control.
•A programmable frequency signal from 24 Hz to 1⁄10.73 Hz (8 bits, 256 steps) with
programmable duty cycle (8 bits, 256 steps) is used to provide a global blinking
control.
Minimum pulse width for LEDn Brightness Control is 40 ns.
Minimum pulse width for Group Dimming is 20.48 µs.
When M = 1 (GRPPWM register value), the resulting LEDn Brightness Control + Group Dimming signal will have 2 pulses of
the LED Brightness Control signal (pulse width = N ×40 ns, with ‘N’ defined in PWMx register).
This resulting Brightness + Group Dimming signal above shows a resulting Control signal with M = 4 (8 pulses).
Fig 11. Brightness + Group Dimming signals
123456789101112 507508509510511512 1234567891011
Brightness Control signal (LEDn)
M × 256 × 2 × 40 ns
with M = (0 to 255)
(GRPPWM Register)
N × 40 ns
with N = (0 to 255)
(PWMx Register)
256 × 40 ns = 10.24 µs
(97.6 kHz)
1234567812345678
Group Dimming signal
resulting Brightness + Group Dimming signal
256 × 2 × 256 × 40 ns = 5.24 ms (190.7 Hz)
002aab417

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 21 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
8. Characteristics of the I2C-bus
The I2C-bus is for 2-way, 2-line communication between different ICs or modules. The two
lines are a serial data line (SDA) and a serial clock line (SCL). Both lines must be
connected to a positive supply via a pull-up resistor when connected to the output stages
of a device. Data transfer may be initiated only when the bus is not busy.
8.1 Bit transfer
One data bit is transferred during each clock pulse. The data on the SDA line must remain
stable during the HIGH period of the clock pulse as changes in the data line at this time
will be interpreted as control signals (see Figure 12).
8.1.1 START and STOP conditions
Both data and clock lines remain HIGH when the bus is not busy. A HIGH-to-LOW
transition of the data line while the clock is HIGH is defined as the START condition (S). A
LOW-to-HIGH transition of the data line while the clock is HIGH is defined as the STOP
condition (P) (see Figure 13).
8.2 System configuration
A device generating a message is a ‘transmitter’; a device receiving is the ‘receiver’. The
device that controls the message is the ‘master’ and the devices which are controlled by
the master are the ‘slaves’ (see Figure 14).
Fig 12. Bit transfer
mba607
data line
stable;
data valid
change
of data
allowed
SDA
SCL
Fig 13. Definition of START and STOP conditions
mba608
SDA
SCL P
STOP condition
SDA
SCL
S
START condition

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 22 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
8.3 Acknowledge
The number of data bytes transferred between the START and the STOP conditions from
transmitter to receiver is not limited. Each byte of eight bits is followed by one
acknowledge bit. The acknowledge bit is a HIGH level put on the bus by the transmitter,
whereas the master generates an extra acknowledge related clock pulse.
A slave receiver which is addressed must generate an acknowledge after the reception of
each byte. Also a master must generate an acknowledge after the reception of each byte
that has been clocked out of the slave transmitter. The device that acknowledges has to
pull down the SDA line during the acknowledge clock pulse, so that the SDA line is stable
LOW during the HIGH period of the acknowledge related clock pulse; set-up time and hold
time must be taken into account.
A master receiver must signal an end of data to the transmitter by not generating an
acknowledge on the last byte that has been clocked out of the slave. In this event, the
transmitter must leave the data line HIGH to enable the master to generate a STOP
condition.
Fig 14. System configuration
002aaa966
MASTER
TRANSMITTER/
RECEIVER
SLAVE
RECEIVER
SLAVE
TRANSMITTER/
RECEIVER
MASTER
TRANSMITTER
MASTER
TRANSMITTER/
RECEIVER
SDA
SCL
I2C-BUS
MULTIPLEXER
SLAVE
Fig 15. Acknowledgement on the I2C-bus
002aaa987
S
START
condition
9821
clock pulse for
acknowledgement
not acknowledge
acknowledge
data output
by transmitter
data output
by receiver
SCL from master
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 23 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
9. Bus transactions
(1) 16-pin version only.
(2) See Table 7 for register definition.
Fig 16. Write to a specific register
A5 A4 A3 A2 A1 A0 0 AS A6
slave address(1)
START condition R/W
acknowledge
from slave
002aab418
data for register D3, D2, D1, D0(2)
X X 0 D3 D2 D1 D0X
control register
Auto-Increment flag
Auto-Increment options
A
acknowledge
from slave
A
acknowledge
from slave
P
STOP
condition
(1) 16-pin version only.
Fig 17. Write to all registers using the Auto-Increment feature
A5 A4 A3 A2 A1 A0 0 AS A6
slave address(1)
START condition R/W
acknowledge
from slave
002aab419
MODE1 register
00000001
control register
Auto-Increment on
Auto-Increment
on all registers
A
acknowledge
from slave
A
acknowledge
from slave
P
STOP
condition
(cont.)
(cont.)
MODE1
register
selection
MODE2 register
A
acknowledge
from slave
SUBADR3 register
A
acknowledge
from slave
ALLCALLADR register
A
acknowledge
from slave
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 24 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
(1) 16-pin version only.
Fig 18. Multiple writes to Individual Brightness registers only using the Auto-Increment feature
A5 A4 A3 A2 A1 A0 0 AS A6
slave address(1)
START condition R/W
acknowledge
from slave
002aab420
PWM0 register
01000101
control register
Auto-Increment on
increment
on Individual
brightness
registers only
A
acknowledge
from slave
A
acknowledge
from slave
P
STOP
condition
(cont.)
(cont.)
PWM0
register
selection
PWM1 register
A
acknowledge
from slave
PWM2 register
A
acknowledge
from slave
PWM3 register
A
acknowledge
from slave
PWM0 register
A
acknowledge
from slave
PWMx register
A
acknowledge
from slave
(1) 16-pin version only.
Fig 19. Read all registers using the Auto-Increment feature
A5 A4 A3 A2 A1 A0 0 AS A6
slave address(1)
START condition R/W
acknowledge
from slave
002aab423
00000001
control register
Auto-Increment on
Auto-Increment
on all registers
A
acknowledge
from slave
(cont.)
(cont.)
MODE1
register
selection
data from MODE1 register
A
acknowledge
from master
Sr
ReSTART
condition
A5 A4 A3 A2 A1 A0 1 AA6
slave address(1)
R/W
acknowledge
from slave
data from MODE2 register
A
acknowledge
from master
data from PWM0
A
acknowledge
from master
data from
ALLCALLADR register
A
acknowledge
from master
data from
MODE1 register
A
acknowledge
from master
(cont.)
(cont.)
data from last read byte
A
not acknowledge
from master
P
STOP
condition

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 25 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
(1) 10-pin version is used for this figure. Four PCA9633DP2s are used and the same sequence (A) (above) is sent to each of them.
A[1:0] = 00 to 11.
(2) ALLCALL bit in MODE1 register is equal to 1 for this example.
(3) OCH bit in MODE2 register is equal to 1 for this example.
Fig 20. LED All Call I2C-bus address programming and LED All Call sequence example
1 0 0 0 A1 A0 0 AS 1
slave address(1)
START condition R/W
acknowledge
from slave
002aab424
X X 0 1 1 0 0X
control register
Auto-Increment on
A
acknowledge
from slave
ALLCALLADR
register selection
0 1 0 1 0 1 X1
new LED All Call I2C address(2)
P
STOP
condition
A
acknowledge
from slave
0101010AS1
LED All Call I2C address
START condition R/W
acknowledge
from the
4 devices
X X 0 1 0 0 0X
control register
A
acknowledge
from the
4 devices
LEDOUT
register selection
10101010
LEDOUT register (LED fully ON)
P
STOP
condition
A
acknowledge
from the
4 devices
the 16 LEDs are on at the acknowledge(3)
sequence (A)
sequence (B)
Fig 21. Software Reset (SWRST) Call sequence
002aab425
0000110AS0
SWRST Call I2C address
START condition R/W
acknowledge
from slave(s)
01001011
SWRST data
Byte 1 = A5h
A
acknowledge
from slave(s)
10110100
SWRST data
Byte 2 = 5Ah
P
PCA9633(s) is(are) reset.
Registers are set to default power-up values.
A
acknowledge
from slave(s)
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 26 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
10. Application design-in information
Question 1: What kind of edge rate control is there on the outputs?
•The typical edge rates depend on the output configuration, supply voltage, and the
applied load. The outputs can be configured as either open-drain NMOS or totem pole
outputs. If the customer is using the part to directly drive LEDs, they should be using it
in an open-drain NMOS, if they are concerned about the maximum ISS and ground
bounce. The edge rate control was designed primarily to slow down the turn-on of the
output device; it turns off rather quickly (~1.5 ns). In simulation, the typical turn-on
time for the open-drain NMOS was ~14 ns (VDD = 3.6 V; CL= 50 pF; RPU = 500 Ω).
Question 2: Is ground bounce possible?
•Ground bounce is a possibility, especially if all 16 outputs are changed at full current
(25 mA each). There is a fair amount of decoupling capacitance on chip (~50 pF),
which is intended to suppress some of the ground bounce. The customer will need to
determine if additional decoupling capacitance externally placed as close as
physically possible to the device is required.
I2C-bus address = 0010 101X.
All of the 4 LEDn outputs configurable as either open-drain or totem pole. Mixing of configurations is not possible.
(1) OE requires pull-up resistor if control signal from the master is open-drain.
Fig 22. Typical application
PCA9633
LED0
LED1
SDA
SCL
OE
VDD = 2.5 V, 3.3 V or 5.0 V
I2C-BUS/SMBus
MASTER
002aab286
SDA
SCL
10 kΩ
OE
10 kΩ
LED2
LED3
A0
A1
A2
VDD
A3
A4
A5
A6
VSS
5 V
10 kΩ(1)
12 V

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 27 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
Question 3: Can I really sink 400 mA through the single ground pin on the package and
will this cause any ground bounce problem due to the PWM of the LEDs?
•Yes, you can sink 400 mA through a single ground pin on the package. Although the
package only has one ground pin, there are two ground pads on the die itself
connected to this one pin. Although some ground bounce is likely, it will not disrupt the
operation of the part and would be reduced by the external decoupling capacitance.
Question 4: I can’t turn the LEDs on or off, but their registers are set properly. Why?
•Check the Mode Register 1 bit 4 SLEEP setting. The value needs to be 0 so that the
OSC is turn on. If the OSC is turned off, the LEDs cannot be turned on or off and also
can’t be dimmed or blinked.
Question 5: I’m using LEDs with integrated Zener diodes and the IC is getting very hot.
Why?
•The IC outputs can be set to either open-drain or push-pull and default to push-pull
outputs. In this application with the Zener diodes, they need to be set to open-drain
since in the push-pull architecture there is a low resistance path to GND through the
Zener and this is causing the IC to overheat. The PCA9632/33/34/35 ICs all power-up
in the push-pull output mode and with the logic state HIGH, so one of the first things
that need to be done is to set the outputs to open-drain.
11. Limiting values
Table 19. Limiting values
In accordance with the Absolute Maximum Rating System (IEC 60134).
Symbol Parameter Conditions Min Max Unit
VDD supply voltage −0.5 +6.0 V
VI/O voltage on an input/output pin VSS −0.5 5.5 V
IO(LEDn) output current on pin LEDn - 25 mA
ISS ground supply current - 100 mA
Ptot total power dissipation - 400 mW
Tstg storage temperature −65 +150 °C
Tamb ambient temperature operating −40 +85 °C

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 28 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
12. Static characteristics
Table 20. Static characteristics
V
DD
= 2.3 V to 5.5 V; V
SS
=0V; T
amb
=
−
40
°
Cto+85
°
C; unless otherwise specified.
Symbol Parameter Conditions Min Typ Max Unit
Supply
VDD supply voltage 2.3 - 5.5 V
IDD supply current operating mode; no load; fSCL = 1 MHz
VDD = 2.3 V - 2.5 10 mA
VDD = 3.3 V - 2.5 10 mA
VDD = 5.5 V - 2.5 10 mA
Istb standby current no load; fSCL = 0 Hz; I/O = inputs; VI=V
DD
VDD = 2.3 V - 2.3 11 µA
VDD = 3.3 V - 2.9 12 µA
VDD = 5.5 V - 3.8 15.5 µA
VPOR power-on reset voltage no load; VI=V
DD or VSS [1] - 1.70 2.0 V
Input SCL; input/output SDA
VIL LOW-level input voltage −0.5 - +0.3VDD V
VIH HIGH-level input voltage 0.7VDD - 5.5 V
IOL LOW-level output current VOL = 0.4 V; VDD = 2.3 V 20 - - mA
VOL = 0.4 V; VDD = 5.0 V 30 - - mA
ILleakage current VI=V
DD or VSS −1- +1µA
Ciinput capacitance VI=V
SS - 6 10 pF
LED driver outputs
IOL LOW-level output current VOL = 0.5 V; VDD = 2.3 V [2] 12 - - mA
VOL = 0.5 V; VDD = 3.0 V [2] 17 - - mA
VOL = 0.5 V; VDD = 4.5 V [2] 25 - - mA
IOL(tot) total LOW-level output
current VOL = 0.5 V; VDD = 4.5 V [2] - - 100 mA
IOH HIGH-level output
current open-drain; VOH =V
DD −50 - +50 µA
VOH HIGH-level output
voltage IOH =−10 mA; VDD = 2.3 V 1.6 - - V
IOH =−10 mA; VDD = 3.0 V 2.3 - - V
IOH =−10 mA; VDD = 4.5 V 4.0 - - V
Cooutput capacitance - 2.5 5 pF
OE input
VIL LOW-level input voltage −0.5 - +0.8 V
VIH HIGH-level input voltage 2 - 5.5 V
ILI input leakage current −1- +1µA
Ciinput capacitance - 3.7 5 pF
10F
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 29 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
[1] VDD must be lowered to 0.2 V in order to reset part.
[2] Each bit must be limited to a maximum of 25 mA and the total package limited to 100 mA due to internal busing limits.
13. Dynamic characteristics
[1] Minimum SCL clock frequency is limited by the bus time-out feature, which resets the serial bus interface if either SDA or SCL is held
LOW for a minimum of 25 ms. Disable bus time-out feature for DC operation.
[2] tVD;ACK = time for Acknowledgement signal from SCL LOW to SDA (out) LOW.
[3] tVD;DAT = minimum time for SDA data out to be valid following SCL LOW.
[4] Cb= total capacitance of one bus line in pF.
Address inputs
VIL LOW-level input voltage −0.5 - +0.3VDD V
VIH HIGH-level input voltage 0.7VDD - 5.5 V
ILI input leakage current −1- +1µA
Ciinput capacitance - 3.7 5 pF
Table 20. Static characteristics
…continued
V
DD
= 2.3 V to 5.5 V; V
SS
=0V; T
amb
=
−
40
°
Cto+85
°
C; unless otherwise specified.
Symbol Parameter Conditions Min Typ Max Unit
Table 21. Dynamic characteristics
Symbol Parameter Conditions Standard- mode
I2C-bus Fast-mode
I2C-bus Fast-mode
Plus I2C-bus Unit
Min Max Min Max Min Max
fSCL SCL clock frequency [1] 0 100 0 400 0 1000 kHz
tBUF bus free time between a
STOP and START condition 4.7 - 1.3 - 0.5 - µs
tHD;STA hold time (repeated) START
condition 4.0 - 0.6 - 0.26 - µs
tSU;STA set-up time for a repeated
START condition 4.7 - 0.6 - 0.26 - µs
tSU;STO set-up time for STOP
condition 4.0 - 0.6 - 0.26 - µs
tHD;DAT data hold time 0 - 0 - 0 - ns
tVD;ACK data valid acknowledge time [2] 0.3 3.45 0.1 0.9 0.05 0.45 µs
tVD;DAT data valid time [3] 0.3 3.45 0.1 0.9 0.05 0.45 µs
tSU;DAT data set-up time 250 - 100 - 50 - ns
tLOW LOW period of the SCL
clock 4.7 - 1.3 - 0.5 - µs
tHIGH HIGH period of the SCL
clock 4.0 - 0.6 - 0.26 - µs
tffall time of both SDA and
SCL signals
[5][6] - 300 20 + 0.1Cb[4] 300 - 120 ns
trrise time of both SDA and
SCL signals - 1000 20 + 0.1Cb[4] 300 - 120 ns
tSP pulse width of spikes that
must be suppressed by the
input filter
[7] - 50 - 50 - 50 ns
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 30 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
[5] A master device must internally provide a hold time of at least 300 ns for the SDA signal (refer to the VIL of the SCL signal) in order to
bridge the undefined region of SCL’s falling edge.
[6] The maximum tffor the SDA and SCL bus lines is specified at 300 ns. The maximum fall time (tf) for the SDA output stage is specified at
250 ns. This allows series protection resistors to be connected between the SDA and the SCL pins and the SDA/SCL bus lines without
exceeding the maximum specified tf.
[7] Input filters on the SDA and SCL inputs suppress noise spikes less than 50 ns.
Fig 23. Definition of timing
tSP
tBUF
tHD;STA
PP S
tLOW
tr
tHD;DAT
tf
tHIGH tSU;DAT
tSU;STA
Sr
tHD;STA
tSU;STO
SDA
SCL
002aaa986
Rise and fall times refer to VIL and VIH.
Fig 24. I2C-bus timing diagram
SCL
SDA
tHD;STA tSU;DAT tHD;DAT
tf
tBUF
tSU;STA tLOW tHIGH
tVD;ACK
002aab285
tSU;STO
protocol START
condition
(S)
bit 7
MSB
(A7)
bit 6
(A6) bit 1
(D1) bit 0
(D0)
1 / fSCL
tr
tVD;DAT
acknowledge
(A)
STOP
condition
(P)

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 31 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
14. Test information
RL = Load resistor for LEDn. RL for SDA and SCL > 1 kΩ (3 mA or less current).
CL = Load capacitance includes jig and probe capacitance.
RT = Termination resistance should be equal to the output impedance Zo of the pulse generators.
Fig 25. Test circuitry for switching times
PULSE
GENERATOR
VO
CL
50 pF
RL
500 Ω
002aab880
RT
VI
VDD
DUT
VDD
open
VSS
f%
i
’\
FHHHHHHHH
,—;—
GHEPHLHHHH
+D +PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 32 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
15. Package outline
Fig 26. Package outline SOT109-1 (SO16)
X
wM
θ
A
A1
A2
bp
D
HE
Lp
Q
detail X
E
Z
e
c
L
vMA
(A )
3
A
8
9
1
16
y
pin 1 index
UNIT A
max. A1A2A3bpcD
(1) E(1) (1)
eH
ELL
pQZywv θ
REFERENCES
OUTLINE
VERSION EUROPEAN
PROJECTION ISSUE DATE
IEC JEDEC JEITA
mm
inches
1.75 0.25
0.10 1.45
1.25 0.25 0.49
0.36 0.25
0.19 10.0
9.8 4.0
3.8 1.27 6.2
5.8 0.7
0.6 0.7
0.3 8
0
o
o
0.25 0.1
DIMENSIONS (inch dimensions are derived from the original mm dimensions)
Note
1. Plastic or metal protrusions of 0.15 mm (0.006 inch) maximum per side are not included.
1.0
0.4
SOT109-1 99-12-27
03-02-19
076E07 MS-012
0.069 0.010
0.004 0.057
0.049 0.01 0.019
0.014
0.0100
0.0075 0.39
0.38 0.16
0.15 0.05
1.05
0.041
0.244
0.228 0.028
0.020 0.028
0.012
0.01
0.25
0.01 0.004
0.039
0.016
0 2.5 5 mm
scale
SO16: plastic small outline package; 16 leads; body width 3.9 mm SOT109-1
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 33 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
Fig 27. Package outline SOT505-1 (TSSOP8)
UNIT A1
A
max. A2A3bpLHELpwyv
ceD(1) E(2) Z(1) θ
REFERENCES
OUTLINE
VERSION EUROPEAN
PROJECTION ISSUE DATE
IEC JEDEC JEITA
mm 0.15
0.05 0.95
0.80 0.45
0.25 0.28
0.15 3.1
2.9 3.1
2.9 0.65 5.1
4.7 0.70
0.35 6°
0°
0.1 0.10.10.94
DIMENSIONS (mm are the original dimensions)
Notes
1. Plastic or metal protrusions of 0.15 mm maximum per side are not included.
2. Plastic or metal protrusions of 0.25 mm maximum per side are not included.
0.7
0.4
SOT505-1 99-04-09
03-02-18
wM
bp
D
Z
e
0.25
14
85
θ
A
A2A1
Lp
(A3)
detail X
L
HE
E
c
vMA
X
A
y
2.5 5 mm0
scale
TSSOP8: plastic thin shrink small outline package; 8 leads; body width 3 mm SOT505-1
1.1
pin 1 index
(11
M
;
S©M
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 34 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
Fig 28. Package outline SOT552-1 (TSSOP10)
UNIT A1
A
max. A2A3bpLHELpwyv
ceD(1) E(2) Z(1) θ
REFERENCES
OUTLINE
VERSION EUROPEAN
PROJECTION ISSUE DATE
IEC JEDEC JEITA
mm 0.15
0.05 0.95
0.80 0.30
0.15 0.23
0.15 3.1
2.9 3.1
2.9 0.5 5.0
4.8 0.67
0.34 6°
0°
0.1 0.10.10.95
DIMENSIONS (mm are the original dimensions)
Notes
1. Plastic or metal protrusions of 0.15 mm maximum per side are not included.
2. Plastic or metal protrusions of 0.25 mm maximum per side are not included.
0.7
0.4
SOT552-1 99-07-29
03-02-18
wM
bp
D
Z
e
0.25
15
10 6
θ
A
A2A1
Lp
(A3)
detail X
L
HE
E
c
vMA
X
A
y
2.5 5 mm0
scale
TSSOP10: plastic thin shrink small outline package; 10 leads; body width 3 mm SOT552-1
1.1
pin 1 index
G‘HHH1HHHF
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 35 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
Fig 29. Package outline SOT403-1 (TSSOP16)
UNIT A1A2A3bpcD
(1) E(2) (1)
eH
ELL
pQZywv θ
REFERENCES
OUTLINE
VERSION EUROPEAN
PROJECTION ISSUE DATE
IEC JEDEC JEITA
mm 0.15
0.05 0.95
0.80 0.30
0.19 0.2
0.1 5.1
4.9 4.5
4.3 0.65 6.6
6.2 0.4
0.3 0.40
0.06 8
0
o
o
0.13 0.10.21
DIMENSIONS (mm are the original dimensions)
Notes
1. Plastic or metal protrusions of 0.15 mm maximum per side are not included.
2. Plastic interlead protrusions of 0.25 mm maximum per side are not included.
0.75
0.50
SOT403-1 MO-153 99-12-27
03-02-18
wM
bp
D
Z
e
0.25
18
16 9
θ
A
A1
A2
Lp
Q
detail X
L
(A )
3
HE
E
c
vMA
X
A
y
0 2.5 5 mm
scale
TSSOP16: plastic thin shrink small outline package; 16 leads; body width 4.4 mm SOT403-1
A
max.
1.1
pin 1 index
E@ m
E flfi _ ‘
7 4- w
DJ ‘8 ED
D , m$ vat?
W a EC 5
\M‘ , ‘
11L \\\\\\ kfimm ‘‘‘‘‘ W “““ m a
i R flw i H
W , U , w P
/ W W g 33 a
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 36 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
Fig 30. Package outline SOT629-1 (HVQFN16)
terminal 1
index area
0.651
A1Eh
b
UNIT ye
0.2
c
REFERENCES
OUTLINE
VERSION EUROPEAN
PROJECTION ISSUE DATE
IEC JEDEC JEITA
mm 4.1
3.9
Dh
2.25
1.95
y1
4.1
3.9 2.25
1.95
e1
1.95
e2
1.95
0.38
0.23
0.05
0.00 0.05 0.1
DIMENSIONS (mm are the original dimensions)
SOT629-1 MO-220 - - -- - -
0.75
0.50
L
0.1
v
0.05
w
0 2.5 5 mm
scale
SOT629-1
HVQFN16: plastic thermal enhanced very thin quad flat package; no leads;
16 terminals; body 4 x 4 x 0.85 mm
A(1)
max.
AA1
c
detail X
y
y1C
e
L
Eh
Dh
e
e1
b
58
16 13
12
9
4
1
X
D
E
C
BA
e2
01-08-08
02-10-22
terminal 1
index area
1/2 e
1/2 e
AC
C
B
vM
wM
E(1)
Note
1. Plastic or metal protrusions of 0.075 mm maximum per side are not included.
D(1)
r |:| ,
MW 3
wi+i , ,,,
mmlmm a
E©
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 37 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
Fig 31. Package outline SOT908-1 (HVSON8)
0.50.21 0.05
0.00
A1Eh
b
UNIT D(1) ye
1.5
e1
REFERENCES
OUTLINE
VERSION EUROPEAN
PROJECTION ISSUE DATE
IEC JEDEC JEITA
mm 3.1
2.9
cD
h
1.65
1.35
y1
3.1
2.9
2.25
1.95
0.3
0.2 0.05 0.1
DIMENSIONS (mm are the original dimensions)
SOT908-1 MO-229
E(1)
0.5
0.3
L
0.1
v
0.05
w
SOT908-1
HVSON8: plastic thermal enhanced very thin small outline package; no leads;
8 terminals; body 3 x 3 x 0.85 mm
A(1)
max.
05-09-26
05-10-05
Note
1. Plastic or metal protrusions of 0.075 mm maximum per side are not included.
X
terminal 1
index area
B A
D
E
detail X
A
A1
c
C
y
C
y1
exposed tie bar (4×)
exposed tie bar (4×)
b
terminal 1
index area
e1
eAC B
vM
C wM
Eh
Dh
L
14
58
0 1 2 mm
scale

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 38 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
16. Handling information
Inputs and outputs are protected against electrostatic discharge in normal handling.
However, to be completely safe you must take normal precautions appropriate to handling
integrated circuits.
17. Soldering of SMD packages
This text provides a very brief insight into a complex technology. A more in-depth account
of soldering ICs can be found in Application Note
AN10365 “Surface mount reflow
soldering description”
.
17.1 Introduction to soldering
Soldering is one of the most common methods through which packages are attached to
Printed Circuit Boards (PCBs), to form electrical circuits. The soldered joint provides both
the mechanical and the electrical connection. There is no single soldering method that is
ideal for all IC packages. Wave soldering is often preferred when through-hole and
Surface Mount Devices (SMDs) are mixed on one printed wiring board; however, it is not
suitable for fine pitch SMDs. Reflow soldering is ideal for the small pitches and high
densities that come with increased miniaturization.
17.2 Wave and reflow soldering
Wave soldering is a joining technology in which the joints are made by solder coming from
a standing wave of liquid solder. The wave soldering process is suitable for the following:
•Through-hole components
•Leaded or leadless SMDs, which are glued to the surface of the printed circuit board
Not all SMDs can be wave soldered. Packages with solder balls, and some leadless
packages which have solder lands underneath the body, cannot be wave soldered. Also,
leaded SMDs with leads having a pitch smaller than ~0.6 mm cannot be wave soldered,
due to an increased probability of bridging.
The reflow soldering process involves applying solder paste to a board, followed by
component placement and exposure to a temperature profile. Leaded packages,
packages with solder balls, and leadless packages are all reflow solderable.
Key characteristics in both wave and reflow soldering are:
•Board specifications, including the board finish, solder masks and vias
•Package footprints, including solder thieves and orientation
•The moisture sensitivity level of the packages
•Package placement
•Inspection and repair
•Lead-free soldering versus SnPb soldering
17.3 Wave soldering
Key characteristics in wave soldering are:

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 39 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
•Process issues, such as application of adhesive and flux, clinching of leads, board
transport, the solder wave parameters, and the time during which components are
exposed to the wave
•Solder bath specifications, including temperature and impurities
17.4 Reflow soldering
Key characteristics in reflow soldering are:
•Lead-free versus SnPb soldering; note that a lead-free reflow process usually leads to
higher minimum peak temperatures (see Figure 32) than a SnPb process, thus
reducing the process window
•Solder paste printing issues including smearing, release, and adjusting the process
window for a mix of large and small components on one board
•Reflow temperature profile; this profile includes preheat, reflow (in which the board is
heated to the peak temperature) and cooling down. It is imperative that the peak
temperature is high enough for the solder to make reliable solder joints (a solder paste
characteristic). In addition, the peak temperature must be low enough that the
packages and/or boards are not damaged. The peak temperature of the package
depends on package thickness and volume and is classified in accordance with
Table 22 and 23
Moisture sensitivity precautions, as indicated on the packing, must be respected at all
times.
Studies have shown that small packages reach higher temperatures during reflow
soldering, see Figure 32.
Table 22. SnPb eutectic process (from J-STD-020C)
Package thickness (mm) Package reflow temperature (°C)
Volume (mm3)
< 350 ≥ 350
< 2.5 235 220
≥ 2.5 220 220
Table 23. Lead-free process (from J-STD-020C)
Package thickness (mm) Package reflow temperature (°C)
Volume (mm3)
< 350 350 to 2000 > 2000
< 1.6 260 260 260
1.6 to 2.5 260 250 245
> 2.5 250 245 245
maxmum peak tempevaiure
= MSL mun damage level
mmmum peaklempevamve
= mwnwmum somenng tempevamre
PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 40 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
For further information on temperature profiles, refer to Application Note
AN10365
“Surface mount reflow soldering description”
.
18. Abbreviations
MSL: Moisture Sensitivity Level
Fig 32. Temperature profiles for large and small components
001aac844
temperature
time
minimum peak temperature
= minimum soldering temperature
maximum peak temperature
= MSL limit, damage level
peak
temperature
Table 24. Abbreviations
Acronym Description
CDM Charged-Device Model
DUT Device Under Test
EMI ElectroMagnetic Interference
ESD ElectroStatic Discharge
HBM Human Body Model
I2C-bus Inter-Integrated Circuit bus
LCD Liquid Crystal Display
LED Light Emitting Diode
LSB Least Significant Bit
MM Machine Model
MSB Most Significant Bit
NMOS Negative-channel Metal-Oxide Semiconductor
PCB Printed-Circuit Board
PMOS Positive-channel Metal-Oxide Semiconductor
PWM Pulse Width Modulation
RGB Red/Green/Blue
RGBA Red/Green/Blue/Amber
SMBus System Management Bus

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 41 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
19. Revision history
Table 25. Revision history
Document ID Release date Data sheet status Change notice Supersedes
PCA9633_5 20080725 Product data sheet - PCA9633_4
Modifications: •Section 2 “Features”:
–9th bullet item: changed “up to 4 and 126 PCA9633 devices” to “up to 4 and 126 devices”
–deleted (old) 12th bullet item
•Section 7.1.1 “Regular I2C-bus slave address”: Remark re-written; added (new) 1st and 2nd bullet
items
•Figure 21 “Software Reset (SWRST) Call sequence”:
–changed “Byte 1 = 0xA5” to “Byte 1 = A5h”
–changed “Byte 2 = 0x5A” to “Byte 2 = 5Ah”
•Figure 25 “Test circuitry for switching times”: changed “GND” to “VSS”
PCA9633_4 20080304 Product data sheet - PCA9633_3
PCA9633_3 20061220 Product data sheet - PCA9633_2
PCA9633_2 20061114 Product data sheet - PCA9633_1
PCA9633_1
(9397 750 14614) 20060123 Product data sheet - -

PCA9633_5 © NXP B.V. 2008. All rights reserved.
Product data sheet Rev. 05 — 25 July 2008 42 of 43
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
20. Legal information
20.1 Data sheet status
[1] Please consult the most recently issued document before initiating or completing a design.
[2] The term ‘short data sheet’ is explained in section “Definitions”.
[3] The product status of device(s) described in this document may have changed since this document was published and may differ in case of multiple devices. The latest product status
information is available on the Internet at URL http://www.nxp.com.
20.2 Definitions
Draft — The document is a draft version only. The content is still under
internal review and subject to formal approval, which may result in
modifications or additions. NXP Semiconductors does not give any
representations or warranties as to the accuracy or completeness of
information included herein and shall have no liability for the consequences of
use of such information.
Short data sheet — A short data sheet is an extract from a full data sheet
with the same product type number(s) and title. A short data sheet is intended
for quick reference only and should not be relied upon to contain detailed and
full information. For detailed and full information see the relevant full data
sheet, which is available on request via the local NXP Semiconductors sales
office. In case of any inconsistency or conflict with the short data sheet, the
full data sheet shall prevail.
20.3 Disclaimers
General — Information in this document is believed to be accurate and
reliable. However, NXP Semiconductors does not give any representations or
warranties, expressed or implied, as to the accuracy or completeness of such
information and shall have no liability for the consequences of use of such
information.
Right to make changes — NXP Semiconductors reserves the right to make
changes to information published in this document, including without
limitation specifications and product descriptions, at any time and without
notice. This document supersedes and replaces all information supplied prior
to the publication hereof.
Suitability for use — NXP Semiconductors products are not designed,
authorized or warranted to be suitable for use in medical, military, aircraft,
space or life support equipment, nor in applications where failure or
malfunction of an NXP Semiconductors product can reasonably be expected
to result in personal injury, death or severe property or environmental
damage. NXP Semiconductors accepts no liability for inclusion and/or use of
NXP Semiconductors products in such equipment or applications and
therefore such inclusion and/or use is at the customer’s own risk.
Applications — Applications that are described herein for any of these
products are for illustrative purposes only. NXP Semiconductors makes no
representation or warranty that such applications will be suitable for the
specified use without further testing or modification.
Limiting values — Stress above one or more limiting values (as defined in
the Absolute Maximum Ratings System of IEC 60134) may cause permanent
damage to the device. Limiting values are stress ratings only and operation of
the device at these or any other conditions above those given in the
Characteristics sections of this document is not implied. Exposure to limiting
values for extended periods may affect device reliability.
Terms and conditions of sale — NXP Semiconductors products are sold
subject to the general terms and conditions of commercial sale, as published
at http://www.nxp.com/profile/terms, including those pertaining to warranty,
intellectual property rights infringement and limitation of liability, unless
explicitly otherwise agreed to in writing by NXP Semiconductors. In case of
any inconsistency or conflict between information in this document and such
terms and conditions, the latter will prevail.
No offer to sell or license — Nothing in this document may be interpreted
or construed as an offer to sell products that is open for acceptance or the
grant, conveyance or implication of any license under any copyrights, patents
or other industrial or intellectual property rights.
20.4 Trademarks
Notice: All referenced brands, product names, service names and trademarks
are the property of their respective owners.
I2C-bus — logo is a trademark of NXP B.V.
21. Contact information
For more information, please visit: http://www.nxp.com
For sales office addresses, please send an email to: salesaddresses@nxp.com
Document status[1][2] Product status[3] Definition
Objective [short] data sheet Development This document contains data from the objective specification for product development.
Preliminary [short] data sheet Qualification This document contains data from the preliminary specification.
Product [short] data sheet Production This document contains the product specification.
founded by
PHILIPS
NXP Semiconductors PCA9633
4-bit Fm+ I2C-bus LED driver
© NXP B.V. 2008. All rights reserved.
For more information, please visit: http://www.nxp.com
For sales office addresses, please send an email to: salesaddresses@nxp.com
Date of release: 25 July 2008
Document identifier: PCA9633_5
Please be aware that important notices concerning this document and the product(s)
described herein, have been included in section ‘Legal information’.
22. Contents
1 General description . . . . . . . . . . . . . . . . . . . . . . 1
2 Features . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 2
3 Applications . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3
4 Ordering information. . . . . . . . . . . . . . . . . . . . . 3
5 Block diagram . . . . . . . . . . . . . . . . . . . . . . . . . . 4
6 Pinning information. . . . . . . . . . . . . . . . . . . . . . 5
6.1 Pinning . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5
6.2 Pin description . . . . . . . . . . . . . . . . . . . . . . . . . 6
7 Functional description . . . . . . . . . . . . . . . . . . . 8
7.1 Device addresses . . . . . . . . . . . . . . . . . . . . . . . 8
7.1.1 Regular I2C-bus slave address . . . . . . . . . . . . . 8
7.1.2 LED All Call I2C-bus address . . . . . . . . . . . . . . 9
7.1.3 LED Sub Call I2C-bus addresses . . . . . . . . . . . 9
7.1.4 Software Reset I2C-bus address . . . . . . . . . . . 9
7.2 Control register . . . . . . . . . . . . . . . . . . . . . . . . 10
7.3 Register definitions . . . . . . . . . . . . . . . . . . . . . 11
7.3.1 Mode register 1, MODE1 . . . . . . . . . . . . . . . . 12
7.3.2 Mode register 2, MODE2 . . . . . . . . . . . . . . . . 12
7.3.3 PWM registers 0 to 3, PWMx — Individual
brightness control registers . . . . . . . . . . . . . . 13
7.3.4 Group duty cycle control, GRPPWM . . . . . . . 13
7.3.5 Group frequency, GRPFREQ . . . . . . . . . . . . . 14
7.3.6 LED driver output state, LEDOUT . . . . . . . . . 14
7.3.7 I2C-bus subaddress 1 to 3, SUBADRx . . . . . . 15
7.3.8 LED All Call I2C-bus address, ALLCALLADR. 15
7.4 Active LOW output enable input . . . . . . . . . . . 16
7.5 Power-on reset . . . . . . . . . . . . . . . . . . . . . . . . 16
7.6 Software Reset . . . . . . . . . . . . . . . . . . . . . . . . 17
7.7 Using the PCA9633 with and without
external drivers . . . . . . . . . . . . . . . . . . . . . . . . 18
7.8 Individual brightness control with group
dimming/blinking. . . . . . . . . . . . . . . . . . . . . . . 20
8 Characteristics of the I2C-bus. . . . . . . . . . . . . 21
8.1 Bit transfer . . . . . . . . . . . . . . . . . . . . . . . . . . . 21
8.1.1 START and STOP conditions . . . . . . . . . . . . . 21
8.2 System configuration . . . . . . . . . . . . . . . . . . . 21
8.3 Acknowledge . . . . . . . . . . . . . . . . . . . . . . . . . 22
9 Bus transactions . . . . . . . . . . . . . . . . . . . . . . . 23
10 Application design-in information . . . . . . . . . 26
11 Limiting values. . . . . . . . . . . . . . . . . . . . . . . . . 27
12 Static characteristics. . . . . . . . . . . . . . . . . . . . 28
13 Dynamic characteristics . . . . . . . . . . . . . . . . . 29
14 Test information. . . . . . . . . . . . . . . . . . . . . . . . 31
15 Package outline . . . . . . . . . . . . . . . . . . . . . . . . 32
16 Handling information. . . . . . . . . . . . . . . . . . . . 38
17 Soldering of SMD packages . . . . . . . . . . . . . . 38
17.1 Introduction to soldering. . . . . . . . . . . . . . . . . 38
17.2 Wave and reflow soldering . . . . . . . . . . . . . . . 38
17.3 Wave soldering. . . . . . . . . . . . . . . . . . . . . . . . 38
17.4 Reflow soldering. . . . . . . . . . . . . . . . . . . . . . . 39
18 Abbreviations . . . . . . . . . . . . . . . . . . . . . . . . . 40
19 Revision history . . . . . . . . . . . . . . . . . . . . . . . 41
20 Legal information . . . . . . . . . . . . . . . . . . . . . . 42
20.1 Data sheet status . . . . . . . . . . . . . . . . . . . . . . 42
20.2 Definitions . . . . . . . . . . . . . . . . . . . . . . . . . . . 42
20.3 Disclaimers. . . . . . . . . . . . . . . . . . . . . . . . . . . 42
20.4 Trademarks . . . . . . . . . . . . . . . . . . . . . . . . . . 42
21 Contact information . . . . . . . . . . . . . . . . . . . . 42
22 Contents. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 43
Products related to this Datasheet
IC LED DRVR LIN DIM 25MA 16HVQFN
IC LED DRIVER PS DIM 25MA 16SO
IC LED DRVR PS DIM 25MA 16TSSOP
IC LED DRVR LIN DIM 25MA 16HVQFN
BOARD DEMO FOR PHILIPS PCA9633
IC LED DRIVER PS DIM 25MA 16SO
IC LED DRVR LIN DIM 25MA 16HVQFN
IC LED DRIVER PS DIM 25MA 16SO
IC LED DRIVER PS DIM 25MA 16SO