D6T Series Catalog Datasheet by Omron Electronics Inc-EMC Div

View All Related Products | Download PDF Datasheet
MEMS Thermal Sensors
D6T
Contactless measurement
creating energy-efficient and comfortable living spaces
Application examples provided in this document are for reference only. In actual applications, confirm equipment functions and safety before using the product.
Consult your OMRON representative before using the product under conditions which are not described in the manual or applying the product to nuclear control systems, railroad
systems, aviation systems, vehicles, combustion systems, medical equipment, amusement machines, safety equipment, and other systems or equipment that may have a serious
influence on lives and property if used improperly. Make sure that the ratings and performance characteristics of the product provide a margin of safety for the system or
equipment, and be sure to provide the system or equipment with double safety mechanisms.
OMRON Corporation
Electronic and Mechanical Components Company
Regional Contact
Cat. No. A274-E1-01
0318-0.5M(0318)(O)
Americas Europe
https://www.components.omron.com/ http://components.omron.eu/
Asia-Pacific China
https://ecb.omron.com.sg/ https://www.ecb.omron.com.cn/
Korea Japan
https://www.omron-ecb.co.kr/ https://www.omron.co.jp/ecb/
In the interest of product improvement, specifications are subject to change without notice.
© OMRON Corporation 2018 All Rights Reserved.
Detect wavelengths in the range 8-12 μm
Infrared ray
Achieving the highest level of SNR* in the world *2
* SNR: Signal-to-Noise Ratio. Compares the level of a signal to the level of background noise
*2 As of December 2017, according to OMRON research
Converts sensor signal to digital temperature
output allowing easy use of microcontroller
Space-saving design,
well-suited for embedded applications
Easy
connection
Compact size
MEMS Thermal Sensors D6T
Silicon lens
far-infrared focusing
MEMS
thermopile
Detection principle
MEMS thermopile
Electromotive force occurrence
Thermopile
Hot junction
Infrared rayCold junction Cold junction
ASIC
Low noise amplifier
MCU
A/D conversion,
calculation, I2C and I/F
Si
High Accuracy, Smaller Footprint, East to Work With
OMRON's unique MEMS technology allows combining thermopile elements
and ASICs into one package resulting to ultra-compact footprint.
MEMS Thermal (IR* sensor) measures the surface temperature of objects without touching them
when the thermopile element absorbs the amount of radiant energy from the object.
*IR: Infrared Ray
Low noise
Cross-section
view of D6T sensor
The sensor utilizes the seebeck effect in which thermoelectric
force is generated due to the temperature difference that occurs
across the junction points of two different types of metal.
2 3
microcontroller
Detect wavelengths in the range 8-12 μm
Infrared ray
Achieving the highest level of SNR* in the world *2
* SNR: Signal-to-Noise Ratio. Compares the level of a signal to the level of background noise
*2 As of December 2017, according to OMRON research
Converts sensor signal to digital temperature
output allowing easy use of microcontroller
Space-saving design,
well-suited for embedded applications
Easy
connection
Compact size
MEMS Thermal Sensors D6T
Silicon lens
far-infrared focusing
MEMS
thermopile
Detection principle
MEMS thermopile
Electromotive force occurrence
Thermopile
Hot junction
Infrared rayCold junction Cold junction
ASIC
Low noise amplifier
MCU
A/D conversion,
calculation, I2C and I/F
Si
High Accuracy, Smaller Footprint, East to Work With
OMRON's unique MEMS technology allows combining thermopile elements
and ASICs into one package resulting to ultra-compact footprint.
MEMS Thermal (IR* sensor) measures the surface temperature of objects without touching them
when the thermopile element absorbs the amount of radiant energy from the object.
*IR: Infrared Ray
Low noise
Cross-section
view of D6T sensor
The sensor utilizes the seebeck effect in which thermoelectric
force is generated due to the temperature difference that occurs
across the junction points of two different types of metal.
2 3
MEMS Thermal Sensors D6T
D6T series sensors can detect the slightest temperature changes that can be used in
variety of applications including energy-efficient home appliances and security systems.
The sensors can also be used in the application fields of HEMS (Home Energy Management
System) and BEMS (Building Energy Management System).
Human Detection
2m
2m
1m
4m
Sensor
Detection results of temperature distribution
Installation condition
D6T application fields Air conditioners, lighting systems, security systems, nursing care and monitoring equipment
63.5°
4m 2m 6m
Recommended type: D6T-44L-06 (4x4-element / viewing angle: X=44.2 Y=45.7° / Object temperature range: 0 50degC)
D6T series sensors can detect human presence by sensing changes in human
body temperature with respect to the surrounding temperature.
4 5
MEMS Thermal Sensors D6T
D6T series sensors can detect the slightest temperature changes that can be used in
variety of applications including energy-efficient home appliances and security systems.
The sensors can also be used in the application fields of HEMS (Home Energy Management
System) and BEMS (Building Energy Management System).
Human Detection
2m
2m
1m
4m
Sensor
Detection results of temperature distribution
Installation condition
D6T application fields Air conditioners, lighting systems, security systems, nursing care and monitoring equipment
63.5°
4m 2m 6m
Recommended type: D6T-44L-06 (4x4-element / viewing angle: X=44.2 Y=45.7° / Object temperature range: 0 – 50degC)
D6T series sensors can detect human presence by sensing changes in human
body temperature with respect to the surrounding temperature.
4 5
MEMS Thermal Sensors D6T
Object Detection
D6T sensors can detect objects by pinpointing the target object temperature.
D6T application fields Industrial equipment, non-contact thermometers, refrigerators, microwave ovens, IH cooking heaters, data centers
D6T sensor meets customer needs by
providing a wide range of application support
from home appliances to industrial use.
D6T sensors let you measure temperature without the need to physically touch the object.
This allows measuring temperature where it was not possible for contact thermal sensors due to
space shortage.
The sensors can be used in a wide range of applications including FEMS (Factory Energy
Management System).
6 7
MEMS Thermal Sensors D6T
Object Detection
D6T sensors can detect objects by pinpointing the target object temperature.
D6T application fields Industrial equipment, non-contact thermometers, refrigerators, microwave ovens, IH cooking heaters, data centers
D6T sensor meets customer needs by
providing a wide range of application support
from home appliances to industrial use.
D6T sensors let you measure temperature without the need to physically touch the object.
This allows measuring temperature where it was not possible for contact thermal sensors due to
space shortage.
The sensors can be used in a wide range of applications including FEMS (Factory Energy
Management System).
6 7
MEMS Thermal Sensors D6T
Comparison with Pyroelectric Sensor Viewing Angle and Measurement Area
Pyroelectric sensor
Choose your preferred sensor viewing angle to meet your application needs.
Sensor type D6T-1A-01 D6T-1A-02 D6T-8L-09 D6T- 44L- 06
Number of
elements
Appearance
Size of
measuremen
t area
Distance 1m
Distance 2m
Distance 3m
Number of
elements
X-direction
Y-direction
MEMS thermal sensor (thermopile)
* The sizes of measurement area indicated above are for reference only.
* The size of measurement area changes according to sensor mounting angle.
Output signal
Able to detect human (object) motion Unable to detect stationary
human (object) presence
Able to detect human (object) motion
Able to detect both stationary and motion state of humans (objects).
Detected Undetected
Distance
XX
Y
Y
XX
Y
Y
XX
Y
Y
X = 58.0°
Y = 58.0°
X = 111cm
Y = 111cm
X = 222cm
Y = 222cm
X = 333cm
Y = 333cm
X = 47cm
Y = 47cm
X = 94cm
Y = 94cm
X = 141cm
Y = 141cm
X = 103cm
Y = 10cm
X = 206cm
Y = 20cm
X = 309cm
Y = 30cm
X = 81cm
Y = 84cm
X = 162cm
Y = 169cm
X = 244cm
Y = 253cm
1(1x1) 8(1x8) 16(4x4)
X = 26.5°
Y = 26.5°
X = 54.5°
Y = 5.5°
X=44.2°
Y=45.7°
Both the pyroelectric sensor and non-contact MEMS thermal sensor can detect even the slightest
amount of radiant energy from objects such as infrared radiation and convert them into temperature
readings. However, unlike pyroelectric sensor that relies on motion detection, non-contact MEMS
thermal sensor is able to detect the presence of stationary humans (or objects).
Converts temperature readings only when detecting “temperature changes in the radiant
energy” in its field of view.
Converts temperature readings by “continuously detecting the
temperature of radiant energy” in its field of view
Detected
Output signal Detected Detected Detected
Distance Distance
8 9
7R 1111111 ‘i x i
Sensor type
D6T-1A-01 D6T-1A-02 D6T-8L-09/09H D6T-44L-06/06H D6T-32L-01A
X = 58.0°
Y = 58.0°
X = 111c m
Y = 111c m
X = 222cm
Y = 222cm
X = 333cm
Y = 333cm
X = 47cm
Y = 47cm
X = 94cm
Y = 94cm
X = 141cm
Y = 141cm
X = 103cm
Y = 10cm
X = 206cm
Y = 20cm
X = 309cm
Y = 30cm
X = 81cm
Y = 84cm
X = 162cm
Y = 169cm
X = 244cm
Y = 253cm
X = 200cm
Y = 200cm
X = 400cm
Y = 400cm
X = 600cm
Y = 600cm
1(1x1) 8(1x8) 16(4x4)
X = 26.5°
Y = 26.5°
X = 54.5°
Y = 5.5°
X=44.
Y=45.7°
1024(32x32)
X=90.0°
Y=9 0.0°
Viewing Angle and Measurement Area
Choose your preferred sensor viewing angle to meet your application needs.
* The sizes of measurement area indicated above are for reference only.
* The size of measurement area changes according to sensor mounting angle.
Distance
Number of
elements
Appearance
Size of
measurement
area
Distance 1m
Distance 2m
Distance 3m
Number of
elements
X-direction
Y-direction
Distance Distance Distance
9
10
D6T
D6T
MEMS Thermal Sensors
High Sensitivity Enables Detection
of Stationary Human Presence
OMRON’s unique MEMS and ASIC technology achieve a high SNR
(except for the D6T-32L-01A).
• Superior noise immunity with a digital output.
High-precision area temperature detection with low cross-talk field
of view characteristics.
Ordering Information
Thermal Sensors
Accessories (Sold separately)
Model Number Legend
(1) Number of elements
44L : 16 (4 4)
8L : 8 (1 8)
1A : 1 (1 1)
32L : 1024 (32 32)
(2) Viewing angle
06 : X direction=44.2°, Y direction=45.7°
09 : X direction=54.5°, Y direction=5.5°
01 : X direction, Y direction=58.0°
02 : X direction, Y direction=26.5°
01A : X direction, Y direction=90.0°
(3) Special Functions
H : High-temperature type
Non-display : Standard sensor
RoHS Compliant
Refer to Safety Precautions on page 17.
Element type Model Shape
4×4D6T-44L-06/06H
1×8D6T-8L-09/09H
1×1
D6T-1A-01
D6T-1A-02
32×32 D6T-32L-01A
Type Model
Cable Harness D6T-HARNESS-02
D6T-@-@ @
(1) (2) (3)
11
D6T MEMS Thermal Sensors
Ratings, Specifications, and Functions
Ratings
Characteristics
Functions
*1. Refer to Field of View Characteristics.
*2. Refer to Object Temperature Detection Range.
*3. Reference data
*4. Taken to be the average value of the central 4 pixels.
Item Model D6T-44L-06/06H D6T-8L-09/09H D6T-1A-01 D6T-1A-02 D6T-32L-01A
Power supply voltage 4.5 to 5.5 VDC
Storage temperature range -10 to 60°C -20 to 80°C -20 to 80°C -40 to 80°C -20 to 80°C
(with no icing or condensation)
Operating temperature range 0 to 50°C 0 to 60°C0 to 60°C -40 to 80°C -10 to 70°C
(with no icing or condensation)
Storage humidity range 85% max. 95% max. 95% max. 95% max. 95% max.
(with no icing or condensation)
Operating humidity range 20% to 85% 20% to 95% 20% to 95% 20% to 95% 20% to 95%
(with no icing or condensation)
Item Model D6T-44L-06/06H D6T-8L-09/09H D6T-1A-01 D6T-1A-02 D6T-32L-01A
View angle *1 X direction 44.2°54.5°58.0°26.5°90°
Y direction 45.7°5.5°58.0°26.5°90°
Object temperature
output accuracy *2
Accuracy 1
±1.5°C max.
Measurement conditions: Vcc = 5.0 V
(1) Tx = 25°C, Ta = 25°C
(2) Tx = 45°C, Ta = 25°C
(3) Tx = 45°C, Ta = 45°C
Within ±3.0°C
Measurement
conditions: Vcc = 5.0 V
Tx = 25°C, Ta = 25°C
Central 16-pixel area
Accuracy 2
±3.0°C max.
Measurement conditions: Vcc = 5.0 V
(4) Tx = 25°C, Ta = 45°C
Within ±5.0°C
Measurement
conditions: Vcc = 5.0 V
Tx = 80°C, Ta = 25°C
Central 16-pixel area
Current consumption 5 mA typical 3.5 mA typical 19 mA typical
Item Model D6T-44L-06/06H D6T-8L-09/09H D6T-1A-01 D6T-1A-02 D6T-32L-01A
Object temperature detection
range *2 5 to 50°C/5 to 200°C 5 to 50°C/5 to 200°C 5 to 50°C-40 to 80°C 0 to 200°C
Ambient temperature detection
range *2 5 to 45°C 5 to 45°C 5 to 45°C-40 to 80°C 0 to 80°C
Output specifications Digital values that correspond to the object temperature (Tx) and reference temperature
(Ta) are output from a serial communications port.
Output form Binary code (10 times the detected temperature (°C))
Communications form I2C compliant
Temperature resolution (NETD) *3 0.06°C0.03°C0.02°C0.06°C0.33°C *4
12
D6T MEMS Thermal Sensors
D6T
Object Temperature Detection Range
D6T-44L-06, D6T-8L-09, D6T-1A-01
D6T-44L-06H, D6T-8L-09H
D6T-1A-02
D6T-32L-01A
Connections
Thermal Sensor Configuration Diagram
<D6T-8L-09/09H>
Note: The D6T-44L-06/06H has pixels 0 to 15.
The D6T-1A-01/02 has pixel 0.
The D6T-32L-01A has pixel 0 to 1023.
Terminal Arrangement
-
5 5 15 25 400 102030 455035 55
55
50
45
40
35
30
25
20
15
10
5
0
-
5
Object temperature Tx (°C)
Reference temperature Ta (°C)
: Object temperature
detection range
: Object temperature detection range
0
5
10
15
20
25
30
35
40
45
50
-10 0 20 40 60 80 100 120 140 160 180 200
Object temperature Tx (°C)
Reference temperature Ta (°C)
-50 -30 -10 10 40-40 -20 0 20 50 6030 70 80 90
90
80
70
60
50
40
30
20
10
0
-10
-20
-30
-40
-50
Object temperature Tx (°C)
Reference temperature Ta (°C)
: Object temperature
detection range
Object temperature Tx (°C)
Reference temperature Ta (°C)
: Object temperature detection range
-10
0
10
20
30
40
50
60
70
80
90
-10 0 20 40 60 80 100 120 140 160 180 200
Amplifier Digital processorSensor element
2. VCC
4. SCL
3. SDA
1. GND
Pixel 7
Pixel 0
Terminal Name Function Remarks
1 GND Ground
2VCC
Positive power supply
voltage input
3 SDA Serial data I/O line Connect the open-drain SDA
terminal to a pull-up resistor.
4 SCL Serial clock input Connect the open-drain SCL
terminal to a pull-up resistor.
fining H E
13
D6T MEMS Thermal Sensors
Field of View Characteristics
P0
P1
P2
P3
P4
P5
P6
P7
P8
P9
P10
P11
P12
P13
P14
P15
X direction
Y direction
+
+
X view angle
44.2°
D6T-44L-06/06H
Field of view in X Direction Field of view in Y Direction
Y view angle
45.7°
Detection Area for Each Pixel
Note: Definition of view angle: Using the maximum Sensor output as a refer-
ence, the angular range where the Sensor output is 50% or higher when
the angle of the Sensor is changed is defined as the view angle.
X view angle
54.5°
X direction
Y direction
+
+
P0
P4
P1
P5
P2
P6
P3
P7
D6T-8L-09/09H
Field of view in X Direction Field of view in Y Direction
Y view angle
5.5°
Detection Area for Each Pixel
Note: Definition of view angle: Using the maximum Sensor output as a refer-
ence, the angular range where the Sensor output is 50% or higher when
the angle of the Sensor is changed is defined as the view angle.
DST-1A-01 :' ’ "'7 W W \\ // \\ \ // \ % E \‘7 J" \‘7 7%“ \\ , \‘\ 3' \ a" \ f \ \ % E D67—32L-01A /"” // ”’~\\ LEJ
14
D6T MEMS Thermal Sensors
D6T
X view angle
58.0°
D6T-1A-01
Field of view in X Direction Field of view in Y Direction
Y view angle
58.0°
Detection Area for Each Pixel
X direction
Y direction
D6T-1A-02
Field of view in X Direction Field of view in Y Direction
Y view angle
26.5°
X view angle
26.5°
Note: Definition of view angle: Using the maximum Sensor output as a refer-
ence, the angular range where the Sensor output is 50% or higher when
the angle of the Sensor is changed is defined as the view angle.
D6T-32L-01A
Field of view in X Direction Field of view in Y Direction Detection Area for Each Pixel
Note: Definition of view angle: Using the maximum Sensor output as a refer-
ence, the angular range where the Sensor output is 50% or higher when
the angle of the Sensor is changed is defined as the view angle.
Y view angle
90.0°
X view angle
90.0°
+
+
-
-
X direction
Y direction
P992
P0
P1
P2
P32
P33
P64
P1023
P3
P30
P31
D6T—44L-06/06H A fl Egg D6T—8L-09/09H OOOHPFV # fl EEEEE GEE” : : Tom .4, 1 \W E mam Oman
15
D6T MEMS Thermal Sensors
Dimensions (Unit: mm)
Note: Unless otherwise specified, a tolerance of ±0.3 mm applies to all dimensions.
1
1.5
R1
1
1
1
1
GND
VCCSDA
SCL
SM04B-GHS-TB(JST)
8.25
4.05
(0.85)
4.4
(3.75)
11.5
5
11 14
18
8.3 dia.
1
3.4
Two, 1 dia.
2.5
2.5
R1
R1
R1
D6T-44L-06/06H Supporting and Mounting Area (Shaded Portion)
Top View
Bottom View
Note: Due to insulation distance limitations, do
not allow metal parts to come into contact
with the Sensor.
1 max.
GND
VCCSDA
SCL
SM04B-GHS-TB(JST)
8.25
4.05
(0.78)
4.4
5.32
5
11.6
12
8.3 dia.
1
0.8 max.
0.8 max.
1 max.
1 max.
2 max.
2 max.
2 max.
2 max.
D6T-8L-09/09H Supporting and Mounting Area (Shaded Portion)
Top View
Bottom View
Note: Due to insulation distance limitations, do
not allow metal parts to come into contact
with the Sensor.
D6T—1A—01102 WWWWW UIEIIOCC “J J
16
D6T MEMS Thermal Sensors
D6T
Note: Unless otherwise specified, a tolerance of ±0.3 mm applies to all dimensions.
1 max.
GND
VCCSDA
SCL
SM04B-GHS-TB(JST)
8.25
4.05
0.78
4.4
(3.79)
5
11.6±0.2
12±0.2
8.3 dia.
1
0.8 max.
0.8 max.
1 max.
1 max.
2 max.
2 max.
2 max.
2 max.
D6T-1A-01/02 Supporting and Mounting Area (Shaded Portion)
Top View
Note: Due to insulation distance limitations, do not allow
metal parts to come into contact with the Sensor.
Bottom View
8.25
18
5
14.8
10.7 14
8.15 dia.
Max3.5
4.05
(0.85)
4.4
1
1
2.9
2.9
1
1
3.2
3.2
3.1 3.1
1
1
2.8 2.8
1
4.53
GND
VCCSDA
SCL
SM04B-GHS-TBLFSN(JST)
4-1.3 dia.
R1.2
4-R1.5
D6T-32L-01A Supporting and Mounting Area (Shaded Portion)
Top View
Bottom View
Note: Due to insulation distance limitations, do not allow
metal parts to come into contact with the Sensor.
Cable Color
GND ¡ BLACK Wire
VCC ¡ RED Wire
SDA ¡ BLUE Wire
SCL ¡ YELLOW Wire
* Length of Cable
removed sheath.
Cable :UL1061.AWG#28
UL Tube : T-105-2 No.8
Connector : GHR-04V-S
Contact : SSHL-002T-P0.2
5
15±3 730±10
750±10
GND
VCC
SDA
SCL
660±10
(ϕ3.38 PVC·Black)
*
D6T-HARNESS-02 (Optional - sold separately)
17
D6T MEMS Thermal Sensors
Safety Precautions
Installation
The Sensor may not achieve the characteristics given in this
datasheet due to the ambient environment or installation loca-
tion. Before using the Sensor, please acquire an adequate
understanding and make a prior assessment of Sensor char-
acteristics in your actual system.
Operating Environment
Do not use the Sensor in locations where dust, dirt, oil, and
other foreign matter will adhere to the lens. This may prevent
correct temperature measurements.
Do not use the Sensor in any of the following locations.
Locations where the Sensor may come into contact with
water or oil
• Outdoors
Locations subject to direct sunlight.
Locations subject to corrosive gases (in particular, chlo-
ride, sulfide, or ammonia gases).
Locations subject to extreme temperature changes
Locations subject to icing or condensation.
Locations subject to excessive vibration or shock.
Noise Countermeasures
The Sensor does not contain any protective circuits. Never
subject it to an electrical load that exceeds the absolute maxi-
mum ratings for even an instance. The circuits may be dam-
aged. Install protective circuits as required so that the absolute
maximum ratings are not exceeded.
Keep as much space as possible between the Sensor and
devices that generates high frequencies (such as high-frequency
welders and high-frequency sewing machines) or surges.
Attach a surge protector or noise filter on nearby noise-generating
devices (in particular, motors, transformers, solenoids, magnetic
coils, or devices that have an inductance component).
• In order to prevent inductive noise, separate the connector of
the Sensor from power lines carrying high voltages or large
currents. Using a shielded line is also effective.
If a switching requlator is used, check that malfunctions will not
occur due to switching noise from the power supply.
Handling
This Sensor is a precision device. Do not drop it or subject it to
excessive shock or force. Doing so may damage the Sensor or
change its characteristics. Never subject the connector to
unnecessary force. Do not use a Sensor that has been
dropped.
Take countermeasures against static electricity before you
handle the Sensor.
Turn OFF the power supply to the system before you install
the Sensor. Working with the Sensor while the power supply is
turned ON may cause malfunctions.
Secure the Sensor firmly so that the optical axis does not
move.
Install the Sensor on a flat surface. If the installation surface is
not even, the Sensor may be deformed, preventing correct
measurements.
• Do not install the Sensor with screws. Screws may cause the
resist to peel from the board. Secure the Sensor in a way that
will not cause the resist to peel.
Always check operation after you install the Sensor.
• Use the specified connector (GHR-04 from JST) and connect
it securely so that it will not come off. If you solder directly to
the connector terminals, the Sensor may be damaged.
• Make sure to wire the polarity of the terminals correctly. Incor-
rect polarity may damage the Sensor.
Never attempt to disassemble the Sensor.
Do not use the cable harness to the other product.
Precautions for Correct Use
18
MEMO
Read and understand this catalog. Warranties. Limitation on Liability; Etc. Suitability 0! Use. Programmable Products. Performance Data. Change in Specifications. Errors and Omissions.
19
Terms and Conditions Agreement
Read and understand this catalog.
Please read and understand this catalog before purchasing the products. Please consult your OMRON representative if you have
any questions or comments.
Warranties.
(a) Exclusive Warranty. Omron’s exclusive warranty is that the Products will be free from defects in materials and workmanship
for a period of twelve months from the date of sale by Omron (or such other period expressed in writing
by Omron). Omron disclaims all other warranties, express or implied.
(b) Limitations. OMRON MAKES NO WARRANTY OR REPRESENTATION, EXPRESS OR IMPLIED, ABOUT
NON-INFRINGEMENT, MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE OF THE
PRODUCTS. BUYER ACKNOWLEDGES THAT IT ALONE HAS DETERMINED THAT THE PRODUCTS WILL
SUITABLY MEET THE REQUIREMENTS OF THEIR INTENDED USE.
Omron further disclaims all warranties and responsibility of any type for claims or expenses based on infringement by the Products
or otherwise of any intellectual property right. (c) Buyer Remedy. Omron’s sole obligation hereunder shall be, at Omron’s election,
to (i) replace (in the form originally shipped with Buyer responsible for labor charges for removal or replacement thereof) the
non-complying Product, (ii) repair the non-complying Product, or (iii) repay or credit Buyer an amount equal to the purchase price
of the non-complying Product; provided that in no event shall Omron be responsible for warranty, repair, indemnity or any other
claims or expenses regarding the Products unless Omron’s analysis confirms that the Products were properly handled, stored,
installed and maintained and not subject to contamination, abuse, misuse or inappropriate modification. Return of any Products by
Buyer must be approved in writing by Omron before shipment. Omron Companies shall not be liable for the suitability or
unsuitability or the results from the use of Products in combination with any electrical or electronic components, circuits, system
assemblies or any other materials or substances or environments. Any advice, recommendations or information given orally or in
writing, are not to be construed as an amendment or addition to the above warranty.
See http://www.omron.com/global/ or contact your Omron representative for published information.
Limitation on Liability; Etc.
OMRON COMPANIES SHALL NOT BE LIABLE FOR SPECIAL, INDIRECT, INCIDENTAL, OR CONSEQUENTIAL DAMAGES,
LOSS OF PROFITS OR PRODUCTION OR COMMERCIAL LOSS IN ANY WAY CONNECTED WITH THE PRODUCTS,
WHETHER SUCH CLAIM IS BASED IN CONTRACT, WARRANTY, NEGLIGENCE OR STRICT LIABILITY.
Further, in no event shall liability of Omron Companies exceed the individual price of the Product on which liability is asserted.
Suitability of Use.
Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the
combination of the Product in the Buyer’s application or use of the Product. At Buyer’s request, Omron will provide applicable
third party certification documents identifying ratings and limitations of use which apply to the Product. This information by itself is
not sufficient for a complete determination of the suitability of the Product in combination with the end product, machine, system,
or other application or use. Buyer shall be solely responsible for determining appropriateness of the particular Product with
respect to Buyer’s application, product or system. Buyer shall take application responsibility in all cases.
NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY OR IN LARGE
QUANTITIES WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS,
AND THAT THE OMRON PRODUCT(S) IS PROPERLY RATED AND INSTALLED FOR THE INTENDED USE WITHIN THE
OVERALL EQUIPMENT OR SYSTEM.
Programmable Products.
Omron Companies shall not be responsible for the user’s programming of a programmable Product, or any consequence thereof.
Performance Data.
Data presented in Omron Company websites, catalogs and other materials is provided as a guide for the user in determining
suitability and does not constitute a warranty. It may represent the result of Omron’s test conditions, and the user must correlate it
to actual application requirements. Actual performance is subject to the Omron’s Warranty and Limitations of Liability.
Change in Specifications.
Product specifications and accessories may be changed at any time based on improvements and other reasons. It is our practice
to change part numbers when published ratings or features are changed, or when significant construction changes are made.
However, some specifications of the Product may be changed without any notice. When in doubt, special part numbers may be
assigned to fix or establish key specifications for your application. Please consult with your Omron’s representative at any time to
confirm actual specifications of purchased Product.
Errors and Omissions.
Information presented by Omron Companies has been checked and is believed to be accurate; however, no responsibility is
assumed for clerical, typographical or proofreading errors or omissions.
Regional Contact Amerlcas ImpsJ/wwwcomponenlsommn cum/ AsIa-Pacmc hlmsJ/ecbnmanomsg/ Korea hlmsJ/wwwnmronrecnco kr/ Europe http://componenlsommn ,eu/ Chlna httpszflwwwecb umron mmcn/ Japan hups://www.ommn.co Jp/ecb/ _
Application examples provided in this document are for reference only. In actual applications, confirm equipment functions and safety before using the product.
Consult your OMRON representative before using the product under conditions which are not described in the manual or applying the product to nuclear control systems, railroad
systems, aviation systems, vehicles, combustion systems, medical equipment, amusement machines, safety equipment, and other systems or equipment that may have a serious
influence on lives and property if used improperly. Make sure that the ratings and performance characteristics of the product provide a margin of safety for the system or
equipment, and be sure to provide the system or equipment with double safety mechanisms.
OMRON Corporation
Electronic and Mechanical Components Company
Regional Contact
Cat. No. A274-E1-03
0819(0318)(O)
Americas Europe
https://www.components.omron.com/ http://components.omron.eu/
Asia-Pacific China
https://ecb.omron.com.sg/ https://www.ecb.omron.com.cn/
Korea Japan
https://www.omron-ecb.co.kr/ https://www.omron.co.jp/ecb/
In the interest of product improvement, specifications are subject to change without notice.
© OMRON Corporation 2018-2019 All Rights Reserved.

Products related to this Datasheet

SENSOR DIGITAL -40C-80C MODULE
SENSOR DIGITAL 0C-50C MODULE
SENSOR DIGITAL 0C-50C MODULE
SENSOR DIGITAL 0C-60C MODULE
SENSOR DIGITAL 0C-60C MODULE
CONN CBL HARNESS FOR D6T CAMERA