111P, 233P(-1.5) Series, Install Instr Datasheet by Littelfuse Inc.
View All Related Products | Download PDF Datasheet
®
IIAI I 12334 SPAB
WWW.SymC0m.C0m 222 Disk Dnve, Rapwd cuy, SD 57701
V yuurelecrronircontml@profectfonspecialists (300)3433348 WWW 5mm“ °°’“
INSTALLATION
INSTRUCTIONS
MODEL 233P/111P/233P-1.5
Revision C
Rapid City, SD, USA, 07/2015
II-111-233-15P-B
HAZARDOUS VOLYAGES MAY BE PRESENT DURING INSYALLATION.
Elecmcal shock can cause duth or swans mjury.
Installation should be done byqualmed yevsonnel (OHM/lug ail natlonal, state and local elect-1cm codes
CONNECTIONS
© 2015 SymCom, Inc. All Rights Reserved 2
BE SURE POWER IS DISCONNECTED PRIOR TO INSTALLATION!
FOLLOW NATIONAL, STATE AND LOCAL CODES.
READ THESE INSTRUCTIONS ENTIRELY BEFORE INSTALLATION.
SymCom’s PumpSaver®Plus is a pump monitor designed to protect single-phase pumps from dry-
well, dead-head, jammed impeller, rapid-cycling, overvoltage and undervoltage conditions. The
PumpSaver®Plus Model 233P protects 230V, 2 or 3-wire, 1/3 to 3 hp pumps. The PumpSaver®Plus
Model 233P-1.5 protects 230V, 2 or 3-wire, 1/3 to 1.5 hp pumps. The PumpSaver®Plus Model 111P
protects 115V, 2 or 3-wire, 1/3 to 1 hp pumps. Typical applications include submersible pumps,
centrifugal pumps, circulating pumps, cooling pumps, environmental pumps, residential waterwells,
commercial waterwells, irrigation wells, and golf course and other sprinkler systems.
CONNECTIONS
NOTE: Use with UL/CSA listed overload or impedance protected pumps or motors only.
1. Mount the PumpSaver®Plus in a convenient location in or near the pump control box. If the
location is wet or dusty a NEMA 3R, 4, or 12 enclosure should be used. The PumpSaver®Plus
must be protected by a fuse or circuit breaker (30A RK5 fuse or 30A inverse time breaker max).
2. Connect one line from the fused disconnect to the L1 IN terminal of the PumpSaver®Plus. Run
a wire from the L1 OUT terminal to the other in-line controls such as pressure or float switches.
3. Connect the other line from the fused disconnect (ungrounded fused conductor) to the L2 IN
terminal of the PumpSaver®Plus. Run a wire from the L2 OUT terminal to the other in-line
controls such as pressure or float switches (see Figure 1).
4. Refer to the appropriate wiring diagram for your specific application:
Typical wiring diagram – Figure 1
Standard 3-wire control box – Figure 2
Deluxe control box – Figure 3
2-Wire pump direct feed – Figure 4
*** WARNING ***
PROPER OPERATION REQUIRES FIELD CALIBRATION
GND L2 L1
0 T T
encmnuvscmu
mmm
w mm m: nuxu
L1
L1 I. rus-wnnvmcx . (N
am: i .
massmmm m :
IE \Nsuusn am:- siren: ‘
\1 “as“ wwm
ax mm m wmmmms
a. mu comm
conoL aox
HF Rzuumzu) —> m wzmmox
—’ IMPEDANCE waovscrsn
—’ MOYDR
_>
Gm) u u
TTT
®
® ® ® ® 8 ® .mmcmumsn
4' smwmfip 3.me
comm m
mm m 2119
m my mum»
© 2015 SymCom, Inc. All Rights Reserved 3
FIGURE 1: Typical Wiring Diagram
FIGURE 2: Standard Control Box Wiring Diagram
Gm) u u
TTT
L.
e, x
9ND \ I \
JJ ,, L, 1W
a. mm mm.» n3 msmm ow
® ® 8 ® ® ® mpswczpmzcrzn
MOYOI
. 5me mez
comm Box
m. 3va m mp
mmm m»
GND L2 L1
may we snou—
cllcw uovEcnau
mm
an. m Fuss 0R
:mA mvsls: nu: “ma:
L: : "55mm _;_r\_
an umzl mum ‘
GN n - ‘
Arnzssulz swlvcn m
as wsnLLEn mm mm
an mm m wmmmmfi PREssunEswncN
a. mu canvlm
YD THERMALLYOR
\MPEDANCE PROYECYED
MDYDR
© 2015 SymCom, Inc. All Rights Reserved 4
FIGURE 3: Deluxe Control Box Wiring Diagram
FIGURE 4: 2-Wire Pump Direct-Feed Wiring Diagram
OPERATION
CALIBRATION
CALIBRATING WHILE PUMPING
SENSITIVITV
FIESET MODE / RESTAFIT DELAV
© 2015 SymCom, Inc. All Rights Reserved 5
OPERATION
The PumpSaver®Plus monitors pump load in amps and kilowatts. When the current (amps) exceeds
approximately 125% of calibrated current, or power (kW) drops below the adjustable underload trip
point, the PumpSaver®Plus—after the trip delay—will turn off the pump. The PumpSaver®Plus will
time through the restart delay, and then restart the pump. The calibration is stored in permanent
memory—it does not need to be recalibrated if power is lost.
CALIBRATION
NOTE: The PumpSaver®Plus should be calibrated
during normal pumping conditions.
1. Turn the RESTART DELAY/ CALIBRATION knob
fully counter-clockwise to the CAL. position.
2. Ensure the pressure or float switch is fully closed
so there is a “call for water”.
3. Apply power—the pump will run for approximately
10 seconds then shut off.
4. Set the RESTART DELAY/ CALIBRATION knob
to the desired restart delay (dry-well recovery
time)—the pump will turn on.
CALIBRATING WHILE PUMPING
The PumpSaver®Plus can also be calibrated while the pump is running. Turn the RESTART DELAY/
CALIBRATION knob to CAL. while pumping. Wait for the pump to turn off (approximately 10
seconds), then adjust the RESTART DELAY/ CALIBRATION knob to the desired setting.
SENSITIVITY
The PumpSaver®Plus has an adjustment knob to set the underload trip sensitivity. Setting
SENSITIVITY to the middle position (straight up) is equivalent to SymCom’s standard underload trip
level. Adjust the SENSITIVITY knob to increase/decrease underload sensitivity up to approximately
10% of the standard trip. It may be necessary to increase the sensitivity if the PumpSaver®Plus does
not trip on dry-run or dead-head or it is known that the water level in the well is very low relative to
the pump’s capabilities.
WARNING: Decreasing the SENSITIVITY may compromise the PumpSaver®Plus’ ability to
detect dry-run and/or dead-head conditions.
RESET MODE / RESTART DELAY
Any restart delay can be by-passed by rotating the RESTART DELAY/ CALIBRATION knob to the
RESET position and back to the desired restart delay setting.
NOTE: The restart delay setting can be changed at any time. The current and subsequent
trips will follow the new restart delay setting.
The RESTART DELAY/ CALIBRATION knob can be placed in the RESET position for manual
reset. If the PumpSaver®Plus trips off in this mode due to a voltage or load problem, the RESTART
DELAY/ CALIBRATION knob must be rotated out of the RESET position to restart the pump.
RUN HOURS / FAULT HISTORV
USING AN INFORMER
comgletely comgletely
To Resel Run Hours and Clear Fault History:
RAPID CVCLING
RAPIDCVCLINGlL eS e/Upstream
comgletely comgletely
To Enable Ranid-Cvcle Protection when a Control Device is Installed BEFORE the
PumpSaverl’Plus:
© 2015 SymCom, Inc. All Rights Reserved 6
RUN HOURS / FAULT HISTORY
The PumpSaver®Plus records pump run hours. Run hours can be displayed by a PumpSaver®
Informer (see USING AN INFORMER at the bottom of this page). Run hours and fault history can be
cleared on the PumpSaver®Plus. Read the following instructions fully before performing the
procedure.
NOTE: Turn the SENSITIVITY knob completely to the left (counter-clockwise) or completely to
the right (clockwise) when directed.
To Reset Run Hours and Clear Fault History:
1. Remove power to the PumpSaver®Plus.
2. Set the RESTART DELAY/ CALIBRATION knob to RESET and the SENSITIVITY knob to the
middle (12:00) position.
3. Apply power to the PumpSaver®Plus—the CAL. LIGHT will turn on.
4. Turn the SENSITIVITY knob to the right—the CAL. LIGHT will turn off and the RUN LIGHT will
turn on.
5. Turn the SENSITIVITY knob to the left—both lights will turn on.
6. Turn the SENSITIVITY knob to the right.
7. After 10 seconds, the CAL. and RUN LIGHTS will blink twice indicating the run hours and fault
history have successfully been cleared.
RAPID CYCLING
Rapid cycling is defined as more than 4 restarts in a 60-second period. The PumpSaver®Plus is
capable of detecting a rapid-cycle condition whether a control device, such as a pressure switch, is
installed before* or after it. Upon detecting either form of rapid cycling, the PumpSaver®Plus will
lock-out, preventing damage to the pump. To reset the PumpSaver®Plus, remove and re-apply
power.
RAPID CYCLING (Line Side / Upstream)
Rapid cycling of the line side of the PumpSaver®Plus may be caused by several naturally occurring
conditions which are indistinguishable from true rapid cycling. For this reason, once tripped, the
PumpSaver®Plus will wait 30 minutes and restart. If the restart is successful (the pump runs for
more than one minute), the rapid cycle counter will reset to zero. If the PumpSaver®Plus encounters
rapid cycle 4 times without a successful restart, it will lock-out and require a manual reset. To reset
the PumpSaver®Plus, remove and re-apply power.
*Protection against rapid cycling of a control device installed before the PumpSaver®Plus is
disabled by default. Read the following instructions fully before performing the procedure to enable
this feature.
NOTE: Turn the SENSITIVITY knob completely to the left (counter-clockwise) or completely to
the right (clockwise) when directed.
To Enable Rapid-Cycle Protection when a Control Device is Installed BEFORE the
PumpSaver®Plus: (to disable, follow the same procedure)
1. Remove power to the PumpSaver®Plus.
2. Set the RESTART DELAY/ CALIBRATION knob to RESET and the SENSITIVITY knob to the
middle (12:00) position.
3. Apply power to the PumpSaver®Plus —the CAL. LIGHT will turn on.
4. Turn the SENSITIVITY knob to the right—the CAL. LIGHT will turn off, RUN LIGHT will turn on.
5. Turn the SENSITIVITY knob to the left—both lights will turn on.
6. Turn the SENSITIVITY knob right—left—right—left—right.
7. After 2 seconds, the CAL. and RUN LIGHTS will blink once indicating line side rapid-cycle
RAPID CVCLING (Load de / Downstream)
USING AN INFORMER
© 2015 SymCom, Inc. All Rights Reserved 7
protection has been enabled.
RAPID CYCLING (Load Side / Downstream)
Load side rapid cycling of the pump will immediately result in a manual lock-out. The pump will not
restart automatically. To reset the PumpSaver®Plus, remove and re-apply power.
Note: Protection against rapid cycling of a control device installed after the PumpSaver®Plus is
always enabled. Disabling line side detection will not disable load side detection.
USING AN INFORMER
PumpSaver®Plus products are equipped with an infrared LED that will communicate to a SymCom
Informer—a handheld, battery-operated, diagnostic tool. The Informer—when directed at the
PumpSaver®Plus—will display real-time voltage, current and power; dry-well and overcurrent trip
points; calibration voltage; last 20 faults; voltage, current and power at the last fault; highest/lowest
voltage and current since calibration; the model number; and the CT size if applicable. The Informer
can be used on any single-phase PumpSaver®Plus equipped with an infrared LED transmitter.
Contact SymCom for more information at 800-843-8848 or visit our website: www.symcom.com.
TROUBLESHOOTING
© 2015 SymCom, Inc. All Rights Reserved 8
TROUBLESHOOTING
RUN LIGHT
CAL. LIGHT
PROBLEM or FUNCTION
CORRECTIVE ACTION
On Steady
Off
RUN:
Pump is running—or ready to
run—no problems in operation
If pump is not running, check for
loose wiring and ensure proper
function of pressure or float
switches.
On Steady
On Steady
CAL:
The PumpSaver®Plus is in the
calibration process.
None
Off
On Steady
CAL COMPLETE:
The PumpSaver®Plus has
calibrated, the RESTART
DELAY/ CALIBRATION knob
was left in the CAL. position.
Pump is off.
Pump will restart as soon as the
RESTART DELAY/
CALIBRATION knob is rotated
out of the CAL. position.
Off
Off
OFF / MANUAL RESTART:
The pump is not running. Either
the PumpSaver®Plus has tripped
on dry-run, dead-head, or
overcurrent while the RESTART
DELAY/ CALIBRATION knob
was in the RESET position or
source power is not present.
If knob is in the RESET position,
rotate out of RESET—If the CAL.
light blinks, check for an
overcurrent condition. If the RUN
light blinks, look for a dry-run or
dead-head condition. If no lights
come on, check incoming power
for adequate voltage.
Blinking
Off
DRY RUN / DEAD HEAD:
The PumpSaver®Plus has shut
the pump off due to a dry run or
dead head condition. The unit is
timing through the restart delay
and will try to restart.
Check for restricted flow or
inadequate supply of liquid.
Off
Blinking
OVERCURRENT:
The PumpSaver®Plus has shut
the pump off due to an
overcurrent condition. The unit is
timing through the restart delay
and will try to restart if line voltage
is at an acceptable level.
Check for low or high voltage or
jammed pump impellers. If these
conditions do not exist,
recalibrate the unit while it is
drawing higher current (amps
should not exceed SFA).
Blinking
alternately
with the
CAL. LIGHT
Blinking
alternately
with the
RUN LIGHT
VOLTAGE FAULT:
The PumpSaver®Plus is
preventing the pump from starting
due to voltage problems. The
voltage is being interrogated and
the unit will remain in this mode
until the voltage is at an
acceptable level.
If the unit remains in this state for
more than 5 seconds, check for
high or low voltage.
Blinking in
unison with
the CAL.
LIGHT
Blinking in
unison with
the RUN
LIGHT
RAPID CYCLE:
The PumpSaver®Plus has shut
down on rapid cycling. Power
must be removed and reapplied
to reset the unit.
Check for a broken bladder in the
pressure tank (if used), or check
for a defective pressure or float
switch.
FHVSICAL DIMENSIONS
© 2015 SymCom, Inc. All Rights Reserved 9
PHYSICAL DIMENSIONS
4.05" (102.87)
5.26" (133.60)
4.50" (114.30)
.375"
(9.53)
2.93"
(74.42)
2.17"
(55.12)
2.90"
(73.66)
FRONT VIEW
BOTTOM VIEW
SPECIFICATIONS
© 2015 SymCom, Inc. All Rights Reserved 10
SPECIFICATIONS
Functional Specifications
Adjustments/Settings
Overcurrent
125% of calibration point
Underload (dry-well)
Adjustable (70-90% of calibrated run power)
Overvoltage
233P, 233P-1.5
265VAC
111P
132.5VAC
Undervoltage
233P, 233P-1.5
190VAC
111P
95VAC
Number of restarts allowed in 60
second period (rapid-cycling)
4
Trip Delay Times
Overcurrent
5 seconds
Dry-well
4 seconds
Dry-well Optional*
8 seconds
Restart Delay Times
Over/undervoltage
2 seconds
All other faults
Manual, 2-225 minutes
Input Characteristics
Supply Voltage
233P, 233P-1.5
230VAC
111P
115VAC
Load Range
233P
1/3 – 3 hp
233P-1.5
1/3 – 1.5 hp
111P
1/3 – 1 hp
Frequency
50/60Hz
(NOTE: 50Hz will increase all delay timers by 20%)
Output Characteristics
Output Contact Rating-SPST
233P
3hp @ 240VAC (17 Amps max.)
233P-1.5
1.5hp @ 240VAC (10 Amps max.)
111P
1hp @ 120VAC (16 Amps max.)
General Characteristics
Operating Temperature
-40° to 55°C (-40° to 131°F)
Maximum Input Power
5 W
Wire Gauge
Solid or stranded 10 – 22 AWG
Terminal Torque
13 in.-lbs.
Standards Passed
Electrostatic Discharge (ESD)
Surge Immunity
IEC 61000-4-2, Level 2, 4kV contact, 6kV air
IEC 61000-4-5, Level 4, 4kV line-to-line and line-to-
ground
Safety Marks
cUL Listed
UL508 & C22.2 No. 14
Dimensions
2.90” H x 5.26” W x 2.93” D
Weight
14 oz.
Mounting Methods
#8 screws
*use part number 233P-UCTD8
OTES
© 2015 SymCom, Inc. All Rights Reserved 11
NOTES
Visit us at www.5ymcom.com to see
© 2015 SymCom, Inc. All Rights Reserved 12
For warranty information, please see Terms and Conditions at
www.symcom.com
Visit us at www.symcom.com to see
our complete product listing!
Need something special?
Contact SymCom today
for your custom solution!
800-843-8848
Products related to this Datasheet
1-PHASE PUMPSAVERPLUS / 115 V
1-PHASE PUMPSAVERPLUS/ 230V/ 1
1-PHASE PUMPSAVERPLUS / 230V
1-PHASE PUMPSAVERPLUS / 230V
1-PHASE PUMPSAVERPLUS/230V/1/3