NetFPGA-SUME Get Started Guide Datasheet by Digilent, Inc.
View All Related Products | Download PDF Datasheet
Page 1 of 4
Getting Started Guide
Welcome to the NetFPGA-SUME getting started guide!
This guide is for new users. It covers:
• System Requirements.
• Downloading the code repository.
• Installation.
• Testing your board.
• What to do next!
Let's get started...
In principle, any operating system that is supported by the Xilinx Vivado Design Suite
should work for composing and synthesizing the IP in the code base. However, please
note that the NetFPGA team develops strictly on Linux. While hardware composition and
synthesis can be done on any platform which runs the Xilinx tools, software components
of the NetFPGA-SUME platform have been and will continue to be developed initially for
Linux. The Linux Operating System that NetFPGA team is using for development is
Ubuntu 14.04 (x86_64), and releases are tested only on this operating system. Special
care is needed for installing the driver on Linux Operating Systems. The Reference
Operating System page will provide you instructions about how to set up the development
system.
To do any development you will need the Xilinx Vivado Design Suite. Please note that
(until the SUME project is stable) the NetFPGA team strives to always use the latest
version of the tools, and we strongly advise all other developers to do the same. At the
time of writing, the version is Xilinx Vivado Design Suite 2014.4.
In order to build bitstreams, you must have a valid license for Xilinx 10G MAC.
The NetFPGA-SUME board has four SFP+ connectors for 10Gb Ethernet. The IP core
supports 10GBASE-SR/LR transceivers. The transceiver we used in development is
AVAGO AFBR-709SMZ with Multimode OM3 10Gb Fibre.
Section I: System Requirement
Operating Systems
Xilinx Tools
Xilinx IP Core License
Network Cables
Host Motherboard
Page 1 of 4
Page 2 of 4
The NetFPGA-SUME board works both standalone and inside a host. If you intend to use
the NetFPGA-SUME board in a host, you need to make sure that the motherboard
supports PCI Express Gen3 x8 configuration. It is recommended to have an up-to-date
firmware on your motherboard. For some motherboards, you may need to set the PCI
Express configuration to Gen3 in the BIOS configuration manually.
You need a micro-USB cable to access the JTAG chain or serial port of the reference
design. You can also use a Xilinx Platform Programming cable to access the JTAG chain
on board.
Prior to accessing code, we need you to register here. We do this to understand who is
using NetFPGA-SUME, so please give as complete answers as you can. The better
usage we can show, the more support we can motivate our sponsors to provide. Feel free
to explore the wiki, it is publicly readable.
Continue on from here once you have registered.
The code base for NetFPGA-SUME board is available as a git repository hosted on
GitHub.
After you have gained access to the repository, change into your desired directory and
execute the following command:
git clone git@github.com:NetFPGA/NetFPGASUMElive.git
For more information about git and GitHub in general, please consult GitHub help.
The NetFPGA-SUME package contains the following:
• NetFPGA-SUME board
• A micro-USB cable
• 4 unique MAC address stickers (one per 10G SFP+ Ethernet port)
Below is an image of the NetFPGA-SUME board, out of the box:
Other Stuff
Section II: Register to the Beta Program
Download the Code Base
Section III: NetFPGA-SUME Board Kit Content
Page 2 of 4
Page 3 of 4
The NetFPGA-SUME board is pre-configured with a manufacturing production test project.
The board can be powered up either in a stand alone mode or within a host. The following
instructions apply to both modes:
• Plug a PCI-E 2x3/2x4-pin power connector into the 2x4-pin PCI Express Auxiliary
Power receptacle (header J14)
• Connect the USB-JTAG port (J16, marked by a "USB JTAG" label) on NetFPGA-
SUME board to your PC with the micro-USB cable
• Turn on the power switch (SW1)
• You should see Power LED (LD10) and DONE LED (LD4) turn on immediately. This
is an indication of functioning power circuit and FPGA configuration circuit.
• Communicate with the board through hyper-terminal by opening the corresponding
serial port with a baud rate of 115200, 8 data bits, 1 stop bit, no parity checking, and
no flow control. An operating UART interface also indicates a functioning
programming interface. In the following image, minicom is used as the hyper-terminal
program in Linux to open the serial port /dev/ttyUSB1.
Section IV: NetFPGA-SUME First Power Up
Page 3 of 4
Ffl: Edn
Vlew Seam Termina| Help
Welcome to mlnlcom 2.6.2
OPTIONS:
Cnmpilnd an Jun 25 mm. m:
Ilfin
:21
Port ldev/ttyusfil, 17:38:22
Press CTRL»A z for help on special keys
NetFDGA-lGG-SUME Production Tnst
Reg
Reg
Reg
Reg
Reg
Reg
Reg
Reg
Re
Reg
https://git11ub.com/NetFPGA/NetFPGA-SUME-public/wiki/Getting-Starled-Guide
25:
31:
32:
33:
40:
41:
Q:
43:
44:
45:
m
NLHS = 0er
NCliLS
NCLLS
NCliLS
0x06
9x09
0x03
u l u
N27HSiL$ - excz
N2_HS_LS 0x49
N27H57LS - GxEF
N31 = 0x00
N31 0x77
N31 > 6x08
Page 4 of 4
3/31/2015
• The NetFPGA group is still working on an acceptance test project for users to fully
verify their boards with minimum amount of external test fixtures. We will update as
soon as we finalize the production test project. The new production test project will be
available at the NetFPGA-SUME-live repository.
Currently, there are no known issues. We are looking forward to your feedback after you
get the board. And we will populate this list as issues are reported along the way.
Section V: Known issues and Trouble Shoot
Status API Training Shop Blog About
Page 4 of 4
3
/
31
/
201
5
htt
p
s://
g
ithub.com/NetFPGA/NetFPG
A
-SUM
E
-
p
ublic/wiki/Gettin
g
-Starte
d
-Guid
e
Products related to this Datasheet
BOARD NETFPGA-SUME