ADIGILENT”
www dlgllentm com
Capynghl mm, In: All nghls mama
Other product and company names menlmned may be trademarks of the" respmm owners.
1300 Henley Court
Pullman, WA 99163
509.334.6306
www.digilentinc.com
Basys 2™ FPGA Board Reference Manual
Revised April 8, 2016
This manual applies to the Basys 2 rev. C
DOC#: 502-155
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 1 of 12
Overview
The Basys 2 board is a circuit design and implementation platform that anyone can use to gain experience building
real digital circuits. Built around a Xilinx Spartan-3E Field Programmable Gate Array and a Atmel AT90USB2 USB
controller, the Basys 2 board provides complete, ready-to-use hardware suitable for hosting circuits ranging from
basic logic devices to complex controllers. A large collection of on-board I/O devices and all required FPGA support
circuits are included, so countless designs can be created without the need for any other components.
Four standard expansion ports allow designs to grow beyond the Basys 2 board using breadboards, user-designed
circuit boards, or Pmods (Pmods are inexpensive analog and digital I/O modules that offer A/D & D/A conversion,
motor drivers, sensor inputs, and many other features). Signals on the 6-pin connectors are protected against ESD
damage and short-circuits, ensuring a long operating life in any environment. The Basys 2 board works seamlessly
with all versions of the Xilinx ISE tools, including the free WebPack. It ships with a USB cable that provides power
and a programming interface, so no other power supplies or programming cables are required.
The Basys 2 board can draw power and be programmed via its on-board USB2 port. Digilent’s freely available PC-
based Adept software automatically detects the Basys 2 board, provides a programming interface for the FPGA and
Platform Flash ROM, and allows user data transfers (see www.digilentinc.com for more information).
Xilinx Spartan3E-100 CP132
VGA Port
Platform
Flash
(config ROM)
Settable Clock
Source
(25 / 50 / 100 MHz)
Full Speed
USB2 Port
(JTAG and data transfers)
20
JA JB JC JD
JTAG
port
I/O Devices PS/2
Port Pmod Connectors
4444
8 bit
color
232
Data
port
Figure 1. The Basys 2 board block diagram and features.
100,000-gate Xilinx Spartan 3E FPGA
Atmel AT90USB2 Full-speed USB2 port
providing board power and programming/data
transfer interface
Xilinx Platform Flash ROM to store FPGA
configurations
8 LEDs, 4-digit 7-segment display, 4 buttons, 8
slide switches
PS/2 port and 8-bit VGA port
User-settable clock (25/50/100MHz), plus
socket for 2nd clock
Four 6-pin header expansion connectors
ESD and short-circuit protection on all I/O
signals.
Ca ynghl DrgHEnl, m: All nghls mama
www Ilrnx omlrsel.
Basys 2
m 9 product and camvany "am; mgnuangd may m lradgmarks al the" respetlwg owners
ADIGILENT'
USB
Connector
Battery
Connector
Power
Switch
Basys2™ FPGA Board Reference Manual
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 2 of 12
The Basys 2 board is designed to work with the free ISE WebPack CAD software from Xilinx. WebPack can be used
to define circuits using schematics or HDLs, to simulate and synthesize circuits, and to create programming files.
WebPack can be downloaded free of charge from www.xilinx.com/ise/.
The Basys 2 board ships with a built-in self-test/demo stored in its ROM that can be used to test all board features.
To run the test, set the Mode Jumper (see below) to ROM and apply board power. If the test is erased from the
ROM, it can be downloaded and reinstalled at any time. See Basys 2 for the test project as well as further
documentation, reference designs, and tutorials.
1 Board Power
The Basys 2 board is typically powered from a USB cable, but a battery
connector is also provided so that external supplies can be used. To use USB
power, simply attach the USB cable. To power the Basys 2 using a battery or
other external source, attach a 3.5V-5.5V battery pack (or other power
source) to the 2-pin, 100-mil spaced battery connector (three AA cells in
series make a good 4.5+/- volt supply). Voltages higher than 5.5V on either
power connector may cause permanent damage.
Input power is routed through the power switch (SW8) to the four 6-pin
expansion connectors and to a Linear Technology LTC3545 voltage
regulator. The LTC3545 produces the main 3.3V supply for the board, and it
also produces 2.5V and 1.2V supply voltages required by the FPGA. Total
board current is dependent on FPGA configuration, clock frequency, and
external connections. In test circuits with roughly 20K gates routed, a 50MHz clock source, and all LEDs
illuminated, about 100mA of current is drawn from the 1.2V supply, 50mA from the 2.5V supply, and 50mA from
the 3.3V supply. Required current will increase if larger circuits are configured in the FPGA, or if peripheral boards
are attached.
The Basys 2 board uses a four layer PCB, with the inner layers dedicated to VCC and GND planes. The FPGA and the
other ICs on the board have large complements of ceramic bypass capacitors placed as close as possible to each
VCC pin, resulting in a very clean, low-noise power supply.
2 Configuration
After power-on, the FPGA on the Basys 2 board must be configured before it can perform any useful functions.
During configuration, a “bit” file is transferred into memory cells within the FPGA to define the logical functions
and circuit interconnects. The free ISE/WebPack CAD software from Xilinx can be used to create bit files from
VHDL, Verilog, or schematic-based source files.
Digilent’s PC-based program called Adept can be used to configure the FPGA with any suitable bit file stored on the
computer. Adept uses the USB cable to transfer a selected bit file from the PC to the FPGA (via the FPGA’s JTAG
programming port). Adept can also program a bit file into an on-board non-volatile ROM called “Platform Flash”.
Once programmed, the Platform Flash can automatically transfer a stored bit file to the FPGA at a subsequent
power-on or reset event if the Mode Jumper (JP3) is set to ROM. The FPGA will remain configured until it is reset
by a power-cycle event. The Platform Flash ROM will retain a bit file until it is reprogrammed, regardless of power-
cycle events.
Figure 2. Basys 2 power circuits.
ADIGILENT'
n III-luv
. (Illa-dull] ,,
7. --
106
2 Socket
1 . ’1‘ ‘ o
. . »
ww glkey.com
Cu ynghl mguem, Inc. All um; mama
()1 er pmduu and company names menlmned may be trademarks 00 men respeclwg owners
Basys2™ FPGA Board Reference Manual
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 3 of 12
To program the Basys 2 board, set the mode jumper
to PC and attach the USB cable to the board. Start
the Adept software, and wait for the FPGA and the
Platform Flash ROM to be recognized. Use the
browse function to associate the desired .bit file
with the FPGA, and/or the desired .mcs file with the
Platform Flash ROM. Right-click on the device to be
programmed, and select the “program” function.
The configuration file will be sent to the FPGA or
Platform Flash, and the software will indicate
whether programming was successful. The “Status
LED” LED (LD_8) will also blink after the FPGA has
been successfully configured. For further
information on using Adept, please see the Adept
documentation available at the Digilent website.
3 Oscillators
The Basys 2 board includes a primary, user-settable silicon
oscillator that produces 25MHz, 50MHz, or 100MHz based
on the position of the clock select jumper at JP4. Initially,
this jumper is not loaded and must be soldered in place. A
socket for a second oscillator is provided at IC6 (the IC6
socket can accommodate any 3.3V CMOS oscillator in a half-
size DIP package). The primary and secondary oscillators are
connected to global clock input pins at pin B8 and pin M6
respectively.
Both clock inputs can drive the clock synthesizer DLL on the
Spartan 3E, allowing for a wide range if internal frequencies,
from 4 times the input frequency to any integer divisor of
the input frequency.
The primary silicon oscillator is flexible and inexpensive, but
it lacks the frequency stability of a crystal oscillator. Some
circuits that drive a VGA monitor may realize a slight
improvement in image stability by using a crystal oscillator
installed in the IC6 socket. For these applications, a 25MHz
(or 50MHz) crystal oscillator, available from any catalog
distributor, is recommended (see for example part number SG-8002JF-PCC at www.digikey.com ).
XCF02
Platform
Flash
JTAG
Spartan 3E
FPGA
Mode
Jumper
PC ROM
USB miniB
connector
Atmel
AT90USB2
Slave
serial
port
JTAG
port
LD8
Figure 4. Basys 2 Programming Circuits.
Spartan-3E
FPGA
B8 CLK_OUT
Linear Tech.
LTC6905
Oscillator
Frequency
Select
Jumper
25MHz
50MHz
100MHz
Figure 5. Basys 2 oscillator circuits.
ADIGILENT'
Cnfiynghl mguem, m: All nghls veserved
on av product and camvany names menuaned may be Uademarks al the" respetuve owners
Basys2™ FPGA Board Reference Manual
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 4 of 12
4 User I/O
Four pushbuttons and eight slide switches are provided for circuit inputs. Pushbutton inputs are normally low and
driven high only when the pushbutton is pressed. Slide switches generate constant high or low inputs depending
on position. Pushbuttons and slide switches all have series resistors for protection against short circuits (a short
circuit would occur if an FPGA pin assigned to a pushbutton or slide switch was inadvertently defined as an
output).
Eight LEDs and a four-digit seven-segment LED display are provided for circuit outputs. LED anodes are driven from
the FPGA via current-limiting resistors, so they will illuminate when a logic ‘1’ is written to the corresponding FPGA
pin. A ninth LED is provided as a power-indicator LED, and a tenth LED (LD-D) illuminates any time the FPGA has
been successfully programmed.
4.1 Seven-segment display
Each of the four digits of the seven-segment LED display is composed of seven LED segments arranged in a “figure
8” pattern. Segment LEDs can be individually illuminated, so any one of 128 patterns can be displayed on a digit by
illuminating certain LED segments and leaving the others dark. Of these 128 possible patterns, the ten
corresponding to the decimal digits are the most useful.
The anodes of the seven LEDs forming each digit are tied together into one common anode circuit node, but the
LED cathodes remain separate. The common anode signals are available as four “digit enable” input signals to the
4-digit display. The cathodes of similar segments on all four displays are connected into seven circuit nodes labeled
CA through CG (so, for example, the four “D” cathodes from the four digits are grouped together into a single
circuit node called “CD”). These seven cathode signals are available as inputs to the 4-digit display. This signal
connection scheme creates a multiplexed display, where the cathode signals are common to all digits but they can
only illuminate the segments of the digit whose corresponding anode signal is asserted.
A scanning display controller circuit can be used to show a four-digit number on this display. This circuit drives the
anode signals and corresponding cathode patterns of each digit in a repeating, continuous succession, at an update
rate that is faster than the human eye response. Each digit is illuminated just one-quarter of the time, but because
the eye cannot perceive the darkening of a digit before it is illuminated again, the digit appears continuously
illuminated. If the update or “refresh” rate is slowed to a given point (around 45 hertz), then most people will
begin to see the display flicker.
ADIGILENT'
l :l :l
-1
l L.
Ll l‘ I:
l .1 LI
_I III 1:!
l Ll _l
| | | 1 fl!
DUDE 1
1_ .1.1. 1.1.1.1. ; ’
Cnfiynghl D1g11enl,\n: All "gm; veserved
on e1 product and company names menuaneu may be Uademarks a! the" respetlwe owners
Basys2™ FPGA Board Reference Manual
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 5 of 12
For each of the four digits to appear bright and continuously illuminated, all four digits should be driven once every
1 to 16ms (for a refresh frequency of 1KHz to
60Hz). For example, in a 60Hz refresh scheme,
the entire display would be refreshed once every
16ms, and each digit would be illuminated for ¼
of the refresh cycle, or 4ms. The controller must
assure that the correct cathode pattern is
present when the corresponding anode signal is
driven. To illustrate the process, if AN1 is
asserted while CB and CC are asserted, then a
“1” will be displayed in digit position 1. Then, if
AN2 is asserted while CA, CB and CC are
asserted, then a “7” will be displayed in digit
position 2. If A1 and CB, CC are driven for 4ms, and then A2 and CA, CB, CC are driven for 4ms in an endless
succession, the display will show “17” in the first two digits. Figure 8 shows an example timing diagram for a four-
digit seven-segment controller.
5 PS/2 Port
The 6-pin mini-DIN connector can accommodate a PS/2 mouse or keyboard. The PS/2 connector is supplied with
5VDC.
Both the mouse and keyboard use a two-wire serial bus (clock and data) to communicate with a host device. Both
use 11-bit words that include a start, stop and odd parity bit, but the data packets are organized differently, and
the keyboard interface allows bi-directional data transfers (so the host device can illuminate state LEDs on the
keyboard). Bus timings are shown in the figure.
The clock and data signals are only driven when data transfers occur, and otherwise they are held in the “idle”
state at logic ‘1’. The timings define signal requirements for mouse-to-host communications and bi-directional
keyboard communications. A PS/2 interface circuit can be implemented in the FPGA to create a keyboard or
mouse interface.
AN0
AN1
AN2
AN3
Cathodes Digit 0
Refresh period = 1ms to 16ms
Digit period = Refresh / 4
Digit 1 Digit 2 Digit 3
Figure 8. Multiplexed 7seg display timing.
A
F
E
D
C
B
G
Common anode
Individual cathodes
DP
AN1 AN2 AN3 AN4
CA CB CC CD CE CF CG DP
Four-digit Seven
Segment Display
An un-illuminated seven-segment display, and nine
illumination patterns corresponding to decimal digits
Figure 7. Seven-segment display.
ADIGILENT'
Ca ynghl mguem, In: All nghls mama
()1 er pmducl and company names menlmned may be trademarks 00 men respeclwg owners
Basys2™ FPGA Board Reference Manual
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 6 of 12
5.1 Keyboard
The keyboard uses open-collector drivers so the keyboard or an
attached host device can drive the two-wire bus (if the host
device will not send data to the keyboard, then the host can use
input-only ports).
PS2-style keyboards use scan codes to communicate key press
data. Each key is assigned a code that is sent whenever the key
is pressed; if the key is held down, the scan code will be sent
repeatedly about once every 100ms. When a key is released, a
“F0” key-up code is sent, followed by the scan code of the
released key. If a key can be “shifted” to produce a new character (like a capital letter), then a shift character is
sent in addition to the scan code, and the host must determine which ASCII character to use. Some keys, called
extended keys, send an “E0” ahead of the scan code (and they may send more than one scan code). When an
extended key is released, an “E0 F0” key-up code is sent, followed by the scan code. Scan codes for most keys are
shown in the figure. A host device can also send data to the keyboard. Below is a short list of some common
commands a host might send.
ED Set Num Lock, Caps Lock, and Scroll Lock LEDs. Keyboard returns “FA” after receiving “ED”, then host
sends a byte to set LED status: Bit 0 sets Scroll Lock; bit 1 sets Num Lock; and Bit 2 sets Caps lock. Bits 3 to
7 are ignored.
EE Echo (test). Keyboard returns “EE” after receiving “EE”.
F3 Set scan code repeat rate. Keyboard returns “F3” on receiving “FA”, then host sends second byte to set
the repeat rate.
FE Resend. “FE” directs keyboard to re-send most recent scan code.
FF Reset. Resets the keyboard.
The keyboard can send data to the host only when both the data and clock lines are high (or idle). Since the host is
the “bus master”, the keyboard must check to see whether the host is sending data before driving the bus. To
facilitate this, the clock line is used as a “clear to send” signal. If the host pulls the clock line low, the keyboard
must not send any data until the clock is released.
TCK
TSU
Clock time
Data-to-clock setup time
30us
5us
50us
25us
Symbol Parameter Min Max
THLD Clock-to-data hold time 5us 25us
Edge 0
‘0’ start bit ‘1’ stop bit
Edge 10
Tsu
Thld
Tck Tck
Figure 10. PS/2 signal timing
Pin1: Data
Pin2: Data
Pin3: GND
Pin5: Vdd
Pin6: Clock
Pin8: Clock
2 1 35
8 6
1
3
6
2
5
8
(bottom up)
B1
Spartan 3E
FPGA
CLK
DATA
6-pin
mini-DIN
C3
200 W
200 W
Figure 9. PS/2 connector and Basys 2 PS/2 circuit.
ADIGILENT'
HHHHHHHHHHHHHHHHHHHHHHHHHHT
U
HH HH HH HH HH HH HH HH HH HH HH HH HF FH
HH HH HH HH HH HH HH HH HH HH HH HH HH
H H
H
HH HH HH HH HH HH HH HH HH HH HH HH HE]
H H
‘7
HH HH HH HH HH HH HH HH HH HH H0
Cegvmgm DHZHHEM, Hnr AHH rights reserved
0: er product and mmpany names mennaned may he maemam cl men respernve awners
Basys2™ FPGA Board Reference Manual
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 7 of 12
The keyboard sends data to the host in 11-bit words that contain a ‘0’ start bit, followed by 8-bits of scan code (LSB
first), followed by an odd parity bit and terminated with a ‘1’ stop bit. The keyboard generates 11 clock transitions
(at around 20 - 30KHz) when the data is sent, and data is valid on the falling edge of the clock.
5.2 Mouse
The mouse outputs a clock and data signal when it is moved; otherwise, these signals remain at logic ‘1’. Each time
the mouse is moved, three 11-bit words are sent from the mouse to the host device. Each of the 11-bit words
contains a ‘0’ start bit, followed by 8 bits of data (LSB first), followed by an odd parity bit, and terminated with a ‘1’
stop bit. Thus, each data transmission contains 33 bits, where bits 0, 11, and 22 are ‘0’ start bits, and bits 11, 21,
and 33 are ‘1’ stop bits. The three 8-bit data fields contain movement data as shown in the figure above. Data is
valid at the falling edge of the clock, and the clock period is 20 to 30KHz.
The mouse assumes a relative coordinate system wherein moving the mouse to the right generates a positive
number in the X field, and moving to the left generates a negative number. Likewise, moving the mouse up
generates a positive number in the Y field, and moving down represents a negative number (the XS and YS bits in
the status byte are the sign bits – a ‘1’ indicates a negative number). The magnitude of the X and Y numbers
represent the rate of mouse movement – the larger the number, the faster the mouse is moving (the XV and YV
bits in the status byte are movement overflow indicators – a ‘1’ means overflow has occurred). If the mouse moves
continuously, the 33-bit transmissions are repeated every 50ms or so. The L and R fields in the status byte indicate
Left and Right button presses (a ‘1’ indicates the button is being pressed).
ESC
76
` ~
0E
TAB
0D
Caps Lock
58
Shift
12
Ctrl
14
1 !
16 2 @
1E 3 #
26 4 $
25 5 %
2E
Q
15 W
1D E
24 R
2D T
2C
A
1C S
1B D
23 F
2B G
34
Z
1Z X
22 C
21 V
2A B
32
6 ^
36 7 &
3D 8 *
3E 9 (
46 0 )
45 - _
4E = +
55 BackSpace
66
Y
35 U
3C I
43 O
44 P
4D [ {
54 ] }
5B \ |
5D
H
33 J
3B K
42 L
4B ; :
4C ' "
52 Enter
5A
N
31 M
3A , <
41 > .
49 / ?
4A Shift
59
Alt
11 Space
29 Alt
E0 11 Ctrl
E0 14
F1
05 F2
06 F3
04 F4
0C F5
03 F6
0B F7
83 F8
0A F9
01 F10
09 F11
78 F12
07 E0 75
E0 74
E0 6B
E0 72
Figure 11. Keyboard scan codes.
L R 0 1 XS YS XY YY P X0 X1 X2 X3 X4 X5 X6 X7 P Y0 Y1 Y2 Y3 Y4 Y5 Y6 Y7 P1 0 1 00 11
Idle state Start bit
Mouse status byte X direction byte Y direction byte
Stop bit Start bit Stop bit
Idle state
Stop bit Start bit
Figure 12. Mouse data format.
ADIGILENT'
Ca ynghl mguem, In: All nghls mama
m er pmducl and company names menlmned may be lrademzrks 00 men respeclwg owners
Basys2™ FPGA Board Reference Manual
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 8 of 12
6 VGA Port
The Basys 2 board uses 10 FPGA signals to create a VGA port with 8-bit color and the two standard sync signals (HS
– Horizontal Sync, and VS – Vertical Sync). The color signals use resistor-divider circuits that work in conjunction
with the 75-ohm termination resistance of the VGA display to create eight signal levels on the red and green VGA
signals, and four on blue (the human eye is less sensitive to blue levels). This circuit, shown in figure 13, produces
video color signals that proceed in equal increments between 0V (fully off) and 0.7V (fully on). A video controller
circuit must be created in the FPGA to drive the sync and color signals with the correct timing in order to produce a
working display system.
6.2 VGA System Timing
VGA signal timings are specified, published, copyrighted and sold by the VESA organization (www.vesa.org). The
following VGA system timing information is provided as an example of how a VGA monitor might be driven in 640
by 480 mode. For more precise information, or for information on other VGA frequencies, refer to documentation
available at the VESA website.
CRT-based VGA displays use amplitude-modulated moving electron beams (or cathode rays) to display information
on a phosphor-coated screen. LCD displays use an array of switches that can impose a voltage across a small
amount of liquid crystal, thereby changing light permittivity through the crystal on a pixel-by-pixel basis. Although
the following description is limited to CRT displays, LCD displays have evolved to use the same signal timings as
CRT displays (so the “signals” discussion below pertains
to both CRTs and LCDs). Color CRT displays use three
electron beams (one for red, one for blue, and one for
green) to energize the phosphor that coats the inner
side of the display end of a cathode ray tube (see
illustration). Electron beams emanate from “electron
guns” which are finely-pointed heated cathodes placed
in close proximity to a positively charged annular plate
called a “grid”. The electrostatic force imposed by the
grid pulls rays of energized electrons from the
cathodes, and those rays are fed by the current that
flows into the cathodes. These particle rays are initially
accelerated towards the grid, but they soon fall under
the influence of the much larger electrostatic force
that results from the entire phosphor-coated display
surface of the CRT being charged to 20kV (or more).
The rays are focused to a fine beam as they pass
through the center of the grids, and then they accelerate to impact on the phosphor-coated display surface. The
phosphor surface glows brightly at the impact point, and it continues to glow for several hundred microseconds
after the beam is removed. The larger the current fed into the cathode, the brighter the phosphor will glow.
Between the grid and the display surface, the beam passes through the neck of the CRT where two coils of wire
produce orthogonal electromagnetic fields. Because cathode rays are composed of charged particles (electrons),
they can be deflected by these magnetic fields. Current waveforms are passed through the coils to produce
magnetic fields that interact with the cathode rays and cause them to transverse the display surface in a “raster”
pattern, horizontally from left to right and vertically from top to bottom. As the cathode ray moves over the
surface of the display, the current sent to the electron guns can be increased or decreased to change the
brightness of the display at the cathode ray impact point.
Anode (entire screen)
High voltage
supply (>20kV)
Deflection coils
Grid Electron guns
(Red, Blue, Green)
gun
control
grid
control
deflection
control
R,G,B signals
(to guns)
Cathode ray tube
Cathode ray
VGA
cable
Figure 14. CRT deflection system
Com/mam Dwenl, m AH "9mm reserved
ADIGILENT'
Omar product and tampanv names mennaned may he maemam or men respecnve Owner:
Basys2™ FPGA Board Reference Manual
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 9 of 12
Information is only displayed when the beam is moving in the “forward” direction (left to right and top to bottom),
and not during the time the beam is reset back to the left or top edge of the display. Much of the potential display
time is therefore lost in “blanking” periods when the beam is reset and stabilized to begin a new horizontal or
vertical display pass. The size of the beams, the frequency at which the beam can be traced across the display, and
the frequency at which the electron beam can be modulated determine the display resolution. Modern VGA
displays can accommodate different
resolutions, and a VGA controller circuit
dictates the resolution by producing timing
signals to control the raster patterns. The
controller must produce synchronizing pulses
at 3.3V (or 5V) to set the frequency at which
current flows through the deflection coils, and
it must ensure that video data is applied to
the electron guns at the correct time. Raster
video displays define a number of “rows” that
corresponds to the number of horizontal
passes the cathode makes over the display
area, and a number of “columns” that
corresponds to an area on each row that is
assigned to one “picture element” or pixel.
Typical displays use from 240 to 1200 rows
and from 320 to 1600 columns. The overall
size of a display and the number of rows and
columns determines the size of each pixel.
Video data typically comes from a video
refresh memory, with one or more bytes
assigned to each pixel location (the Basys 2
uses three bits per pixel). The controller must
index into video memory as the beams move
across the display, and retrieve and apply
video data to the display at precisely the time
the electron beam is moving across a given pixel.
A VGA controller circuit must generate the HS and VS
timings signals and coordinate the delivery of video
data based on the pixel clock. The pixel clock defines
the time available to display one pixel of
information. The VS signal defines the “refresh”
frequency of the display, or the frequency at which
all information on the display is redrawn. The
minimum refresh frequency is a function of the
display’s phosphor and electron beam intensity, with
practical refresh frequencies falling in the 50Hz to
120Hz range. The number of lines to be displayed at
a given refresh frequency defines the horizontal
“retrace” frequency. For a 640-pixel by 480-row
display using a 25MHz pixel clock and 60 +/-1Hz
refresh, the signal timings shown in the table at right
Current
waveform
through
horizontal
defletion
coil
Stable current ramp - information
is displayed during this time
Retrace - no
information
displayed
during this
time
Total horizontal time
Horizontal display time
Horizontal sync signal
sets retrace frequency
retrace
time
time
HS
"back porch""front porch"
Display Surface
640 pixels per row are displayed
during forward beam trace
pixel 0,639
pixel 0,0
pixel 479,0 pixel 479,639
Figure 15. VGA system signals.
TS
Tdisp
Tpw
Tfp
Tbp
TS
Tdisp
Tpw
Tfp
Tbp
Sync pulse
Display time
Pulse width
Front porch
Back porch
16.7ms
15.36ms
64 us
320 us
928 us
416,800
384,000
1,600
8,000
23,200
521
480
2
10
29
Symbol Parameter Time Clocks Lines
Vertical Sync
32 us
25.6 us
3.84 us
640 ns
1.92 us
800
640
96
16
48
Clks
Horiz. Sync
Time
Figure 16. VGA system timings for 640x480 display
ADIGILENT'
www Igllentlnc om
Cu ynghl mguem, Inc. All um; mama
()1 er pmduu and company names menlmned may be trademarks 00 men respeclwg owners
Basys2™ FPGA Board Reference Manual
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 10 of 12
can be derived. Timings for sync pulse width and front and back porch intervals (porch intervals are the pre- and
post-sync pulse times during which information cannot be displayed) are based on observations taken from actual
VGA displays.
A VGA controller circuit decodes the output of a horizontal-sync counter driven by the pixel clock to generate HS
signal timings. This counter can be used to locate any pixel location on a given row. Likewise, the output of a
vertical-sync counter that increments with each HS pulse can be used to generate VS signal timings, and this
counter can be used to locate any given row. These two continually running counters can be used to form an
address into video RAM. No time relationship between the onset of the HS pulse and the onset of the VS pulse is
specified, so the designer can arrange the counters to easily form video RAM addresses, or to minimize decoding
logic for sync pulse generation.
7 Expansion Connectors (6-pin Headers)
The Basys 2 board provides four 6-pin peripheral module connectors. Each connector provides Vdd, GND, and four
unique FPGA signals. Several 6-pin module boards that can attach to this connector are available from Digilent,
including A/D converters, speaker amplifiers, microphones, H-bridge amplifiers, etc. Please see
www.digilentinc.com for more information.
Spartan 3E
FPGA
B2
A3
J3
B5
ESD protection
diodes
1
6-pin
header
2
3
4
5
6
JA
Short-circuit protection
resistors
3.3V
16-pin
header
2
3
4JB
16-pin
header
2
3
4JC
16-pin
header
2
3
4JD
C6
B6
C5
B7
A9
B9
A10
C9
C12
A13
C13
D12
Figure 18. Basys 2 Pmod port circuits.
ADIGILENT’
Ca rlgm Dlgllem m. Allriums msewed
er pmdun and company names memvmed may be "3.1mm: ohhelrrespemve owners
Basys2™ FPGA Board Reference Manual
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 11 of 12
8 FPGA Pin Definitions
The table below shows all pin definitions for the Spartan-3E on the Basys 2 board. Pins in grey boxes are not
available to the user.
FPGA pin definition table color key
Grey
Not available to user
Green
User I/O devices
Yellow
Data ports
Tan
Pmod port signals
Blue
USB signals
Basys 2 Spartan-3E pin definitions
Pin
Signal
Pin
Signal
Pin
Signal
Pin
Signal
Pin
Signal
Pin
Signal
C12
JD1
P11
SW0
N14
CC
B2
JA1
P8
MODE0
M7
GND
A13
JD2
M2
USB-DB1
N13
DP
C2
USB-WRITE
N7
MODE1
P5
GND
A12
NC
N2
USB-DB0
M13
AN2
C3
PS2D
N6
MODE2
P10
GND
B12
NC
M9
NC
M12
CG
D1
NC
N12
CCLK
P14
GND
B11
NC
N9
NC
L14
CA
D2
USB-WAIT
P13
DONE
A6
VDDO-3
C11
BTN1
M10
NC
L13
CF
L2
USB-DB4
A1
PROG
B10
VDDO-3
C6
JB1
N10
NC
F13
RED2
L1
USB-DB3
N8
DIN
E13
VDDO-3
B6
JB2
M11
LD1
F14
GRN0
M1
USB-DB2
N1
INIT
M14
VDDO-3
C5
JB3
N11
CD
D12
JD4
L3
SW1
P1
NC
P3
VDDO-3
B5
JA4
P12
CE
D13
RED1
E2
SW6
B3
GND
M8
VDDO-3
C4
NC
N3
SW7
C13
JD3
F3
SW5
A4
GND
E1
VDDO-3
B4
SW3
M6
UCLK
C14
RED0
F2
USB-ASTB
A8
GND
J2
VDDO-3
A3
JA2
P6
LD3
G12
BTN0
F1
USB-DSTB
C1
GND
A5
VDDO-2
A10
JC3
P7
LD2
K14
AN3
G1
LD7
C7
GND
E12
VDDO-2
C9
JC4
M4
BTN2
J12
AN1
G3
SW4
C10
GND
K1
VDDO-2
B9
JC2
N4
LD5
J13
BLU2
H1
USB-DB6
E3
GND
P9
VDDO-2
A9
JC1
M5
LD0
J14
HSYNC
H2
USB-DB5
E14
GND
A11
VDDO-1
B8
MCLK
N5
LD4
H13
BLU1
H3
USB-DB7
G2
GND
D3
VDDO-1
C8
RCCLK
G14
GRN2
H12
CB
B14
TMS
H14
GND
D14
VDDO-1
A7
BTN3
G13
GRN1
J3
JA3
B13
TCK-FPGA
J1
GND
K2
VDDO-1
B7
JB4
F12
AN0
K3
SW2
A2
TDO-USB
K12
GND
L12
VDDO-1
P4
LD6
K13
VSYNC
B1
PS2C
A14
TDO-S3
M3
GND
P2
VDDO-1
9 Built-In Self Test
The Basys 2 board comes preloaded with a simple self test/demonstration project stored in its ROM. The demo
project (available at the website) shows how the Xilinx CAD tools connect FPGA signals to Basys 2 circuits. Since the
project is stored in ROM, it can also be used to check board functions. To run the demo, set the ROM/USB jumper
(JP3) to ROM and apply power to the board; the seven-segment display will show counting digits, the switches will
turn on individual LEDs, the buttons will turn off individual digits on the seven segment display, and a test pattern
is driven on the VGA port.
ADIGILENT'
Cnfiynghl mguem, m: All nghls veserved
on av product and camvany names menuaned may be Uademarks al the" respetuve owners
Basys2™ FPGA Board Reference Manual
Copyright Digilent, Inc. All rights reserved.
Other product and company names mentioned may be trademarks of their respective owners.
Page 12 of 12
If the self test is not resident in the Platform Flash ROM, it can be programmed into the FPGA or reloaded into the
ROM using the Adept programming software.
Products related to this Datasheet
BOARD BASYS2 FOR SPARTAN-3E
KIT BASYS2-250 SPARTAN-3E 250K