SI4831/35 Datasheet by Silicon Labs

View All Related Products | Download PDF Datasheet
$9 SILIEflNVLABS
Rev. 0.1 4/11 Copyright © 2011 by Silicon Laboratories Si4831/35 FAQ
Si4831/35 AM/FM/SW TUNER
FREQUENTLY ASKED QUESTIONS
Rev. 0.1 4/11 Copyright © 2011 by Silicon Laboratories Si4831/35 FAQ
G? SllIEflN/LAHS
Rev. 0.1 4/11 Copyright © 2011 by Silicon Laboratories Si4831/35 FAQ
Si4831/35 FAQ
SI4831/35 AM/FM/SW TUNER—FREQUENTLY ASKED QUESTIONS
Table of Contents
What's the advantage of using PVR tuning instead of PVC? . . . . . . . . . . . . . . . . . . . . . . . . . . 4
PVR tuning stable under different environmental conditions? . . . . . . . . . . . . . . . . . . . . . . . . . 5
What do I need to change on the appearance of my existing model if using Si4831/35? . . . . 6
How is the tuning feel of PVR with Si4831/35, is it easy to tune exactly to a station? . . . . . . . 6
How is the frequency display accuracy of Si4831/35 PVR tuning
compared with PVC tuning? . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6
Why are some of my Si4831/35 models occasionally unable to power up
after quick power off/on cycles? . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7
Why is the measured SNR and Sensitivity often better when using an audio analyzer
than when using a multimeter? 9
If my application is mono audio, how should I use Si4831/35? . . . . . . . . . . . . . . . . . . . . . . . . 9
When switching on the power supply, there is a small but audible power on pop noise.
How can this pop noise be mitigated? . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9
Why is the narrow FM AFC range not a problem in the Si4831/35? . . . . . . . . . . . . . . . . . . . 10
How do I minimize the frequency display position hysteresis with PVR tuning? . . . . . . . . . . 10
Q35" SILIEIJNUIIS
Si4831/35 FAQ
4 Rev. 0.1
Q: What's the advantage of using PVR tuning instead of PVC?
Keyword(s): PVR, PVC, resistance ratio
Device(s): Si4831/35
HW Rev(s): All
A: PVR tuning has the following advantages compared with PVC tuning:
1. Cost saving
Material cost: PVR is $0.05 vs. PVC for $0.12 for the same quantity and quality
Labor cost
2. Reliable life time and endurance (test proven) is better than PVC
Test Method: 100,000 PVR full range rotations
SINAD, SNR, sensitivity at three frequency points remain unchanged before and after rotation test
PVR value and the frequency display mark stay within spec:
After 10K times rotations, PVR value stays the same, frequency/display alignment unchanged
After 100K times rotations, PVR value changes less than10%, no visible change to frequency/display
alignment. This is because Si4831/35 uses resistance ratio, not the absolute resistance value, for tuning
to ensure display accuracy
Figure 1. PVR Resistance Ratio
FM Test
Points(MHz)
Before Test After Test
SINAD
(dB) S/N (dB) Sensitivity
(dBµV) SINAD
(dB) S/N (dB) Sensitivity
(dBµV)
88.1 57 58 2 57 58 2
98.1 57 58 2 57 58 2
107.9 56 57 3 56 57 3
e" SILIEIJN’lAES
Si4831/35 FAQ
Rev. 0.1 5
Q: PVR tuning stable under different environmental conditions?
Keyword(s): PVR tuning, environmental conditions
Device(s): Si4831/35
HW Rev(s): All
A. Yes, PVR tuning frequency stays stable at various conditions while PVC tuning frequency drifts. Reliability
test results proved the following:
Testing platform: Si4835-DEMO with R121 PVR and Sony clock radio ICF-C218 with PVC
Tuned frequency is determined at maximum SINAD and S/N point
Tests Settings Si4831/35 PVR SONY–ICF-C218 PVC
Hot temp / Humidity
Room(start) 98.1 MHz 98.1 MHz
T:45 °C,H:80% 98.1 MHz 98.14 MHz
Room(end) 98.1 MHz 98.1 MHz
Cold
Room(start) 98.1 MHz 98.1 MHz
T:1C 98.1MHz 98.17MHz
Room(end) 98.1 MHz 98.17 MHz
Long term high temp / humidity
(T = 60° C/H = 90%/100 Hour)
Room(start) 98.1 MHz 98.1 MHz
Room(end) 98.1 MHz 98.28 MHz
Short term high temp /humidity
(T = 60° C/H = 80%/6 Hour)
Room(start) 98.1 MHz 98.1 MHz
Room(end) 98.1 MHz 97.98 MHz
Short term cold
(T = –25° C/6 Hour)
Room(start) 98.1 MHz 98.1 MHz
Room(end) 98.1 MHz 98.1 MHz
Hot /cold cycle test
(T = 70° C/T = –10° C/5 cycles)
Room(start) 98.1 MHz 98.1 MHz
Room(end) 98.1 MHz 98.06 MHz
Traditional PVC non-linear frequency display (:3 Ioé I I ‘93 ea 93 98 103 we MHz F"? ‘05 SmBBl/BS PVR linear frequency display ‘93 103' 88 93 98 103 108 MHZ I58 Mix Q35" SIlIEIJN lAflS
Si4831/35 FAQ
6 Rev. 0.1
Q: What do I need to change on the appearance of my existing model if using Si4831/35?
Keyword(s): Existing model
Device(s): Si4831/35
HW Rev(s): All
A. The traditional PVC frequency display is non-linear; however, the Si4831/35's advanced tuning algorithm
makes the tuned frequency linear with the PVR turning angle, so Si4831/35 offers more accuracy to estimate
the frequency from the analog display marking. To use Si4831/35 for existing PVC models, you only need to
change the frequency marking and make it linear.
Figure 2. PVC PVR Frequency Display
Q: How is the tuning feel of PVR with Si4831/35, is it easy to tune exactly to a station?
Keyword(s): Tuning feel
Device(s): Si4831/35
HW Rev(s): All
A: Compared with Si4830/34-A20, the Si4831/35 uses a new tuning algorithm that allows the user to hear one
station across a larger frequency range. At the same time, the user can easily feel or tell if the tuned position is
the best by the sound. The new tuning algorithm was added to improve the tuning feel and has been well
received in the marketplace. The algorithm was carefully optimized such that selectivity was not compromised;
therefore, weak station is still easy to tune.
Q: How is the frequency display accuracy of Si4831/35 PVR tuning compared with PVC tuning?
Keyword(s): Frequency display accuracy
Device(s): Si4831/35
HW Rev(s): All
A: Si4831/35 PVR tuning frequency display accuracy is not any worse than traditional analog radios. The
tuning position inaccuracy has most to do with the PVR itself, but this is not unique to PVR. PVC will also have
some position inaccuracy. Traditional PVC tuning analog radio has a much more severe tuned position drifting
problem than Si4831/35, and for a longer term. PVR tuning position accuracy of the Si4831/35 is better; refer
to the second question for more information.
"i R—ST Q3" SILIEIJNUIIS
Si4831/35 FAQ
Rev. 0.1 7
Q: Why are some of my Si4831/35 models occasionally unable to power up after quick power off/on
cycles?
Keyword(s): Power off/on cycles, power up, reset, reset pulse
Device(s): Si4831/35
HW Rev(s): All
A: Sometimes, when the power switch is turned off/on quickly, or the power plug is plugged in/out quickly, the
Si4831/35 can't be powered up properly and it can't go into normal working mode. The reason for this is that,
during this type of fast power off/on process, the chip occasionally is not reset properly.
Si4831/35 is digital in nature—an MCU and a DSP are integrated inside the chip. To power up properly, the
chip needs a proper negative reset pulse during the quick power off/on cycle. As shown in Figure 3, the
needed pulse width of tSRST is several ms. Because there are large filtering capacitors in the power supply
circuit, the dc supply voltage VCC to tuner is still present (even though the main plug is disconnected) and falls
down slowly. Accordingly, the RST pin voltage falls down slowly, so there is no needed reset pulse generated.
Figure 5 shows a typical VCC and RST voltage change curve during a power off /on cycle. In this case, the RST
voltage level doesn't drop below 0.3 VCC, so the chip is not reset properly and can't be powered up and go into
normal working mode.
Figure 3. Reset Pulse for Si4831/35
Figure 4. RC Reset Circuit of Si4831/35
70%
30%
tSRST
RST
GND
GND
13
14
15
C19
0.1µ
VCC
RST
R6
100k
VOUT I: VAX-12mm Am pm mv Nomi] x v ; v1 «1 mw o‘zvnzwl "J oz apnmam Cap Vame , \‘ aosu :I VIN R42 “(7 : CONTROL Q3} SILIEIJNUIIS
Si4831/35 FAQ
8 Rev. 0.1
Figure 5. VCC (green) and RST (yellow) Change During Power Off
Figure 6. Typical Power Supply Circuit
Figure 6 shows the typical power supply circuit of a tuner; the solution to the power up issue is:
1. Add a discharge resistor at the output of tuner power supply to speed up the discharge process when the power is
off.
2. Optimize the filtering caps capacity to a small value. Si4831/35 consumes only around 20 mA current in normal
working mode, so the power supply circuits do not need to contain a large value of filtering caps; normally, no
more than 47 µF is recommended.
Q3" SILIEIJNUIIS
Si4831/35 FAQ
Rev. 0.1 9
Q: Why is the measured SNR and Sensitivity often better when using an audio analyzer than when using
a multimeter?
Keyword(s): Audio analyzer, multimeter, SNR, Sensitivity
Device(s): Si4831/35
HW Rev(s): All
A: Normally, there are two kinds of instruments used for measuring SNR and Sensitivity: one is a professional
audio analyzer and another is a multimeter or voltmeter, which can be a traditional needle display type or more
modern digital display type. The voltmeter is low cost and is widely used by many audio customers. A typical
voltmeter model is TVT-322.
Using the audio analyzer, the measured SNR and sensitivity is normally better than when using a voltmeter for
the following reasons:
1. The frequency bandwidth of an audio analyzer is narrower than a voltmeter’s bandwidth. Audio analyzer
bandwidth is normally up to 22 kHz; this is the real audio signal bandwidth. For the voltmeter, the frequency
bandwidth is much wider, and different models have different bandwidths, normally above 200 kHz. For the TVT-
322, the bandwidth is up to 1 MHz. Because of the wider frequency bandwidth, the voltmeter always measures a
higher noise level than the audio analyzer and therefore has a lower SNR value and Sensitivity value. But for true
audio measurement, the noise level above 22 kHz should not be counted as it is beyond the human ear frequency
audible range.
2. The audio analyzer is a more advanced instrument than the voltmeter; it can measure signal level and noise level
at the same time, and can directly calculate SNR data. For the voltmeter, SNR data can only be obtained by first
turning on modulation to get the signal level, then turning off modulation to get the noise level, and then calculating
SNR data as the delta. So for the voltmeter, the measured signal level and noise level do not occur at the same
time, hence it is not a true SNR measurement.
Q: If my application is mono audio, how should I use Si4831/35?
Keyword(s): Mono Audio, Stereo Audio
Device(s): Si4831/35
HW Rev(s): All
A: The Si4831/35 is a stereo audio tuner with two stereo thresholds: 20 dBµV and 28 dBµV. When the input RF
level is below the selected stereo threshold, the chip outputs mono audio. When the input RF signal is above
the selected stereo threshold, it automatically outputs stereo audio. The following measures are recommended
for mono audio applications:
1. Choose the wanted FM band with stereo indication threshold of 28 dBµV.
2. Connect Lout and Rout together right after the AC coupling capacitors of 4.7 µF.
Q: When switching on the power supply, there is a small but audible power on pop noise. How can this
pop noise be mitigated?
Keyword(s): Pop noise
Device(s): Si4831/35
HW Rev(s): All
A. Compared with Si4830/34-A20, the Si4831/35 has greatly reduced the power on pop noise. To further
migrate the pop noise, the following measures are recommended:
1. The ac coupling capacitors in series with Lout and Rout of Si4831/35 must be no less than 4.7uF.
2. Normally, there is a large power supply filtering capacitor at the power supply of audio AMP, put the capacitor as
close to the power supply pin of audio AMP as possible, and give this capacitor a large value, so that at power up,
audio AMP starts up more slowly than Si4831/35, this will make the power on pop noise smaller.
3. To completely remove the power on pop noise, adding a transistor + E-cap muting circuit as shown in Figure 7 to
Lout and Rout of Si4831/35 respectively.
Q35" SILIEIJNUIIS
Si4831/35 FAQ
10 Rev. 0.1
Figure 7. Power On Pop Noise Muting Circuit
Q: Why is the narrow FM AFC range not a problem in the Si4831/35?
Keyword(s): AFC Range, Traditional Analog FM tuner, Selectivity
Device(s): Si4831/35
HW Rev(s): All
A. For traditional analog FM tuners, the FM AFC range by standard measurement procedures is normally
between 150 and 500 kHz, but for Si4831/35, the tested AFC range is at 40–60 kHz based on the traditional
test method. The Si4831/35 has a digital architecture with an advanced tuning algorithm; therefore, it has
dynamic AFC range. When PVR is rotated during tuning, Si4831/35 broadens its AFC range to around
+/-500 kHz for easy station capturing and locking. When tuning is stopped, Si4831/35 automatically narrows its
AFC range to 40–60 kHz for excellent selectivity performance.
Q: How do I minimize the frequency display position hysteresis with PVR tuning?
Keyword(s): Position Hysteresis, Frequency Display, PVR tuning
Device(s): Si4831/35
HW Rev(s): All
A. The position hysteresis of the frequency display is caused by PVR itself and/or the mechanical structure of
the frequency display method. Si4831/35 itself has no frequency display hysteresis issue. PVRs are normally
used for volume control, where hysteresis is not an issue. Test results showed some PVRs have hysteresis
angles up to 4-5 degrees. Ask your PVR vendor to minimize the PVR position hysteresis. Most of the existing
mechanical structures for traditional analog radio frequency display method also fix the issue.
Q3" SILIEIJNUIIS
Si4831/35 FAQ
Rev. 0.1 11
NOTES:
$96 SlllEflN’lAflS
Si4831/35 FAQ
12 Rev. 0.1
CONTACT INFORMATION
Silicon Laboratories Inc.
400 West Cesar Chavez
Austin, TX 78701
Tel: 1+(512) 416-8500
Fax: 1+(512) 416-9669
Toll Free: 1+(877) 444-3032
Please visit the Silicon Labs Technical Support web page:
https://www.silabs.com/support/pages/contacttechnicalsupport.aspx
and register to submit a technical support request.
Silicon Laboratories and Silicon Labs are trademarks of Silicon Laboratories Inc.
Other products or brandnames mentioned herein are trademarks or registered trademarks of their respective holders.
The information in this document is believed to be accurate in all respects at the time of publication but is subject to change without notice.
Silicon Laboratories assumes no responsibility for errors and omissions, and disclaims responsibility for any consequences resulting from
the use of information included herein. Additionally, Silicon Laboratories assumes no responsibility for the functioning of undescribed features
or parameters. Silicon Laboratories reserves the right to make changes without further notice. Silicon Laboratories makes no warranty, rep-
resentation or guarantee regarding the suitability of its products for any particular purpose, nor does Silicon Laboratories assume any liability
arising out of the application or use of any product or circuit, and specifically disclaims any and all liability, including without limitation conse-
quential or incidental damages. Silicon Laboratories products are not designed, intended, or authorized for use in applications intended to
support or sustain life, or for any other application in which the failure of the Silicon Laboratories product could create a situation where per-
sonal injury or death may occur. Should Buyer purchase or use Silicon Laboratories products for any such unintended or unauthorized ap-
plication, Buyer shall indemnify and hold Silicon Laboratories harmless against all claims and damages.

Products related to this Datasheet

BOARD DEMO SI4831 SI4835 24-SSOP